Arduino Tutorials
  • Products & Partners
  • Arduino
  • Arduino Tutorials
  • More
  • Cancel
Arduino Tutorials
Forum Fix bricked (I think) Uno R3
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino Tutorials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 25 subscribers
  • Views 4381 views
  • Users 0 members are here
Related

Fix bricked (I think) Uno R3

gsd13
gsd13 over 5 years ago

Is there any way possible to fix a bricked Uno R3? At least I believe its bricked. Have removed driver from original com port and reinstalled. No avail. Have tried updating boards in IDE. No avail. It has worked before as I used it as an ISP to flash my 3d printer MB. Could this have caused a problem with the bootloader?

Thanks for any assistance in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • ajcc
    ajcc over 5 years ago +2 suggested
    To make sure you didn't damage the board I would test if the USB-to-serial adapter works on the board. You can do this by sticking a ~1k ohm resistor between D0 and D1 (RX and TX) and then use the Serial…
  • gsd13
    gsd13 over 5 years ago in reply to ajcc +1
    Tried to loop test. Didn't work with any option you suggested above. I am missing a dll from required dir that flip is calling for. I was reading that it is supposed to be in 3 different directories but…
Parents
  • ajcc
    0 ajcc over 5 years ago

    To make sure you didn't damage the board I would test if the USB-to-serial adapter works on the board. You can do this by sticking a ~1k ohm resistor between D0 and D1 (RX and TX) and then use the Serial Monitor in the Arduino IDE to see if what you type comes back. Don't forget to pull the resistor to make sure it's really coming back and not just echoing locally. If that works then something might be wrong with the Atmega328P. If it doesn't work then it could also be that the Arduino is driving the pins high or low, so test it when holding down reset too.

     

    If you don't have a way to program the chip then the cheapest way to revive your board would be to just buy a pre-programmed Atmega328Ppre-programmed Atmega328P with the Arduino bootloader in it already. But that will only fix it if the board isn't damaged.

     

    Since you already know how to use an Arduino as an ISP programmer I assume you only have one and can't reprogram the Atmega328P that way? It's strange that the bootloader would be damaged, but I don't know if Arduino write protect that part of flash, I'd assume it would do.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gsd13
    0 gsd13 over 5 years ago in reply to ajcc

    I have heard about Flip. Might that be the answer. If there is a way to flash a bootloader from an Uno to a Anet A8 V1.5 3d printer mb (this was to run a Marlin sketch for better hotbed safety), would it be wrong to think that I should be able to do the same with a Mega 2560 to an Uno?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ajcc
    0 ajcc over 5 years ago in reply to gsd13

    gsd13 The ArduinoISP sketch seems to support the Mega board, since it's shown programming an Arduino UNO in the tutorial: https://www.arduino.cc/en/Tutorial/BuiltInExamples/ArduinoISP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ajcc
    0 ajcc over 5 years ago in reply to gsd13

    gsd13 The ArduinoISP sketch seems to support the Mega board, since it's shown programming an Arduino UNO in the tutorial: https://www.arduino.cc/en/Tutorial/BuiltInExamples/ArduinoISP