Arduino
  • Products & Partners
  • More
Arduino
Blog Arduino-based Smart Watering of Plants
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: madhugovindarajan
  • Date Created: 28 Jan 2019 6:22 PM Date Created
  • Views 1116 views
  • Likes 3 likes
  • Comments 4 comments
Related
Recommended

Arduino-based Smart Watering of Plants

madhugovindarajan
madhugovindarajan
28 Jan 2019

I found this example really detailed and thorough.

 

https://www.mathworks.com/help/supportpkg/arduino/examples/arduino-based-smart-watering-of-plants.html

 

Any thoughts on what other sensors can come in handy when one uses smart techniques in agricultural space?

  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +5
    You should go with a capacitive sensor for the soil moisture sensor. If you use the sensor shown at 5V, you will find that the sensor contacts will corrode and become erratic. If you lower the voltage…
  • luislabmo
    luislabmo over 7 years ago +3
    On a watering system the most relevant sensor is perhaps the Soil moisture sensor, which is generally used to determine the watering cycle (or the right time to irrigate the plants). Moisture sensors are…
  • madhugovindarajan
    madhugovindarajan over 7 years ago in reply to luislabmo

    Thanks for the suggestions. We will evaluate all the options and hopefully come with an improved version.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 7 years ago

    On a watering system the most relevant sensor is perhaps the Soil moisture sensor, which is generally used to determine the watering cycle (or the right time to irrigate the plants). Moisture sensors are of many types; each with their own set of advantages/disadvantages.

     

    For your Arduino project, the best soil moisture sensors may be RF based like the Vegetronix or Capacitive moisture sensors as these won't have exposed metals that will corrode over time. As DAB has suggested try avoiding Resistive moisture sensors; these are cheap but will corrode real quick, one may suggest to use AC and/or stainless steel but the truth is this will just delay the end result (corrosion) and SS in electrolysis is highly toxic (and other metals).

     

    Other sensors that may be incorporated:

    • UV sensor, helping detect real sun-light (unlike ambient light sensors)
    • Water level sensors, when using a water tank reservoir (filled manually or with rainwater, etc.) which could help alerting under critical water level conditions and also help preserving the water-pump life
    • Temperature

    UV and Temperature sensors won't help much deciding the watering cycles but may help deciding whether certain type of plant is under ideal conditions to grow/survive

     

    Luis

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • madhugovindarajan
    madhugovindarajan over 7 years ago in reply to DAB

    Thanks for sharing that information, I did not know that. Will pass on the information to the right teams here in MathWorks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 7 years ago

    You should go with a capacitive sensor for the soil moisture sensor.

    If you use the sensor shown at 5V, you will find that the sensor contacts will corrode and become erratic.

    If you lower the voltage to about 1V, then you prolong the life of the sensor.

     

    Electrolysis starts at about 1.25 volts, so you want to stay below that value.

     

    DAB

    • Cancel
    • Vote Up +5 Vote Down