Arduino
  • Products & Partners
  • More
Arduino
Blog Arduino Due w/LCD 20 x 4 cursor location
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 19 Jun 2013 7:51 PM Date Created
  • Views 1255 views
  • Likes 0 likes
  • Comments 2 comments
Related
Recommended

Arduino Due w/LCD 20 x 4 cursor location

e14 Contributor
e14 Contributor
19 Jun 2013

I have an Arduino Due interfeced to an LCD (4 line x 20 char).

Its a standard connection scheme using all 8 data bits in this case.

Here is my issue:

I have a program that prints values from 7 analog inputs A0-A6.

I write to A0-A3 in char position 0, lines 0-3 and A4-A6 in char position 01, lines 0-2 in a continuos loop.

My problem is the postion of each value start out as ok but after a little while the items bounce around in

location and it all gets messed up.  Im puzzled.  Can anyone offer ideas?  Ive tried quite a bit to fix it.

Here is my code that Im running in the Arduino Due.

Thanks.

 

Ken

 

 

/****************************************************************************/
#include <LiquidCrystal.h>
/****************************************************************************/
int led = 13;
//LiquidCrystal lcd(12, 11, 5, 4, 3, 2);
LiquidCrystal lcd(12, 11, 9, 8, 7, 6, 5, 4, 3, 2);

/****************************************************************************/
void setup()
{
  // put your setup code here, to run once:
      
pinMode(led, OUTPUT); // initialize the digital pin as an output.
 
Serial1.begin(9600); // initialize serial communication at 9600 bits per second:
lcd.begin(20,4);
lcd.clear();
lcd.home();
lcd.noCursor();

}

void loop() {
   // read the input on analog inputs A0-A6:

      analogReadResolution(12);   // sat analog read resolution to 12 bit, 0-4095
      int sensor0 = analogRead(A0);int sensor1 = analogRead(A1);int sensor2 = analogRead(A2);int sensor3 = analogRead(A3);int sensor4 = analogRead(A4);int sensor5 = analogRead(A5);int sensor6 = analogRead(A6);
        
   // Convert the analog reading (which goes from 0 - 4095) to a voltage (0 - 3.3V):
  
    float sensorV0 = sensor0 * (3.3 / 4095.0);
    float sensorV1 = sensor1 * (3.3 / 4095.0);
    float sensorV2 = sensor2 * (3.3 / 4095.0);
    float sensorV3 = sensor3 * (3.3 / 4095.0);
    float sensorV4 = sensor4 * (3.3 / 4095.0);
    float sensorV5 = sensor5 * (3.3 / 4095.0);
    float sensorV6 = sensor6 * (3.3 / 4095.0);

   // print out tthe (7) analog values
Serial1.print("A0=");Serial1.print(sensorV0,3); Serial1.print("\t");
Serial1.print("A1="); Serial1.print(sensorV1,3);Serial1.print("\t");
Serial1.print("A2=");Serial1.print(sensorV2,3); Serial1.print("\t");
Serial1.print("A3="); Serial1.print(sensorV3,3); Serial1.print("\t");
Serial1.print("A4=");Serial1.print(sensorV4,3); Serial1.print("\t");
Serial1.print("A5="); Serial1.print(sensorV5,3);Serial1.print("\t");
Serial1.print("A6=");Serial1.println(sensorV6,3);

//lcd.setCursor(0,0);
//lcd.print("A6=");lcd.print(sensorV6,3);
lcd.clear();
//lcd.setCursor(0,0);
lcd.print("A0= ");lcd.print(sensorV0,3);
lcd.setCursor(0,1);lcd.print("A1= ");lcd.print(sensorV1,3);
lcd.setCursor(0,2);lcd.print("A2= ");lcd.print(sensorV2,3);
lcd.setCursor(0,3);lcd.print("A3= ");lcd.print(sensorV3,3);
lcd.setCursor(11,0);lcd.print("A4= ");lcd.print(sensorV4,3);
lcd.setCursor(11,1);lcd.print("A5= ");lcd.print(sensorV5,3);
lcd.setCursor(11,2);lcd.print("A6= ");lcd.print(sensorV6,3);

 
digitalWrite(led, HIGH);   // turn the LED on (HIGH is the voltage level)
delay(250);               // wait for a second
digitalWrite(led, LOW);    // turn the LED off by making the voltage LOW

  
delay(500); // a little delay to not hog serial monitor
   // bottom of loop
}

  • Sign in to reply
  • neilk
    neilk over 13 years ago

    I tried (some of) your code on a UNO, driving a 16 x 2 LCD and I was surprised to find that it behaved perfectly without the lcd.setCursor(0,0)

     

    Like David Shaddock, I would have assumed that it was necessary to reset the cursor to (0,0) each time you go round the loop. Apparently not on a 16 x 2, but maybe it is necessary on a 20 x 4.

     

    Best wishes

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Just under the lcd.clear(); line, you have commented out the lcd.setCursor command.  So analog voltage A0 is going to print pretty much wherever the cursor happens to be.  It seems to me that clearing the lcd doesn't restore the cursor to a fixed position, but I haven't worked with the 20X4 display yet; it all depends on what the lcd library says to do.  It may leave the cursor in a random place, or it may remain where it landed last.