Arduino
  • Products & Partners
  • More
Arduino
Blog Arduino  FSK Shield (433MHz)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 6 Dec 2012 3:10 PM Date Created
  • Views 1413 views
  • Likes 1 like
  • Comments 1 comment
  • 433.92mhz
  • rf
  • arduino
  • fsk
  • altelectronics
Related
Recommended

Arduino  FSK Shield (433MHz)

e14 Contributor
e14 Contributor
6 Dec 2012

Dear fellows,

 

We are proud to present a shield that we make, mainly for receiving FSK (and OOK) signals from sensors but not only. The shield comes with a duck antenna and demo examples. 

 

FSK signals at 433MHz are very commonly used by consumer electronics devices including weather stations, power consumption meters, security systems, and home automation controllers.
The RF transceiver used is RF12 from Hope Electronics, this means that the shield is using SPI.
The advantages of SPI are that it runs at a higher data rate, and it has separate input and output connections, so it can send and receive at the same time. It uses one additional line per device to select the active device, so more connections are required if you have many devices to connect. Most Arduino projects use SPI devices for high data rate applications such as Ethernet and memory cards, with just a single device attached.
Arduino releases (from release 0019) include a library that allows communication with SPI devices.

Manufacturer: Altelectronics
Manufacturer Part No: ARD-RF433-SHL

imageimage

Schematics, and software libs are availble for download from out website
Please feel free to ask questions or give feeback if you wish,
Have Fun,
Aurash
  • Sign in to reply
  • Arunasstn
    Arunasstn over 1 year ago

    where found arduino library for this shield ?