Arduino
  • Products & Partners
  • More
Arduino
Blog Arduino Input multiplexer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tabarus12
  • Date Created: 22 Feb 2013 5:27 PM Date Created
  • Views 1314 views
  • Likes 1 like
  • Comments 1 comment
Related
Recommended

Arduino Input multiplexer

tabarus12
tabarus12
22 Feb 2013

This is my latest arduino shield that I made to experiment.

 

It is based on the 74ls151 input multiplexer, you can add more to eatch input that you need turning it in to an 8 bit input.

 

Here are some pictured and a basic schematic and code to read it.

 

Note, the resistor stripe is connecting the inputs to ground for use with switches, remove them to have a true digital input.

 

Have fun using it its very usefull, I know I will.image

Attachments:
image
image
image
Digital_Input_Multiplexer.ino.zip
imageDigital input multiplexer.pdf
  • Sign in to reply
  • tabarus12
    tabarus12 over 13 years ago

    Here a corrected version of the multiplexer program.

     

    Ive added a correction to the array and a for routine to pront serial data to port. Enjoyimage

     

     

    #include<Streaming.h>

     

    int b0 = 8; //Declare bit 0 pin

    int b1 = 9; //Declare bit 1 pin

    int b2 = 10; //Declare bit 2 pin

    int d1 = 11; //Declare data pin 1

    int d2 = 12; //Declare data pin 2

     

    int data1[9] = {0,0,0,0,0,0,0,0}; //Declare data 1 array

    int data2[9] = {0,0,0,0,0,0,0,0}; //Declare data 2 array

    int a = 1; //Declare array position variable

     

    void setup() {

      pinMode(b0,OUTPUT); //Set bit cero pin to output

      pinMode(b1,OUTPUT); //Set bit one pin to output

      pinMode(b2,OUTPUT); //Set bit two pin to output

     

      pinMode(d1,INPUT); //Set data pin 1 to input

      pinMode(d2,INPUT); //Set data pin 2 to input

     

      Serial.begin(9600); //Start serial port transmition

    }

     

    void loop() {

      a=1; //Set array position to 1

     

      for(a=1; a<=9; a++) { //Encrease aray position

        Bin(); //Call for binary print run

        if(digitalRead(d1) == HIGH) { //On data pin 1 enable

          data1[a]=1; //Set data array 1 position value to 1

        }

        else { //On data pin 1 disabled

          data1[a]=0; //Set data 1 array 1 position value to 0

        }

        if(digitalRead(d2) == HIGH) { //On data pin 2 enable

          data2[a]=1; //Set data array 2 position to 1

        }

        else { //On data 2 pin disable

          data2[a]=0; //Set data aray 2 position to 1

        }

        delay(50); //Delat for slow IC

                  //Remove if using fast speed IC

      }

      a=1;

      Serial << "  Mux A   MuxB" << endl;

      for(a=1; a<=8; a++){

        Serial << data1[a];

      }

      a=1;

      Serial << " ";

      for(a=1; a<=8; a++) {

        Serial << data2[a];

      }

      a=1;

      Serial << endl;

      //Print data array 1 and 2 value to serial port

    }

     

    void Bin() { //Binary print routine

      switch (a) { //Select on array position

        case 1: //On first case

          digitalWrite(b0, LOW); //Set bin 0 pin to 0

          digitalWrite(b1, LOW); //Set bin 1 pin to 0

          digitalWrite(b2, LOW); //Set bin 2 pin to 0

          break; //Break case

        case 2: //On second case

          digitalWrite(b0, HIGH); //Set bin 0 pin to 1

          digitalWrite(b1, LOW); //Set bin 1 pin to 0

          digitalWrite(b2, LOW); //Set bin 2 pin to 0

          break; //Break case

        case 3: //On third case

          digitalWrite(b0, LOW); //Set bin 0 pin to 0

          digitalWrite(b1, HIGH); //Set bin 1 pin to 1

          digitalWrite(b2, LOW); //Set bin 2 pin to 0

          break; //Break case

        case 4: //On fourth case

          digitalWrite(b0, HIGH); //Set bin 0 pin to 1

          digitalWrite(b1, HIGH); //Set bin 1 pin to 1

          digitalWrite(b2, LOW); //Set bin 2 pin to 0

          break; //Break case

        case 5: //On fifth case

          digitalWrite(b0, LOW); //Set bin 0 pin to 0

          digitalWrite(b1, LOW); //Set bin 1 pin to 0

          digitalWrite(b2, HIGH); //Set bin 2 pin to 1

          break; //Break case

        case 6: //On sixth case

          digitalWrite(b0, HIGH); //Set bin 0 pin to 1

          digitalWrite(b1, LOW); //Set bin 1 pin to 0

          digitalWrite(b2, HIGH); //Set bin 2 pin to 1

          break; //Break case

        case 7: //On seventh case

          digitalWrite(b0, LOW); //Set bin 0 pin to 0

          digitalWrite(b1, HIGH); //Set bin 1 pin to 1

          digitalWrite(b2, HIGH); //Set bin 2 pin to 1

          break; //Break case

        case 8: //On eight case

          digitalWrite(b0, HIGH); //Set bin 0 pin to 1

          digitalWrite(b1, HIGH); //Set bin 1 pin to 1

          digitalWrite(b2, HIGH); //Set bin 2 pin to 1

          break; //Break case

      }

    }