Arduino
  • Products & Partners
  • More
Arduino
Blog Arduino Nano RP2040 Connect is now available
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 21 May 2021 3:56 PM Date Created
  • Views 3678 views
  • Likes 8 likes
  • Comments 5 comments
  • arduino nano rp2040 connect
  • arduino mbed
  • imu
  • rp2040
  • ublox nina
Related
Recommended

Arduino Nano RP2040 Connect is now available

ralphjy
ralphjy
21 May 2021

I noticed that the Arduino Nano RP2040 Connect  is now available in the Arduino store.  I've been waiting for this board as it adds WiFi and BLE capability to the RP2040  and also adds a microphone, IMU, and 16MB of flash memory.  I can't wait to try it out.  I've seen some complaining about the high cost - $25.50 and the lack of a USB-C connector, but I remember when the Uno was about $20 and we've come a long way since then.  It is already supported in the Arduino IDE as an Mbed board, so it should be easy to get started.

 

image

 

Board Nano RP2040 Connect with Headers

SKU: ABX00053

Microcontroller Raspberry Pi RP2040

USB connector Micro USB

Pins Built-in LED pin 13

Digital I/O Pins 20

Analog Input Pins 8

PWM pins 20 (Except A6, A7)

External interrupts 20 (Except A6, A7)

  Connectivity  Wi-Fi Nina W102 uBlox module

Bluetooth Nina W102 uBlox module

Secure element ATECC608A-MAHDA-T Crypto IC

 

Sensors IMU LSM6DSOXTR (6-axis)

Microphone MP34DT05

Communication UART Yes

I2C Yes

SPI Yes

Power Circuit operating voltage 3.3V

Input Voltage (VIN) 5-21V

DC Current per I/O pin 4 mA

Clock speed Processor 133 MHz

Memory AT25SF128A-MHB-T 16MB Flash IC

Nina W102 uBlox module 448 KB ROM, 520KB SRAM, 16MB Flash

Dimensions Weight 6 g

Width 18 mm

Length 45 mm

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 5 years ago +4
    I was going to say this feels fairly similar to the ESP32, give or take a few features such as a couple of sensors added. But, it actually has an ESP32 : ) The on-board Nina W102 module according to the…
  • dubbie
    dubbie over 5 years ago +3
    This looks good, but as you say, a bit expensive. I might wait until it becomes a bit cheaper, actually, quite a lot cheaper. Does look fun though. I'll probably be able to do every mobile robot project…
  • robogary
    robogary over 5 years ago in reply to dubbie +2
    I had the same thought, where is the camera ? :-) Add a couple servos , attach wings, it becomes a spy cicada robot.
  • DAB
    DAB over 5 years ago

    I look forward to seeing what you find.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • BigG
    BigG over 5 years ago in reply to shabaz

    Just spotted this on the Arduino github page for the Arduino mbed core: "With the latest version (ArduinoCore-mbed 2.1.0) it is possible to use the pico SDK multicore functions..."

     

    So you could say that this little board is a quasi-quad-core. image

     

    The question I'm wondering about is whether you could get both the RP2040 and the ESP32 to share flash (in general, rather than with this particular board config) with a bit a clever memory allocation. Could save a few pence.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 5 years ago in reply to dubbie

    I had the same thought, where is the camera ? :-)   Add a couple servos , attach wings, it becomes a spy cicada robot.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 5 years ago

    I was going to say this feels fairly similar to the ESP32, give or take a few features such as a couple of sensors added. But, it actually has an ESP32 : ) The on-board Nina W102 module according to the PDF datasheet contains an ESP32 inside it!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 5 years ago

    This looks good, but as you say, a bit expensive. I might wait until it becomes a bit cheaper, actually, quite a lot cheaper.

     

    Does look fun though. I'll probably be able to do every mobile robot project I'll ever want to do with one of these. Although, it doesn't have any video - yet!

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down