Arduino
  • Products & Partners
  • More
Arduino
Blog Arduino Portenta - Person Detection
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 25 Oct 2021 2:01 AM Date Created
  • Views 5369 views
  • Likes 0 likes
  • Comments 0 comments
  • mqtt
  • portenta vision shield
  • tinyml
  • person detection
  • arduino portenta h7
Related
Recommended

Arduino Portenta - Person Detection

ralphjy
ralphjy
25 Oct 2021

I recently virtually attended the Arm DevSummit 2021.  One of the workshops was hosted by Edge Impulse and used the Arduino Portenta H7 with the Vision Shield to do Object Classification.  That got me interested in trying to do Object Detection - specifically Person Detection using the Portenta and Mbed OS.

 

I found an example developed by ARM software that basically does just that - TinyML person detection project with Arduino, TensorFlow and Mbed OS.

 

I've also seen OpenMV IDE examples that run with MicroPython, but my preference is to stay within the Arduino IDE framework which is using the Mbed OS - so I decided to give the ARM software example a try.   The example runs a Tensorflow TinyML Person Detection model on the Portenta and posts detection results and images to an HTTP server.  The images and detection results are then viewable in a web browser.  There is a github repo for this project - https://github.com/ARM-software/developer/tree/master/projects/portenta_person_detection .

 

The first step in all my TinyML camera projects is to print a tripod mount so that I can get stable images.  Here is the Portenta with Ethernet vision shield on a desktop tripod (I am using WiFi, not wired Ethernet).  You can see the WiFi antenna sticking out to the right.

image

 

I ran into immediate issues compiling the example code because the Arduino Mbed board libraries have been evolving rapidly and this example is over 6 months old.  Because this project is split over multiple files, I elected not to try to resolve all the versioning issues and just reverted back to the board library that was used with this example - Arduino Mbed OS Boards version 1.3.2 (this library has been deprecated).  The example will compile and work with this older library.

 

Here are files that are used for this project:

image

 

If things will compile, running the example is straightforward.  You need to create a config.h file that contains your WiFi access point info and the ip address of the host computer where the image server is running.

 

config.h

/*
Copyright 2021 Chariot Solutions Inc. (https://chariotsolutions.com)
and ARM (https://arm.com) All Rights Reserved.

Licensed under the Apache License, Version 2.0 (the "License");
you may not use this file except in compliance with the License.
You may obtain a copy of the License at

    http://www.apache.org/licenses/LICENSE-2.0

Unless required by applicable law or agreed to in writing, software
distributed under the License is distributed on an "AS IS" BASIS,
WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
See the License for the specific language governing permissions and
limitations under the License.
==============================================================================*/

/*
 * Put your wifi access point credentials here and save as config.h
 * DO NOT commit config.h to version control
 * DO NOT save / commit this file with password present
 */

#ifndef PERSON_DETECTION_CONFIG_H
#define PERSON_DETECTION_CONFIG_H

#define WIFI_SSID "SSID"
#define WIFI_PASS "PASS"
#define SERVER_IP_ADDRESS "0.0.0.0"

#endif // PERSON_DETECTION_CONFIG_H

 

The model file is contained in a C array in the person_detect_model_data.cpp file which is about 1.4 MB in size.

 

The person_detection.ino program loads and initializes the model, runs the inference, and forwards the results and images to the image server. The RGB LED blinks BLUE for each inference and turns GREEN if a person is detected and RED if no person is detected.

 

person_detection.ino

#include <TensorFlowLite.h>

/* Copyright 2019 The TensorFlow Authors. All Rights Reserved.

Licensed under the Apache License, Version 2.0 (the "License");
you may not use this file except in compliance with the License.
You may obtain a copy of the License at

    http://www.apache.org/licenses/LICENSE-2.0

Unless required by applicable law or agreed to in writing, software
distributed under the License is distributed on an "AS IS" BASIS,
WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
See the License for the specific language governing permissions and
limitations under the License.
==============================================================================*/

/*
   Modified 2021-01-20 and 2021-02-16, Rich Freedman, Chariot Solutions, Inc. (https://chariotsolutions.com)
   for ARM (https://arm.com)

   - Make the code work with the Arduino Portenta H7 board and Portenta Vision Shield
     - Get image from camera at 320x240 (since it's the only size that works reliably right now)
     - Crop 320x240 image to square (240x240)
     - Scale 240x240 image to 96x96 as expected by TensorFlow

   - Optionally write images to the SD Card (kinda broken - often crashes after a few writes)
   - Optionally HTTP Post images to a server for display
   - Optionally log non-errors ("info") to the serial console
   - Update to work with Arduino/Mbed library version 1.3.2
*/

#include <TensorFlowLite.h>

#include "main_functions.h"

#include "detection_responder.h"
#include "image_provider.h"
#include "model_settings.h"
#include "person_detect_model_data.h"
#include "tensorflow/lite/micro/kernels/micro_ops.h"
#include "tensorflow/lite/micro/micro_error_reporter.h"
#include "tensorflow/lite/micro/micro_interpreter.h"
#include "tensorflow/lite/micro/micro_mutable_op_resolver.h"
#include "tensorflow/lite/schema/schema_generated.h"
#include "tensorflow/lite/version.h"

#include "SDMMCBlockDevice.h"
#include "FATFileSystem.h"

#include "ImageCropper.h"
#include "ImageScaler.h"
#include "ImageSender.h"

int image_count = 0; // affects tensor_arena alignment, but doesn't behave properly inside namespace

// Globals, used for compatibility with Arduino-style sketches.
namespace {

    /** Declare no variables before this, so as not to affect the tensor_arena alignment **/
    // tensor_arena - An area of memory to use for input, output, and intermediate arrays.
    // Requires 16 byte alignment - adjust tensor_arena_alignment_shift as necessary if you get an alignment warning at runtime
    constexpr int kTensorArenaSize = 93 * 1024;
    constexpr size_t tensor_arena_alignment_shift = 4;
    constexpr size_t tensor_arena_padded_size = kTensorArenaSize + tensor_arena_alignment_shift;
    static uint8_t tensor_arena[tensor_arena_padded_size];
    uint8_t *p_tensor_arena = tensor_arena + tensor_arena_alignment_shift;

    tflite::ErrorReporter* error_reporter = nullptr;
    const tflite::Model* model = nullptr;
    tflite::MicroInterpreter* interpreter = nullptr;
    TfLiteTensor* input = nullptr;

    constexpr bool use_sd_card = false;
    constexpr bool write_scaled_image = false;
    constexpr bool send_scaled_image = true;
    constexpr bool write_serial_info = true; // controls "info" output only - errors will always be written
    constexpr int images_to_write = 5;

    // SD Card block device and filesystem
    SDMMCBlockDevice block_device;
    mbed::FATFileSystem fs("fs");

    constexpr int pd_large_image_width = 320;
    constexpr int pd_large_image_height = 240;
    constexpr int pd_large_image_size = (pd_large_image_width * pd_large_image_height);
    constexpr int pd_cropped_dimension = 240;
    constexpr int pd_cropped_size = pd_cropped_dimension * pd_cropped_dimension;

    uint8_t largeImage[pd_large_image_size];
    uint8_t croppedImage[pd_cropped_size];
    uint8_t scaledImage[kMaxImageSize];

    boolean sd_card_initialized = false;
    boolean wifi_initialized = false;

    char filename[255];

    ImageCropper image_cropper;
    ImageScaler image_scaler;
    ImageSender image_sender;

}  // namespace

boolean init_sd_card()
{
  delay(2000);

  int err =  fs.mount(&block_device);
  if (err) {
    // Reformat if we can't mount the filesystem
    // this should only happen on the first boot
    Serial.println("formatting sd card");
    err = fs.reformat(&block_device);

    if(err) {
      Serial.print("failed to mount or reformat file system - error code = ");
      Serial.println(err);
      return false;
    }

    Serial.println("init_sd_card done formatting sd card");
  }

  return true;
}

void write_image_to_sd_card(const char* image_type, const uint8_t* image_data, int imageWidth, int imageHeight, int imageSize, int imageNum, const char *recognition)
{
    // form the file name
    sprintf(filename, "/fs/image_%s_%d_%dx%d_%d_%s.raw", image_type, imageNum, imageWidth, imageHeight, imageSize, recognition);

    if(write_serial_info) {
        Serial.print("writing ");
        Serial.print(imageSize);
        Serial.print(" bytes to SD card as ");
        Serial.println(filename);
    }

    FILE *file = fopen(filename, "wb");
    if(file != NULL) {
        size_t chunk_size = 512;
        size_t total_bytes_written = 0;
        while(total_bytes_written < (size_t) imageSize) {
             size_t write_size = min(chunk_size, imageSize - total_bytes_written);
             size_t bytes_written = fwrite(image_data + total_bytes_written, 1, write_size, file);
             total_bytes_written += bytes_written;
             if(bytes_written == 0)  {
                fclose(file);
                Serial.print("failed to write file ");
                Serial.println(filename);
                return;
             }
             if(bytes_written != write_size) {
                Serial.print("short write - attempted ");
                Serial.print(chunk_size);
                Serial.print(", wrote only ");
                Serial.println(bytes_written);
             }

             delay(20);
        }

        fclose(file);

        if(write_serial_info) {
            Serial.print("wrote ");
            Serial.print(total_bytes_written);
            Serial.println(" bytes to SD Card");
        }
    } else {
        Serial.print("fopen failed with error ");
        Serial.println(errno);
    }
}

void setup()
{
  Serial.begin(115200);
  while (!Serial);

  Serial.println("ARM Portenta H7 TensorFlow Person Detection Demo\n");

  if(use_sd_card && write_serial_info) {
      Serial.println("Initializing SD card...");
  }

  if(use_sd_card) {
      if (!init_sd_card()) {
          Serial.println("SD card initialization failed, won't write images");
      } else {
          sd_card_initialized = true;

          if(write_serial_info) {
              Serial.println("SD card initialization done. Images will be written");
          }
      }
  }

  // Set up logging. Google style is to avoid globals or statics because of
  // lifetime uncertainty, but since this has a trivial destructor it's okay.
  // NOLINTNEXTLINE(runtime-global-variables)
  static tflite::MicroErrorReporter micro_error_reporter;
  error_reporter = &micro_error_reporter;

  // Map the model into a usable data structure. This doesn't involve any
  // copying or parsing, it's a very lightweight operation.
  model = tflite::GetModel(g_person_detect_model_data);
  if (model->version() != TFLITE_SCHEMA_VERSION) {
    TF_LITE_REPORT_ERROR(error_reporter,
     "Model provided is schema version %d not equal "
     "to supported version %d.", model->version(), TFLITE_SCHEMA_VERSION
    );
    return;
  }

  // Pull in only the operation implementations we need.
  // This relies on a complete list of all the ops needed by this graph.
  // An easier approach is to just use the AllOpsResolver, but this will
  // incur some penalty in code space for op implementations that are not
  // needed by this graph.
  //
  // NOLINTNEXTLINE(runtime-global-variables)
  static tflite::MicroMutableOpResolver<3> micro_op_resolver;
  micro_op_resolver.AddDepthwiseConv2D();
  micro_op_resolver.AddConv2D();
  micro_op_resolver.AddAveragePool2D();

  // Build an interpreter to run the model with.
  static tflite::MicroInterpreter static_interpreter(model, micro_op_resolver, p_tensor_arena, kTensorArenaSize, error_reporter);
  
  interpreter = &static_interpreter;

  // Allocate memory from the tensor_arena for the model's tensors.
  TfLiteStatus allocate_status = interpreter->AllocateTensors();
  if (allocate_status != kTfLiteOk) {
    TF_LITE_REPORT_ERROR(error_reporter, "AllocateTensors() failed");
    return;
  }

  // Get information about the memory area to use for the model's input.
  input = interpreter->input(0);

  if(send_scaled_image) {
      if(write_serial_info) {
          Serial.println("connecting to wifi");
      }

      if (image_sender.connect_to_wifi(error_reporter) == kTfLiteOk) {
          wifi_initialized = true;

          if(write_serial_info) {
              Serial.println("wifi connected, will attempt to send images to server");
          }
      } else {
          Serial.println("wifi connection failed, will NOT attempt to send images to server");
      }
  }

}

void loop()
{
  if(write_serial_info) {
      Serial.println();
      Serial.println("==============================");
      Serial.println();
      Serial.print("Getting image ");
      Serial.print(image_count);
      Serial.print(" (");
      Serial.print(pd_large_image_width);
      Serial.print("x");
      Serial.print(pd_large_image_height);
      Serial.println(") from camera");
  }

  // get 'large' image from the provider
  if (kTfLiteOk != GetImage(error_reporter, pd_large_image_width, pd_large_image_height, kNumChannels, largeImage)) {
    Serial.println("Image capture failed.");
    return;
  }

  // crop the image to the square aspect ratio that the model expects (will crop to center)
  if(write_serial_info) {
      Serial.print("Cropping image to ");
      Serial.print(pd_cropped_dimension);
      Serial.print("x");
      Serial.println(pd_cropped_dimension);
  }

  image_cropper.crop_image(largeImage, pd_large_image_width, pd_large_image_height, croppedImage, pd_cropped_dimension, pd_cropped_dimension);

  // scale the image to the size that the model expects (96x96)
  if(write_serial_info) {
      Serial.print("Scaling image to ");
      Serial.print(kNumCols);
      Serial.print("x");
      Serial.println(kNumRows);
  }
  int scale_result = image_scaler.scale_image_down(croppedImage, pd_cropped_dimension, pd_cropped_dimension, scaledImage, kNumRows, kNumCols);
  if(scale_result < 0) {
      Serial.println("Failed to scale image");
      return;
  }

  // copy the scaled image to the TF input
  if(write_serial_info) {
      Serial.println("Copying scaled image to TensorFlow model");
  }
  memcpy(input->data.uint8, scaledImage, kMaxImageSize);

  // Run the model on this input and make sure it succeeds.
  if(write_serial_info) {
      Serial.println("Invoking the TensorFlow interpreter");
  }

  if (kTfLiteOk != interpreter->Invoke()) {
    Serial.println("TensorFlow Invocation failed.");
    return;
  }

  TfLiteTensor* output = interpreter->output(0);

  // Process the inference results
  uint8_t person_score = output->data.uint8[kPersonIndex];
  uint8_t no_person_score = output->data.uint8[kNotAPersonIndex];
  RespondToDetection(error_reporter, person_score, no_person_score);

  // write out the scaled image to the SD Card if present
  if(write_scaled_image && sd_card_initialized && image_count < images_to_write) {
     if(write_serial_info) {
          Serial.print("Writing scaled image ");
          Serial.print(image_count);
          Serial.println(" to sd card");
      }

      write_image_to_sd_card("scaled", scaledImage, kNumRows, kNumCols, kMaxImageSize, image_count, person_score > no_person_score ? "PERSON" : "NOPERSON");
  }

  if(send_scaled_image && wifi_initialized) {
      if(write_serial_info) {
          Serial.print("Sending image ");
          Serial.print(image_count);
          Serial.println(" to server");
      }

      // To send the 96x96 image, if desired
      // TfLiteStatus sendStatus = image_sender.send_image(error_reporter, scaledImage, kNumRows, kNumCols, person_score, no_person_score);

      // send the 240x240 image to the server
      TfLiteStatus sendStatus = image_sender.send_image(error_reporter, croppedImage, pd_cropped_dimension, pd_cropped_dimension, person_score, no_person_score);
      if (sendStatus != kTfLiteOk) {
          Serial.println("image send failed");
      }
  }

  image_count++;
}

 

The Himax HM-01B0 camera on the Vision Shield has a monochrome 320x320 sensor that supports QVGA resolution and is capturing at 320x240 in this example.  The image is cropped to 240x240 and scaled to 96x96 for use with the inference model.  The scaled image is sent to the image server, so the image that you get is pretty low resolution - but it works for positioning the field of view and reduces the time required to transmit the image.

 

The Image Server is a Python Flask application running on my Windows 10 PC that is also the host for the Arduino IDE.  The server creates an image viewer in a web browser at port 5000.  I've never used Flask before, so it's another thing to learn image..  The recommendation is to run in a Python virtual environment, so that you don't affect the system environment.

 

I also wanted to add MQTT to the Arduino code so that I could publish the detection result to use in other applications.  I read that others have had issues using the MQTT PubSubClient (that I normally use) with the Portenta library, so I elected to use the arduino-mqtt library (https://github.com/256dpi/arduino-mqtt ) .  I did a simple pub/sub loopback test with that library and it worked.

 

Of course, the devil is in the details...  I've never used MQTT and HTPP simultaneously over WiFi before and when I added the MQTT code - it worked, but the Image Server would no longer connect image.  I guess it is obvious (but not to me) that you cannot use the same WiFi client (which I had done) with two different open connections simultaneously.  I created a separate instance of the WiFi client for MQTT and that fixed the problem.

 

Here is a demo of it working.  I am having issues with the video setup that I use to capture windows on my PC (crashes the computer), so I ended up using my iPhone to capture the video.  I had to do it in two separate videos.  The first shows the Image Viewer and the MQTT dashboard side-by-side and the second video shows the Portenta Serial monitor and the Image Server command window.
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
. The update rate is about 3-5 seconds which I hope is just caused by the overhead of sending the image data.  I'll need to see how much improvement I can get if I just do the inference and publish over MQTT.