Arduino
  • Products & Partners
  • More
Arduino
Blog Arduino using hall effect sensor and servo
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 21 Apr 2012 7:15 AM Date Created
  • Views 1271 views
  • Likes 1 like
  • Comments 2 comments
Related
Recommended

Arduino using hall effect sensor and servo

e14 Contributor
e14 Contributor
21 Apr 2012

I am trying to use a hall effect sensor to activate a servo. I want the servo to move to a specific position when the hall effect sensor is activated and then move back when the sensor is deactivated. When I go to the analog read and look at the values I get from the hall effect sensor, the values are 0 when deactivated, but they range from 195-215 when acivated. I think this is why the servo twitches, but im not certain. I think I should have the input read 0 or 1. When he input is 1 the servo should move to this position and move back for values of 0.  Can you help me out? Heres the code I have so far

 

 

 

 

 

 

#include <Servo.h>

 

Servo myservo;  // create servo object to control a servo

 

int inPin = 0;    // select the input pin for the Hall Effect Sensorr

int val;    // variable to read the value from the analog pin

 

void setup()

{

  myservo.attach(9);  // attaches the servo on pin 9 to the servo object

}

 

void loop()

{

  val = analogRead(inPin);            // reads the value of the Hall Effect Sensorr (value between 0 and 300)

  val = map(val, 0, 300, 0, 20);     // scale it to use it with the servo (value between 0 and 20)

  myservo.write(val);                  // sets the servo position according to the scaled value

  delay(15);                           // waits for the servo to get there

  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    You havnt add constrain and mapping properly. Try this code:

    #include <Servo.h>

     

    Servo myservo; 

     

    int inPin = 0;  

    int val;   

     

    void setup()

    {

      myservo.attach(9);

    }

     

    void loop()

    {

      val = analogRead(inPin);

      val = constrain(val, 0, 275); 

      val = map(val, 0, 300, 0, 180);    

      myservo.write(val);                 

      delay(25); 

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    If you looking for help on this it would be better to post this as a new discussion rather then a blog post.