Arduino
  • Products & Partners
  • More
Arduino
Blog Arduino with Current Transformer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: yyynmh
  • Date Created: 19 Oct 2016 4:22 AM Date Created
  • Views 995 views
  • Likes 0 likes
  • Comments 2 comments
  • current transformer
  • arduino
Related
Recommended

Arduino with Current Transformer

yyynmh
yyynmh
19 Oct 2016

Hi!

 

Does anyone has any experience with current transformer with arduino?

I just bought a split core current transformer (SCT-0400-025) from Magnelab and I want to connect to arduino.

According to the datasheet, the input current is 25A and output voltage will be 0.333V. Should i connect any burden resistor? & how should i go about doing it?

 

Please help!

 

Thank you~

  • Sign in to reply
  • D_Hersey
    D_Hersey over 9 years ago in reply to Robert Peter Oakes

    Or an active rectifier

     

    http://ww1.microchip.com/downloads/en/AppNotes/01353A.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    As per the datasheet, it already has a burden resistor so does not need an additional one

     

    You will however probably need an op amp to boost the signal as your only going to get 0.333V at full 25A, this limits the ADCs range quite a lot. A 10x amplification would help a lot taking the input to the ADC to 3.33V, you could use more gain to increase output to close to 5V if your using a 5V reference on the ADC, if not then you will have to adjust to align with the ADC full scale.

     

    Also the output of the CT is not DC, it is AC so you will have to sample quite fast to profile the waveform, either that or use a diode and a cap to rectify the signal