Arduino
  • Products & Partners
  • More
Arduino
Blog Arno Shield introduces a new way to begin with an Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 15 May 2013 7:44 PM Date Created
  • Views 623 views
  • Likes 1 like
  • Comments 0 comments
  • open-source
  • project
  • cabeatwell
  • learning
  • prototyping
  • arno_shield
  • platform
  • arduino_development
  • arduino
  • beginner
Related
Recommended

Arno Shield introduces a new way to begin with an Arduino

Catwell
Catwell
15 May 2013

image

Learn with Arno Shield... A where to begin complete learning platform (via Olympia Circuits)

 

As many people already know, the Arduino is a versatile platform. It is a great place to start when learning about embedded electronics, or a great stepping-stone to learning about electronics in general. However, some people still struggle to begin with the Arduino and may have difficulties building and connecting circuits for the first time. Peter Gould and Kevin Warner recognized this when they began selling Arduino boards at Maker Faires. As a result, they released what they called the Arno kit.

 

The Arno kit was basically an Arduino board with a bunch of electronic components integrated on to the same board. In addition, they wrote a book to help getting started with the Arno kit. Along with explaining how the electronics on the board worked it also covers over 40 example programs, all with details on what is going on with each line of code. Although the board was a great creation to creating accessible electronics for beginners, their book, Learning Arduino with the Arno, was a hit among many people and was extremely well written.

 

Now the creators have developed their next invention, the Arno Shield. The Arno shield takes a similar approach as the Arno kit did; however, instead of having a board with the Arduino processor and all the components together, they created a shield for Arduinos, which comes packed with components. Therefore, beginners can still work with the easy to use Arno board, but when the time comes to move on, they could just pop off the shield and begin to wire up their experiment.

 

Furthermore, since the shield features all the original components the kit had, they have also decided to include their book in a convenient package deal. The package will run for $60, but as they say, the knowledge gained can be priceless. The components featured on the board include: four green LEDs, one RGB LED, One infrared LED, two push button switches, a thumbwheel potentiometer, a piezobuzzer, a phototransistor, and a temperature sensor.

 

The world of electronics is now more accessible than ever. The Arduino introduced a great way to begin working with microcontrollers. On the other hand, some people who are interested in the Arduino may be hesitant to start due to the fact that they will be learning electronics, programming, and breadboarding all at the same time. For those people the Arno kit and shield is here for you. Along with a well written book, there is no better place to start and no more reasons to be intimidated.

 

C

See more news at:

http://twitter.com/Cabe_e14