Arduino
  • Products & Partners
  • More
Arduino
Blog Build a range scanner using an Arduino and MATLAB
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: anujaapte
  • Date Created: 29 Aug 2014 4:04 PM Date Created
  • Views 1322 views
  • Likes 1 like
  • Comments 1 comment
  • matlab
  • stepper
  • ir
  • arduino
  • simulink
  • range
Related
Recommended

Build a range scanner using an Arduino and MATLAB

anujaapte
anujaapte
29 Aug 2014

I had recently talked about how you can control servo motors using an Arduino and Simulink. I stumbled upon an interesting application which builds on the same topic. The video shows how you can use an IR sensor coupled with a stepper motor to get a rotational range scanner (I would have ideally called it a Mini Radar, but for the fact that the sensor uses infrared waves instead of radio waves). The stepper motor is controlled using an Arduino UNO and an Arduino MotorShield. The Arduino is connected via USB to a PC running MATLAB with Arduino Support from MATLAB.

 

The stepper motor is driven in steps of 1.8 degrees using MATLAB code. At each step, the output of the IR Sensor is passed to MATLAB, where it is converted into an appropriate distance measure using pre-calibrated function. The author also provides a link to a MATLAB implementation of SLAM (Simultaneous Localization and Mapping) which can be used as starting point for creating the functions to obtain distance information.

 

Check out the video and its description as well for more details about the project:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I know my next project is building this device using servo motors instead and can definitely see a user interface similar to a radar monitor to view the results. Have other ideas about this contraption? Feel free to share!

  • Sign in to reply
  • amgalbu
    amgalbu over 11 years ago

    Nice work!
    What is limiting the scanning speed? I don't thing a servo is going to ge better, especially because you will not have a 360 degrees scan

     

    Compliments again

    Ambrogio