Arduino
  • Products & Partners
  • More
Arduino
Blog BYOB Party #7 - Mrs YUN gets chatty with iot.eclipse.org and NRF24L01
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Robert Peter Oakes
  • Date Created: 29 Dec 2014 10:55 AM Date Created
  • Views 1906 views
  • Likes 3 likes
  • Comments 7 comments
  • iot_holidaylights
  • byob_party
Related
Recommended

BYOB Party #7 - Mrs YUN gets chatty with iot.eclipse.org and NRF24L01

Robert Peter Oakes
Robert Peter Oakes
29 Dec 2014

link back to primary post BYOB Party #1, "Bring you own Bulbs" - The Internet of Holiday Lights

 

In this episode I will demonstrate and provide all the code used to allow a browser / smartphone / tablet to adjust the colour of a light strip that is connected via an NRF24L01 2.5Ghz wireless link

 

In a previous episode I showed how to get Mosquitto server, pub and sub clients loaded into the YUN and how to use them

 

This post is extending on Benjamin Cabé's excellent demonstration and after finding all the scripts and getting the page hosted by the YUN itself I have a working demonstration that looks like the following

 

image

 

I can enter colours from either a subscription to the wheel ("theBreadBoard_Strip") being hosted at iot.elcipse.org or by entering colour selections directly at the YUN or the UNO via their serial terminals

 

Pay attention to case as the subscriptions are case sensitive

 

any changes via the wheel is almost instantly relayed to the UNO and subsequently displayed on the light strip,

 

The UNO is supporting a command interpreter to allow direct commands to be sent to it via any configured input mechanism (Serial or NRF at this time)

The YUN is supporting a simpler command structure at this time and simply relays the commands it receives onto the UNO via the NRF radio

 

A point to note is the YUN does not support the standard output pins for SPI, namely the MISO, MOSI and SCK lines do not exist on pins 11, 12, 13 and are only accessible via the programming header and the Infineon Shield needs stacking headers if your to add additional IO devices like a NRF24L01

 

Once all the pins where sorted out it was simply a matter of finding all the additional libraries for the web page to operate, the basic functionality required for talking to iot.elcipse.org of course comes from the PAHO js libraries but the colour wheel , Raphael and the boostrap all had to be found

 

Bootstrap · The world's most popular mobile-first and responsive front-end framework.

Raphaël—JavaScript Library

Color Wheel Demo

 

on the YUN you need to create a folder and sub folder in the root of a micro SD card "/arduino/www", once loaded into the YUN it immediately shows up at this location under the LINUX "/mnt/sda1/arduino/www" and a simpler path "/www/sd", from the home network it can be accessed as "http://arduino.local/sd/", it will automatically serve index.html


I have zipped up the SD card structure and attached for you to use


also the modified sketches for the YUN and the UNO with MQTT support and NRF24L01, there not cleaned up yet but they all work


I will be cleaning up the sketches as I add more functionality etc, I am getting close to full ram usage so it is essential before I continue much further


here is a quick video to show how it functions,

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image



Attachments:
XmasLight.zip
arduino.zip
  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to kartben +1
    that may be true in some cases and while I do have access to hosting pages on the net, not everyone does or would want to, the deployment of the page really is immaterial in the scheme of things, the more…
  • jdlui
    jdlui over 10 years ago +1
    Peter, Thanks again for helping me dive into this world of Arduino and embedded programming back in 2014! Doing my masters over in Vancouver right now and I'm still coming back to these posts and learning…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to jdlui +1
    You're more than welcome and if you want to directly chat you can email me peter@thebreadboard.ca and lets not forget my YouTube channel http://www.youtube.com/thebreadboardca
  • DAB
    DAB over 11 years ago

    Nice update Peter,

     

    How close can you control the spectral output of the LED's?

     

    I am thinking about using the LEDs to look at spectral differences of various materials using a webcam.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kartben
    kartben over 11 years ago

    Cool stuff image However I think it kind of defeats the purpose of having a web app if it has to be served by the Yun, no? My point being it is probably easier to access a webpage that is on a public IP/URL rather than on an Arduino behind your home Internet router?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<