Arduino
  • Products & Partners
  • More
Arduino
Blog Celebrating E14 deliveries * more Christmas in July 2023 *
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: robogary
  • Date Created: 3 Jul 2023 8:32 PM Date Created
  • Views 988 views
  • Likes 12 likes
  • Comments 1 comment
  • robogary
  • arduino_uno
  • arduino uno R4
  • arduino
Related
Recommended

Celebrating E14 deliveries * more Christmas in July 2023 *

robogary
robogary
3 Jul 2023

A Big celebration at RoboGary's house 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Thank you E14 and tariq.ahmad  

A Nicla Vision prize from a previous webinar, and a Arduino UNO R4 MINIMA and an Arduino UNO R4 wifi.

*See the last photo*, it was an unexpected delight when the Arduino R4 LED matrix default powers up with a heart demo.  

There are so many useful features added for Rev 4 

  • The boards can be powered via the VIN pin, supporting a range between 6-24 V
  • A real-time clock (RTC) is used to measure the time and is useful in any time-tracking application.
  • The UNO R4 Minima board features two separate hardware serial ports. One port is connected via USB-C®, and one is connected via RX/TX pins.
  • The UNO R4 also has a DAC with up to 12-bit resolution, that can act as a genuine analog output pin.
  • The analog outputs default resolution is set to 10-bit but can be declared for 12 and 14-bit resolutions. 
  • A real-time clock (RTC) is used to measure the time and is useful in any time-tracking application.

image

image

image

image

  • Sign in to reply
  • DAB
    DAB over 3 years ago

    Nice, I look forward to seeing you put them to use.

    • Cancel
    • Vote Up -1 Vote Down