Arduino
  • Products & Partners
  • More
Arduino
Blog Fast Track to Arduino Programming - Lesson 0, An Empty Sketch
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Robert Peter Oakes
  • Date Created: 9 Jun 2014 3:45 AM Date Created
  • Views 944 views
  • Likes 2 likes
  • Comments 0 comments
  • fast-track
  • sketch
  • ethernet
  • programming
  • fast_track_to_arduino_programming
  • tutorials
  • rogramming - lesson 4a
  • arduino
Related
Recommended

Fast Track to Arduino Programming - Lesson 0, An Empty Sketch

Robert Peter Oakes
Robert Peter Oakes
9 Jun 2014

In this first intro lesson I describe the basic sketch and concept of limited memory and that even an empty sketch uses up valuable system resources

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

/*
Title: Lesson 0. how big is an empty Sketch anyway

Description:  Reading a line of text from the Serial Port and sending to a command process function.
Date created: 27 May 2014
Created By: Peter Oakes
Additional Comments:
Feel free to use and abuse as you wish, I imply NO Warranty
NOTE: defines take no program space untill used so use instead of ints etc when it will never change
Lessons Available
lesson 0. How big is an Empty Sketch anyway
Lesson 1. Reading the Serial input a line at time
Lesson 2. Parsing the line using  "if else if" statements
Lesson 3. Improved parsing and reduced SRAM consumption - "Case" Statements
lesson 4. Reading the Ethernet input a line at time (WEB Query)
lesson 5. Combining Serial and Ehernet into a common sketch
lesson 6. Advanced parsing of commands without "If" or "Case" statements
lesson 7. Adding input buttons to the command control

*/
// Bunch of constants in the form of definitions
// 1 = output debug to serial port, 0 = no debug
#define debug 1 
// define the buffer size... 
#define serialbufferSize 50 
// End of Constants

// Now the real varibles
//char inputBuffer[serialbufferSize]   ; 
//int serialIndex = 0; // keep track of where we are in the buffer
// End of real variables
void setup() 
{ 
  // initialize serial:
//  Serial.begin(9600);
  // do other setup here as needed
}
void loop() 
{
  // Notice how the main loop is very simple and the functions 
  // seperate the logic into easily manageable parts
//  if (CheckSerial()) DoCommand(inputBuffer);
}
//boolean DoCommand(char * commandBuffer)
//{
//  
//#if debug
//  Serial.println(commandBuffer);
//  Serial.print("Free Ram = "); Serial.println(freeRam(), DEC);
//#endif  
//return true;
//}
//
///*
//Checks the serial input for a string, returns true once a '\n' is seen
//users can always look at the global variable "serialIndex" to see if characters have been received already
//*/
//boolean CheckSerial()
//{
//  boolean lineFound = false;
//  // if there's any serial available, read it:
//  while (Serial.available() > 0) {
//    //Read a character as it comes in:
//    //currently this will throw away anything after the buffer is full or the \n is detected
//    char charBuffer = Serial.read(); 
//      if (charBuffer == '\n') {
//           inputBuffer[serialIndex] = 0; // terminate the string
//           lineFound = (serialIndex > 0); // only good if we sent more than an empty line
//           serialIndex=0; // reset for next line of data
//         }
//         else if(serialIndex < serialbufferSize && lineFound == false) {
//           /*Place the character in the string buffer:*/
//           inputBuffer[serialIndex++] = charBuffer; // auto increment index
//         }
//  }// End of While
//  return lineFound;
//}// End of CheckSerial()
//
//#if debug
//// check free ram and return as an integer
//int freeRam () 
//{
//  extern int __heap_start, *__brkval; 
//  int v; 
//  return (int) &v - (__brkval == 0 ? (int) &__heap_start : (int) __brkval); 
//}
//#endif

 

Back to Menu/Intro Page Fast Track to Arduino Programming

Attachments:
Arduino_Lesson_0_An_Empty_Sketch.ino.zip