• Products and Partners
    Products and Partners
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
Arduino
  • Products and Partners
  • More
Arduino
Blog Fast Track to Arduino Programming - Lesson 2, parsing the serial input into usable commands
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Robert Peter Oakes
  • Date Created: 9 Jun 2014 4:05 AM Date Created
  • Views 3527 views
  • Likes 1 like
  • Comments 0 comments
  • fast-track
  • tutorial
  • programming
  • fast_track_to_arduino_programming
  • intermediate
  • arduino
Related
Recommended

Fast Track to Arduino Programming - Lesson 2, parsing the serial input into usable commands

Robert Peter Oakes
Robert Peter Oakes
9 Jun 2014

Now we have seen how to read the serial port we will now expand the capability to include examining the content of the data and comparing to pre-defined strings in order to take different actions based on what was sent

In this tutorial we only send back message to the console, not performing actual IO to any of the built in hardware (That will be in the next lesson). this lesson focuses on simply building up a program capable of making decisions as commanded from the console. The syntax used in this lesson sticks to the commonly used approach of "If, then, Else". It also explores the 3 main comparison functions "==". "strstr" and "strcmp", why one works, one does not and well one kind of works.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

/*
Title: Lesson 2. Parsing the line using  "if else if" statements and == or strcmp
 
Description:  Reading a line of text from the Serial Port and sending to a command process function.
the processing function only echos back to the console for this lesson
This sketch also demonstrates the use of compiler directives to turn on and off blocks of functionality
Date created: 27 May 2014
Created By: Peter Oakes
Additional Comments:
Feel free to use and abuse as you wish, I imply NO Warranty
NOTE: defines take no program space untill used so use instead of ints etc when it will never change
Lessons Available
lesson 0. How big is an Empty Sketch anyway
Lesson 1. Reading the Serial input a line at time
Lesson 2. Parsing the line using  "if else if" statements and == or strcmp
Lesson 3. Improved parsing and reduced SRAM consumption - "Case" Statements
lesson 4. Reading the Ethernet input a line at time (WEB Query)
lesson 5. Combining Serial and Ehernet into a common sketch
lesson 6. Advanced parsing of commands without "If" or "Case" statements
lesson 7. Adding input buttons to the command control

*/

// Bunch of constants in the form of definitions
// 1 = output debug to serial port, 0 = no debug
#define debug 1 
// define the buffer size... 
#define serialbufferSize 50 
// End of Constants
// Now the real varibles
char inputBuffer[serialbufferSize]   ; 
int serialIndex = 0; // keep track of where we are in the buffer
// End of real variables
void setup() 
{ 
  // initialize serial:
  Serial.begin(9600);
  // do other setup here as needed
  
  // Print some pretty instructions
  Serial.println("Hello, please ask me something");
  Serial.println("type \"Hello\", \"Goodby\", \"web\" or \"dosomething\" or make up your own command");
  Serial.println();
}
void loop() 
{
  // Notice how the main loop is very simple and the functions 
  // seperate the logic into easily manageable parts
  if (CheckSerial()) DoCommand(inputBuffer); 
  // Do other stuff
}
boolean DoCommand(char * commandBuffer)
{
  // Standard way to handle commands
  if (strstr(commandBuffer, "Hello")){
    Serial.println("Hello back at you ");
    //    Do some other work here
    //    and here
    //    and here
  }  
  else if (commandBuffer == "Goodby"){
    Serial.println("Hello back at you ");
    //    Do some other work here
    //    and here
    //    and here
  }
  else if (strcmp(commandBuffer , "dosomething")==0){
    Serial.println("Like what ?? ");
    //    Do some other work here
    //    and here
    //    and here
  }
  else if (strstr(commandBuffer , "web")){
    Serial.println("HTTP/1.1 200 OK");
    Serial.println("Content-Type: text/html");
    Serial.println("Connection: close");
    Serial.println();
    Serial.println("<!DOCTYPE html>");
    Serial.println("<html><head><title>TEST</title></head>");
    Serial.println("<body><h1>Hello from www.thebreadboard.ca</h1></body>");
    Serial.println("</html>");
    //    Do some other work here
    //    and here
    //    and here
  }
  else {
    Serial.print("I dont understand you \nYou said: ");
    Serial.println(commandBuffer);
    //    Do some other work here
    //    and here
    //    and here
  }
  
  
  // debug code after here
#if debug
  Serial.print("Free Ram = "); Serial.println(freeRam(), DEC);
#endif  
return true;
}
/*
Checks the serial input for a string, returns true once a '\n' is seen
users can always look at the global variable "serialIndex" to see if characters have been received already
*/
boolean CheckSerial()
{
  boolean lineFound = false;
  // if there's any serial available, read it:
  while (Serial.available() > 0) {
    //Read a character as it comes in:
    //currently this will throw away anything after the buffer is full or the \n is detected
    char charBuffer = Serial.read(); 
      if (charBuffer == '\n') {
           inputBuffer[serialIndex] = 0; // terminate the string
           lineFound = (serialIndex > 0); // only good if we sent more than an empty line
           serialIndex=0; // reset for next line of data
         }
         else if(charBuffer == '\r') {
           // Just ignore the Carrage return, were only interested in new line
         }
         else if(serialIndex < serialbufferSize && lineFound == false) {
           /*Place the character in the string buffer:*/
           inputBuffer[serialIndex++] = charBuffer; // auto increment index
         }
  }// End of While
  return lineFound;
}// End of CheckSerial()
#if debug
// check free ram
int freeRam () 
{
  extern int __heap_start, *__brkval; 
  int v; 
  return (int) &v - (__brkval == 0 ? (int) &__heap_start : (int) __brkval); 
}
#endif

 

 

Back to Menu/Intro Page Fast Track to Arduino Programming

Attachments:
Arduino_Lesson_2___Parsing_the_commands_from_Serial.ino.zip