Arduino
  • Products
  • More
Arduino
Blog IDE ATA Hard Drive with ATmega328p MCU as Controller Question
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: iexpress
  • Date Created: 29 Dec 2014 8:33 PM Date Created
  • Views 3575 views
  • Likes 3 likes
  • Comments 6 comments
  • arduino
Related
Recommended

IDE ATA Hard Drive with ATmega328p MCU as Controller Question

iexpress
iexpress
29 Dec 2014

Hi All,

 

I tried to open a discussion but the website wouldn't publish it so I just created a quick blog about this project.

 

I was planning to make a quick IDE hard drive controller with an ATmega328p, and was wondering if anyone might know how the internal buffer addresses are incremented inside the hard drive during read/write operations?

 

Is there a set rate data has to be read from or written to the hard drive, or would the read/write pins be toggled to load the next set of 16 bit word during the read/write operations?

 

I'm a little confused, searching for tutorials, but they're not describing how the addresses are incremented, they're just saying read or write 512 bytes in one shot for either read or write sector operation.

 

Your help would be appreciated, thanks.

 

I know there are pre-written libraries, but I'll be interfacing this in a circuit of it's ow connected directly to an ATmega which will act solely as a dedicated IDE controller using the LBA access scheme.

  • Sign in to reply

Top Comments

  • muffenme
    muffenme over 11 years ago in reply to iexpress +1
    Did you read this An 8-bit IDE interface @ Retroleum Here some C program for PC Simplix - ide.c Finally I think someone made something for Arduino board this is it Paul's 8051 Code Library, IDE Hard Drive…
  • clem57
    clem57 over 11 years ago +1
    Originally I tried to access the hard drive using Cylinder/Head/Sector (CHS) addressing, and it would not work properly. All of these early attempts were with a Western Digital 1.2 gig drive. I could read…
  • clem57
    clem57 over 11 years ago in reply to iexpress +1
    Here is code I found to base what I know: ; Simple communication with an IDE disk drive ; see http://www.pjrc.com/tech/8051/ide/ for more info ; Modified, January 2005: ; - Update for rev 4/5 8051 development…
  • iexpress
    iexpress over 11 years ago in reply to clem57

    Thanks, I read through the assembly and think I can get it working with the ATmega328p. The missing Init command was probably why I couldn't read or write sectors. I'll give this a try in the morning and post results. It would be amazing if that's all it was. In this example, they sent 0xA0 to register 6 b10100000 while I was using 0xE0 b11100000. I suppose I can try it either way to see which one works. Pretty anxious to get it going, it was a little frustrating. I'll have to connect the hard drive again and give it a go. Thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to iexpress

    Here is code I found to base what I know:

     

    ; Simple communication with an IDE disk drive
    ; see http://www.pjrc.com/tech/8051/ide/ for more info
    
    ; Modified, January 2005:
    ; - Update for rev 4/5 8051 development board
    ; - Fix hold time bug when writing to some drives
    ; - Improve reporting of drive's model/serial/revision
    ; - Added (commented out) status output while waiting for drive
    ; - Other minor cleanup
    
    ; This code is an original work by Paul Stoffregen, written
    ; in December 1999 (modified 2005). This code has been placed
    ; in the ; public domain. You may use it without any restrictions.
    ; You may include it in your own projects, even commercial
    ; (for profit) products.
    
    ; This code is distributed in the hope that they will be useful,
    ; but without any warranty; without even the implied warranty of
    ; merchantability or fitness for a particular purpose.
    
    
    .equ location, 0x2100 ;where this program will exist
    .equ buffer, 0x3000 ;a 512 byte buffer
    
    ;------------------------------------------------------------------
    ; Hardware Configuration
    
    ;8255 chip. Change these to specify where the 8255 is addressed,
    ;and which of the 8255's ports are connected to which ide signals.
    ;The first three control which 8255 ports have the control signals,
    ;upper and lower data bytes. The last two are mode setting for the
    ;8255 to configure its ports, which must correspond to the way that
    ;the first three lines define which ports are connected.
    .equ ide_8255_lsb, 0xF800 ;lower 8 bits
    .equ ide_8255_msb, 0xF801 ;upper 8 bits
    .equ ide_8255_ctl, 0xF802 ;control lines
    .equ cfg_8255, 0xF803
    .equ rd_ide_8255, 10010010b ;ide_8255_ctl out, ide_8255_lsb/msb input
    .equ wr_ide_8255, 10000000b ;all three ports output
    
    ;ide control lines for use with ide_8255_ctl. Change these 8
    ;constants to reflect where each signal of the 8255 each of the
    ;ide control signals is connected. All the control signals must
    ;be on the same port, but these 8 lines let you connect them to
    ;whichever pins on that port.
    .equ ide_a0_line, 0x01 ;direct from 8255 to ide interface
    .equ ide_a1_line, 0x02 ;direct from 8255 to ide interface
    .equ ide_a2_line, 0x04 ;direct from 8255 to ide interface
    .equ ide_cs0_line, 0x08 ;inverter between 8255 and ide interface
    .equ ide_cs1_line, 0x10 ;inverter between 8255 and ide interface
    .equ ide_wr_line, 0x20 ;inverter between 8255 and ide interface
    .equ ide_rd_line, 0x40 ;inverter between 8255 and ide interface
    .equ ide_rst_line, 0x80 ;inverter between 8255 and ide interface
    
    
    ;------------------------------------------------------------------
    ; More symbolic constants... these should not be changed, unless of
    ; course the IDE drive interface changes, perhaps when drives get
    ; to 128G and the PC industry will do yet another kludge.
    
    ;some symbolic constants for the ide registers, which makes the
    ;code more readable than always specifying the address pins
    .equ ide_data, ide_cs0_line
    .equ ide_err, ide_cs0_line + ide_a0_line
    .equ ide_sec_cnt, ide_cs0_line + ide_a1_line
    .equ ide_sector, ide_cs0_line + ide_a1_line + ide_a0_line
    .equ ide_cyl_lsb, ide_cs0_line + ide_a2_line
    .equ ide_cyl_msb, ide_cs0_line + ide_a2_line + ide_a0_line
    .equ ide_head, ide_cs0_line + ide_a2_line + ide_a1_line
    .equ ide_command, ide_cs0_line + ide_a2_line + ide_a1_line + ide_a0_line
    .equ ide_status, ide_cs0_line + ide_a2_line + ide_a1_line + ide_a0_line
    .equ ide_control, ide_cs1_line + ide_a2_line + ide_a1_line
    .equ ide_astatus, ide_cs1_line + ide_a2_line + ide_a1_line + ide_a0_line
    
    ;IDE Command Constants. These should never change.
    .equ ide_cmd_recal, 0x10
    .equ ide_cmd_read, 0x20
    .equ ide_cmd_write, 0x30
    .equ ide_cmd_init, 0x91
    .equ ide_cmd_id, 0xEC
    .equ ide_cmd_spindown, 0xE0
    .equ ide_cmd_spinup, 0xE1
    
    
    ;------------------------------------------------------------------
    ;internal ram usage
    
    .equ lba, 0x10 ;4 bytes, 28 bit Logical Block Address
    .equ stack, 0x40
    
    
    
    ;routines within paulmon2. To make this code stand-alone, just copy
    ;and paste these bits of code from the paulmon2.asm file.
    
    .equ cout, 0x0030 ;Send Acc to serial port
    .equ cin, 0x0032 ;Get Acc from serial port
    .equ phex, 0x0034 ;Print Hex value of Acc
    .equ pstr, 0x0038 ;Print string pointed to by DPTR,
    .equ upper, 0x0040 ;Convert Acc to uppercase
    .equ newline, 0x0048 ;print CR/LF (13 and 10)
    .equ pint8u, 0x004D ;print Acc at an integer, 0 to 255
    .equ pint16u, 0x0053 ;print DPTR as an integer, 0 to 65535
    .equ cin_filter, 0x0062 ;get a character, but look for esc sequences
    
    
    ;------------------------------------------------------------------
    ; Main Program, a simple menu driven interface.
    
    
    .org location
    .db 0xA5,0xE5,0xE0,0xA5 ;signiture bytes
    .db 35,255,0,0 ;id, 35=program
    .db 0,0,0,0 ;reserved
    .db 0,0,0,0 ;reserved
    .db 0,0,0,0 ;reserved
    .db 0,0,0,0 ;reserved
    .db 0,0,0,0 ;user defined
    .db 255,255,255,255 ;length and checksum (255=unused)
    .db "IDE Disk Drive Test",0
    .org location+64 ;executable code begins here
    
    
    begin:
     mov sp, #stack
     mov dptr, #msg_1 ;print a welcome message
     lcall pstr
    
     ;reset the drive
     acall ide_hard_reset
    
     ;initialize the drive. If there is no drive, this may hang
     acall ide_init
    
     ;get the drive id info. If there is no drive, this may hang
     acall drive_id
    
     ; print the drive's model number
     mov dptr, #msg_mdl
     lcall pstr
     mov dptr, #buffer + 54
     mov r0, #20
     acall print_name
     lcall newline
    
     ; print the drive's serial number
     mov dptr, #msg_sn
     lcall pstr
     mov dptr, #buffer + 20
     mov r0, #10
     acall print_name
     lcall newline
    
     ; print the drive's firmware revision string
     mov dptr, #msg_rev
     lcall pstr
     mov dptr, #buffer + 46
     mov r0, #4
     acall print_name
     lcall newline
    
     ; print the drive's cylinder, head, and sector specs
     mov dptr, #msg_cy
     lcall pstr
     mov dptr, #buffer + 2
     acall print_parm
     mov dptr, #msg_hd
     lcall pstr
     mov dptr, #buffer + 6
     acall print_parm
     mov dptr, #msg_sc
     lcall pstr
     mov dptr, #buffer + 12
     acall print_parm
     lcall newline
     lcall newline
    
     ; default position will be first block (master boot record)
     clr a
     mov lba+0, a
     mov lba+1, a
     mov lba+2, a
     mov lba+3, a
    
    
    main_loop: ;print a 1-line prompt
     mov dptr, #msg_l
     lcall pstr
     mov a, lba+3
     lcall phex
     mov a, lba+2
     lcall phex
     mov a, lba+1
     lcall phex
     mov a, lba+0
     lcall phex
     mov dptr, #msg_pmt
     lcall pstr
     lcall cin
     lcall upper
    
    main1: cjne a, #'R', main2 ;read a sector
     acall read_sector
     jz main1b
     push acc
     mov dptr, #msg_err
     lcall pstr
     pop acc
     lcall phex
     lcall newline
     ajmp main_loop
    main1b: mov dptr, #msg_rd
     lcall pstr
     ajmp main_loop
    
    main2: cjne a, #'W', main3 ;write a sector
     mov dptr, #msg_sure
     lcall pstr
     lcall cin
     lcall upper
     cjne a, #'Y', main2c
     acall write_sector
     jz main2b
     push acc
     mov dptr, #msg_err
     lcall pstr
     pop acc
     lcall phex
     lcall newline
     ajmp main_loop
    main2b: mov dptr, #msg_wr
     lcall pstr
    main2c: ajmp main_loop
    
    main3: cjne a, #'L', main4 ;set the logical block address
     mov dptr, #msg_cyh
     lcall pstr
     lcall ghex32_lba
     jc main3b
     mov lba+0, r3
     mov lba+1, r4
     mov lba+2, r5
     mov lba+3, r6
    main3b: lcall newline
     ajmp main_loop
    
    main4: cjne a, #'U', main5 ;cause the drive to spin up
     acall spinup
     ajmp main_loop
    
    main5: cjne a, #'D', main6 ;cause the drive to spin down
     acall spindown
     ajmp main_loop
    
    main6: cjne a, #'Q', main7 ;quit
     ljmp 0
    
    main7: cjne a, #'H', main8
     acall hexdump
     ajmp main_loop
    
    main8: ajmp main_loop
    
    
    msg_1: .db "IDE Disk Drive Test Program",13,10,13,10,0
    msg_mdl:.db "Model: ",0
    msg_sn: .db "S/N: ",0
    msg_rev:.db "Rev: ",0
    msg_cy: .db "Cylinders: ", 0
    msg_hd: .db ", Heads: ", 0
    msg_sc: .db ", Sectors: ", 0
    msg_cyh:.db "Enter LBA (in hex): ", 0
    msg_l: .db "LBA=0x",0
    msg_pmt:.db ", (R)ead (W)rite (L)BA (U)p (D)own (H)exdump (Q)uit",13,10,0
    msg_sure:.db "Warning: this will change data on the drive, are you sure?",13,10,0
    
    msg_rd: .db "Sector Read OK",13,10,0
    msg_wr: .db "Sector Write OK",13,10,0
    msg_err:.db "Error, code = ",0
    
    
    
    
    
    ;------------------------------------------------------------------
    ; Routines that talk with the IDE drive, these should be called by
    ; the main program.
    
    
     ;read a sector, specified by the 4 bytes in "lba",
     ;Return, acc is zero on success, non-zero for an error
    read_sector:
     acall ide_wait_not_busy ;make sure drive is ready
     acall wr_lba ;tell it which sector we want
     mov a, #ide_command
     mov r2, #ide_cmd_read
     acall ide_wr_8 ;ask the drive to read it
     acall ide_wait_drq ;wait until it's got the data
     jb acc.0, get_err
     mov dptr, #buffer
     acall read_data ;grab the data
     clr a
     ret
    
    
     ;when an error occurs, we get acc.0 set from a call to ide_drq
     ;or ide_wait_not_busy (which read the drive's status register). If
     ;that error bit is set, we should jump here to read the drive's
     ;explaination of the error, to be returned to the user. If for
     ;some reason the error code is zero (shouldn't happen), we'll
     ;return 255, so that the main program can always depend on a
     ;return of zero to indicate success.
    get_err:mov a, #ide_err
     acall ide_rd_8
     mov a, r2
     jz gerr2
     ret
    gerr2: mov a, #255
     ret
    
    
     ;write a sector, specified by the 4 bytes in "lba",
     ;whatever is in the buffer gets written to the drive!
     ;Return, acc is zero on success, non-zero for an error
    write_sector:
     acall ide_wait_not_busy ;make sure drive is ready
     acall wr_lba ;tell it which sector we want
     mov a, #ide_command
     mov r2, #ide_cmd_write
     acall ide_wr_8 ;tell drive to write a sector
     acall ide_wait_drq ;wait unit it wants the data
     jb acc.0, get_err
     mov dptr, #buffer
     acall write_data ;give the data to the drive
     acall ide_wait_not_busy ;wait until the write is complete
     jb acc.0, get_err
     clr a
     ret
    
    
    
     ;do the identify drive command, and return with the buffer
     ;filled with info about the drive
    drive_id:
     acall ide_wait_not_busy
     mov a, #ide_head
     mov r2, #10100000b
     acall ide_wr_8 ;select the master device
     acall ide_wait_ready
     mov a, #ide_command
     mov r2, #0xEC
     acall ide_wr_8 ;issue the command
     acall ide_wait_drq
     mov dptr, #buffer
     acall read_data
     ret
    
    
    
    
    
    
    
    
    
    
     ;tell the drive to spin up
    spinup:
     mov r2, #ide_cmd_spinup
    spup2: mov a, #ide_command
     acall ide_wr_8
     acall ide_wait_not_busy
     ret
    
    
     ;tell the drive to spin down
    spindown:
     acall ide_wait_not_busy
     mov r2, #ide_cmd_spindown
     sjmp spup2
    
    
    
     ;initialize the ide drive
    ide_init:
     mov a, #ide_head
     mov r3, #0
     mov r2, #10100000b
     acall ide_wr_8 ;select the master device
     mov a, #ide_status
     acall ide_rd_8
     ; uncomment these if the code hangs, waiting forever for
     ; the drive to respond. This will at least let you see
     ; where it's waiting, and the value of the status register
     ;mov a, #'*'
     ;lcall cout
     ;mov a, r2
     ;lcall phex
     mov a, r2
     ;should probably check for a timeout here
     jnb acc.6, ide_init ;wait for RDY bit to be set
     jb acc.7, ide_init ;wait for BSY bit to be clear
    
     ; uncomment this section if you have a very old hard drive
     ; (probably win3.1 or early win95 era) that does not even
     ; allow LBA accesses until these CHS parameters are set up
     ;mov a, #ide_head
     ;mov r2, #10101111b
     ;acall ide_wr_8 ;what should this config parm be?
     ;mov a, #ide_sec_cnt
     ;mov r2, #64
     ;acall ide_wr_8 ;what should this config parm be?
     ;mov a, #ide_command
     ;mov r2, #ide_cmd_init
     ;acall ide_wr_8 ;do init parameters command
     ;acall ide_wait_not_busy
     ;mov a, #ide_command
     ret
    
    
    
    ; IDE Status Register:
    ; bit 7: Busy 1=busy, 0=not busy
    ; bit 6: Ready 1=ready for command, 0=not ready yet
    ; bit 5: DF 1=fault occured inside drive
    ; bit 4: DSC 1=seek complete
    ; bit 3: DRQ 1=data request ready, 0=not ready to xfer yet
    ; bit 2: CORR 1=correctable error occured
    ; bit 1: IDX vendor specific
    ; bit 0: ERR 1=error occured
    
    
    ;------------------------------------------------------------------
    ; Not quite as low, low level I/O. These routines talk to the drive,
    ; using the low level I/O. Normally a main program should not call
    ; directly to these.
    
     ;Read a block of 512 bytes (one sector) from the drive
     ;and store it in memory @ DPTR
    read_data:
     mov r5, #0
    rdblk2: push dph
     push dpl
     mov a, #ide_data
     acall ide_rd_16
     pop dpl
     pop dph
     mov a, r2
     movx @dptr, a
     inc dptr
     mov a, r3
     movx @dptr, a
     inc dptr
     djnz r5, rdblk2
     ret
    
    
     ;Write a block of 512 bytes (at DPTR) to the drive
    write_data:
     mov r5, #0
    wrblk2: 
     movx a, @dptr
     mov r2, a
     inc dptr
     movx a, @dptr
     mov r3, a
     inc dptr
     push dph
     push dpl
     mov a, #ide_data
     acall ide_wr_16
     pop dpl
     pop dph
     djnz r5, wrblk2
     ret
    
    
     ;write the logical block address to the drive's registers
    wr_lba:
     mov a, lba+3
     anl a, #0x0F
     orl a, #0xE0
     mov r2, a
     mov a, #ide_head
     acall ide_wr_8
     mov a, #ide_cyl_msb
     mov r2, lba+2
     acall ide_wr_8
     mov a, #ide_cyl_lsb
     mov r2, lba+1
     acall ide_wr_8
     mov a, #ide_sector
     mov r2, lba+0
     acall ide_wr_8
     mov a, #ide_sec_cnt
     mov r2, #1
     acall ide_wr_8
     ret
    
    
    
    ide_wait_not_busy:
     mov a, #ide_status ;wait for RDY bit to be set
     acall ide_rd_8
     ; uncomment these if the code hangs, waiting forever for
     ; the drive to respond. This will at least let you see
     ; where it's waiting, and the value of the status register
     ;mov a, #'.'
     ;lcall cout
     ;mov a, r2
     ;lcall phex
     mov a, r2
     ;should probably check for a timeout here
     jb acc.7, ide_wait_not_busy
     ret
    
    
    ide_wait_ready:
     mov a, #ide_status ;wait for RDY bit to be set
     acall ide_rd_8
     ; uncomment these if the code hangs, waiting forever for
     ; the drive to respond. This will at least let you see
     ; where it's waiting, and the value of the status register
     ;mov a, #','
     ;lcall cout
     ;mov a, r2
     ;lcall phex
     mov a, r2
     ;should probably check for a timeout here
     jnb acc.6, ide_wait_ready
     jb acc.7, ide_wait_ready
     ret
    
    
    
    
     ;Wait for the drive to be ready to transfer data.
     ;Returns the drive's status in Acc
    ide_wait_drq:
     mov a, #ide_status ;wait for DRQ bit to be set
     acall ide_rd_8
     ; uncomment these if the code hangs, waiting forever for
     ; the drive to respond. This will at least let you see
     ; where it's waiting, and the value of the status register
     ;mov a, #'_'
     ;lcall cout
     ;mov a, r2
     ;lcall phex
     mov a, r2
     ;should probably check for a timeout here
     jb acc.7, ide_wait_drq ;wait for BSY to be clear
     jnb acc.3, ide_wait_drq ;wait for DRQ to be set
     ret
    
    
    ;------------------------------------------------------------------
    ; Low Level I/O to the drive. These are the routines that talk
    ; directly to the drive, via the 8255 chip. Normally a main
    ; program would not call to these.
    
     ;Do a read bus cycle to the drive, using the 8255.
     ;input acc = ide regsiter address
     ;output r2 = lower byte read from ide drive
     ;output r3 = upper byte read from ide drive
     ;dptr is changed
    ide_rd_16:
     mov dptr, #ide_8255_ctl
     movx @dptr, a ;drive address onto control lines
     orl a, #ide_rd_line 
     movx @dptr, a ;assert read pin
     mov dptr, #ide_8255_msb
     movx a, @dptr ;read the upper byte
     mov r3, a
     mov dptr, #ide_8255_lsb
     movx a, @dptr ;read the lower byte
     mov r2, a
     mov dptr, #ide_8255_ctl
     clr a
     movx @dptr, a ;deassert all control pins
     ret
    
    ide_rd_8:
     mov dptr, #ide_8255_ctl
     movx @dptr, a ;drive address onto control lines
     orl a, #ide_rd_line 
     movx @dptr, a ;assert read pin
     mov dptr, #ide_8255_lsb
     movx a, @dptr ;read the lower byte
     mov r2, a
     mov dptr, #ide_8255_ctl
     clr a
     movx @dptr, a ;deassert all control pins
     ret
    
    
    
     ;Do a write bus cycle to the drive, via the 8255
     ;input acc = ide register address
     ;input r2 = lsb to write
     ;input r3 = msb to write
     ;dptr is changed
    ide_wr_16:
     mov r4, a ;address in r4
     mov dptr, #cfg_8255
     mov a, #wr_ide_8255
     movx @dptr, a ;config 8255 chip, write mode
     mov dptr, #ide_8255_lsb
     mov a, r2
     movx @dptr, a ;drive lower lines with lsb (r2)
     mov dptr, #ide_8255_msb
     mov a, r3
     movx @dptr, a ;drive upper lines with msb (r3)
     mov dptr, #ide_8255_ctl
     mov a, r4
     movx @dptr, a ;drive address onto control lines
     orl a, #ide_wr_line 
     movx @dptr, a ;assert write pin
     nop
     mov a, r4
     movx @dptr, a ;deassert write pin
     mov dptr, #cfg_8255
     mov a, #rd_ide_8255
     movx @dptr, a ;config 8255 chip, read mode
     ret
    
    ide_wr_8:
     mov r4, a ;address in r4
     mov dptr, #cfg_8255
     mov a, #wr_ide_8255
     movx @dptr, a ;config 8255 chip, write mode
     mov dptr, #ide_8255_lsb
     mov a, r2
     movx @dptr, a ;drive lower lines with lsb (r2)
     mov dptr, #ide_8255_ctl
     mov a, r4
     movx @dptr, a ;drive address onto control lines
     orl a, #ide_wr_line 
     movx @dptr, a ;assert write pin
     nop
     mov a, r4
     movx @dptr, a ;deassert write pin
     mov dptr, #cfg_8255
     mov a, #rd_ide_8255
     movx @dptr, a ;config 8255 chip, read mode
     ret
    
    
    
    
     ;do a hard reset on the drive, by pulsing its reset pin.
     ;this should usually be followed with a call to "ide_init".
    ide_hard_reset:
     mov dptr, #cfg_8255
     mov a, #rd_ide_8255
     movx @dptr, a ;config 8255 chip, read mode
     mov dptr, #ide_8255_ctl
     mov a, #ide_rst_line
     movx @dptr, a ;hard reset the disk drive
     mov r2, #40
     mov r3, #0
    rst_dly:djnz r3, rst_dly
     djnz r2, rst_dly ;delay (reset pulse width)
     clr a
     movx @dptr, a ;no ide control lines asserted
     ret
    
    
    
    
    ;------------------------------------------------------------------
    ; Some additional serial I/O routines not available in PAULMON
    
    
     ;print a 16 bit number, located at DPTR
    print_parm:
     movx a, @dptr
     push acc
     inc dptr
     movx a, @dptr
     mov dph, a
     pop dpl
     ljmp pint16u
    
    
     ;print a string, no more than R0 words long
     ;the IDE string are byte swapped. Fetch each
     ;word and swap so the names print correctly
    print_name:
     movx a, @dptr
     mov r2, a
     inc dptr
     movx a, @dptr
     inc dptr
     jz pn_end
     lcall cout
     mov a, r2
     jz pn_end
     lcall cout
     djnz r0, print_name
    pn_end: ret
    
    
    
     ;get a 32 bit input, in hex
    ghex32_lba:
     mov r2, #8
     mov r3, #0
     mov r4, #0
     mov r5, #0
     mov r6, #0
    gh32c: lcall cin_filter
     lcall upper
     cjne a, #27, gh32d
     setb c
     ret
    gh32d: cjne a, #8, gh32f
     sjmp gh32k
    gh32f: cjne a, #127, gh32g
    gh32k: cjne r2, #8, gh32e
     sjmp gh32c
    gh32e: lcall cout
     mov r0, #4
    gh32yy: clr c
     mov a, r6
     rrc a
     mov r6, a
     mov a, r5
     rrc a
     mov r5, a
     mov a, r4
     rrc a
     mov r4, a
     mov a, r3
     rrc a
     mov r3, a
     djnz r0, gh32yy
     inc r2
     sjmp gh32c
    gh32g: cjne a, #13, gh32i
     clr c
     ret
    gh32i: mov r7, a
     acall asc2hex
     jc gh32c
     xch a, r7
     lcall cout
     mov a, r7
     swap a
     mov r7, a
     mov r0, #4
    gh32j: mov a, r7
     rlc a
     mov r7, a
     mov a, r3
     rlc a
     mov r3, a
     mov a, r4
     rlc a
     mov r4, a
     mov a, r5
     rlc a
     mov r5, a
     mov a, r6
     rlc a
     mov r6, a
     djnz r0, gh32j
     djnz r2, gh32c
     clr c
     ret
    
    
    
     ;carry set if invalid input
    asc2hex:
     clr c
     add a, #208
     jnc hex_not
     add a, #246
     jc hex_maybe
     add a, #10
     clr c
     ret
    hex_maybe:
     add a, #249
     jnc hex_not
     add a, #250
     jc hex_not
     add a, #16
     clr c
     ret
    hex_not:setb c
     ret
    
    
     ;print a hexdump of the data in the 512 byte buffer
    hexdump:
     lcall newline
     mov r2, #32 ;print 32 lines
     mov dptr, #buffer
    hd1: mov a, dph
     mov r5, a
     clr c
     subb a, #buffer >> 8
     lcall phex ;print address, starting at zero
     mov a, dpl
     mov r4, a
     lcall phex
     mov a, #':'
     lcall cout
     acall space
     mov r3, #16 ;print 16 hex bytes per line
    hd2: movx a, @dptr
     inc dptr
     lcall phex ;print each byte in hex
     acall space
     djnz r3, hd2
     acall space
     acall space
     acall space
     mov dpl, r4
     mov dph, r5
     mov r3, #16 ;print 16 ascii bytes per line
    hd3: movx a, @dptr
     inc dptr
     anl a, #01111111b ;only 7 bits for ascii
     cjne a, #127, hd3b
     clr a ;avoid 127/255 (delete/rubout) char
    hd3b: add a, #224
     jc hd3c
     clr a ;avoid control characters
    hd3c: add a, #32
     lcall cout
     djnz r3, hd3
     lcall newline
     djnz r2, hd1
     lcall newline
     ret
    
    space: mov a, #' '
     ljmp cout

     

     

         Even though you may not read it, you can get a gist how how to use. It is based on 8051(Atmel 89C2051) MCU with a 82C55 chip for latching .

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • iexpress
    iexpress over 11 years ago in reply to clem57

    Thanks, will give that a try issuing command 0x91 after turning on the drive.

     

    It is an 80 gb Western Digital, and I set it aside for a couple days.

     

    originally, this is what I was doing:

    1) Select CS0, unselect CS1

    2) Send 0xE0 out DataPort

    3) Set Addres to register 6

    4) select write line, then unselect

    5) send 0xEC out DataPort

    6) set address to register 7

    7) select write line, then unselect write line

    8) set register address to 0x00 For register 0

    10) set DataPort as input

    11) select read line, and get data on the dataport.

    12) unselect read line. Repeating the process 256 times to get device info.

     

    initially this was only giving me the very first byte entry and I couldn't figure out how to increment the buffer address inside the hard drive. So if I enter the 0x91 command as you specified, it should work in LBA mode.

     

    I haven't gotten that far yet, but even trying to load in LBA 1 or 2 as a test, reading back the sectors gave me one byte, and the bytes were the same value regardless of the selected LBA. Thanks again, I'll go ahead and wire up the drive again to try sending command 0x91 to the unit.

     

    Strangely, the ATmega328p MCU also only recognizes one command after power on when trying to get into programming mode, which is a Programming Enable 0xAC 53 00 00. All other commands are ignored when the reset pin is low while data entry is fed into the SPI pins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago

    Originally I tried to access the hard drive using Cylinder/Head/Sector (CHS) addressing, and it would not work properly. All of these early attempts were with a Western Digital 1.2 gig drive. I could read the first sector, C=0, S=0, H=0, also known as the Master Boot Record (MBR), but reading from other parts of the drive would not work. After much frustration, I discovered that the drive wanted to receive the Initialize Drive Parameters (0x91) command. I didn't find much documentation about this command on-line. I deleted all the code I wrote for CHS (except for printing info from the drive ID command).

     

    Sounds like that may be your problem!

     

    Cheers,

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • muffenme
    muffenme over 11 years ago in reply to iexpress

    Did you read this An 8-bit IDE interface @ Retroleum

    Here some C program for PC Simplix - ide.c

    Finally I think someone made something for Arduino board this is it Paul's 8051 Code Library, IDE Hard Drive Interface

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>