Arduino
  • Products & Partners
  • More
Arduino
Blog IoT Christmas Ornaments - Everything but the Electronics
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 15 Dec 2014 5:54 PM Date Created
  • Views 2917 views
  • Likes 6 likes
  • Comments 7 comments
  • iot_holidaylights
  • 3d_printing
  • integrated_led_control
Related
Recommended

IoT Christmas Ornaments - Everything but the Electronics

e14 Contributor
e14 Contributor
15 Dec 2014

I seem to be a bit behind the curve compared to other testers, my hardware hasn't shown up quite yet (tracking predicts it'll show up today, so maybe I can get it unboxed and plugged together this evening - we shall see). But that doesn't mean I've been sitting back doing nothing. There's more to my project than just electronics after all!

 

After playing with the necessary 3D design, and printing one unfortunate failure, I realized I was taking the wrong approach to wrapping a flat string of LEDs around a spherical object. A spiral pattern just wasn't going to work given the LED strip's inability to bend along its thin edge. Being the intrepid rapid prototyper that I am, I mulled it over, and decided to give longitudinal mounting a try instead.

 

Here's attempt number two, printing away:

image

 

With a little bit of math, and a little more 3D modeling, I came up with a working design. Each channel is essentially made up of 11mm wide strips of a 40mm radius sphere incised into a 42mm radius sphere, that channel is then rotated 72 degrees around the center line of the sphere, and the process is repeated until there are a total of five channels. That may sound a little confusing, but the practical upshot of this you get five channels that will hold the LED strip and that are sized specifically to fit two segments of the strip (i.e. six LEDs per strip, and 30 LEDs per ornament).

 

My hope is this will give a relatively even lighting effect on the final ornament. But we will see.

 

image

You can see that in addition to the incised channels, the inner sphere has five raised nubs at points 45 degrees up the arc of the sphere. These will provide additional clearance between the inner sphere and the outer shell of the ornament to make for easier mounting of the LED strips and wiring.

image

Each 6 LED segment will have to be wired to its neighbors, and then each ornament will have two sets of wires coming out of it. One to hook to the supply (or the previous ornament) and one to hook to the next ornament. The holes in the top and bottom of the core will be useful for wire routing to keep the surface clear of stray wires.

 

One thing I discovered, but wasn't surprised about, is that the sticky 3M backing on the LED strips seems to be all but worthless. If there's anything it will stick effectively to, PLA plastic isn't it. I'll probably end up having to tack the strips down with hot glue or odorless silicon or something.

image

The only thing missing from the ornament now is the outer shroud. It's mostly designed, but not quite finished, and will be printed in nylon for a nice white diffuser layer that has a nice smooth texture to it.

 

Now... if only my hardware would show up I could put it through its paces and make a glowing ball...

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1 +1
    I did, briefly, but quickly came to the conclusion that mounting these strips to the interior surface of a sphere would be needlessly complex. The pictured print is only the core of the unit, though. There…
  • mcb1
    mcb1 over 11 years ago in reply to e14 Contributor +1
    Okay A two piece ornament ...you guys with 3D printers have all the fun. Mark
  • Problemchild
    Problemchild over 11 years ago +1
    It looks more like one of those Grenades Princess Leia had. Just add a slide switch to start that gives off a high pitched whine
  • pmohan
    pmohan over 11 years ago

    3D printed ornaments image  cool..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago

    Very nice result! Looking forward to the thing lighting up image

     

    My parts arrived today, time to start experimenting!

     

    Frederick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<