Arduino
  • Products & Partners
  • More
Arduino
Blog Meet Omnuino - A Smarter Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 27 Dec 2014 12:13 AM Date Created
  • Views 819 views
  • Likes 1 like
  • Comments 4 comments
  • omnuino
  • smart
  • arduino
  • home
Related
Recommended

Meet Omnuino - A Smarter Arduino

e14 Contributor
e14 Contributor
27 Dec 2014

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
Okay, I confess right up front, this is a bit of a spam, but I think you will forgive me when you see it.  We (Original Design & Development) just launched Omnuino on Kickstarter.  With all the humility and reserve this retiring Brit has in spades, I think it's a pretty cool addition to the Arduino multiverse.  I'll let the picture and Kickstarter tell the story...

  • Sign in to reply
  • cstanton
    cstanton over 11 years ago

    We're happy to support electronics developers and their projects going into production image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to e14 Contributor

    That diagram would be useful. Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gadget.iom

    Thanks for the vote of confidence that I wasn't presuming too much in posting this.

     

    All the usual Arduino pin headers are available on the PCB.  Yes, a few are used for the onboard accessories (mostly shared SPI) but there are still a ton available.  The handheld case has room for wiring directly to the pins but no room for a shield.  The wall-mount case has room for a slim shield but is really designed to go on a wall or panel and then you can keep stacking shields back into the panel and still keep a slim profile on the front.  One minor compromise though is that the central 6 pin ICSP programming header usually found on the Mega is not populated so as to make room for the LiPo battery.  It is copied to the edge of the board so the ICSP is still available (or just use the normal USB) but any sheild that expects those six pins (not may do) will need a bit of hardwiring.  Or, if you don't need the battery you could solder that connector on.  When time allows I'll post a pin diagram on our website.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago

    Thanks for posting that. I wouldn't say it's spammy owing to it's Arduino nature.

     

    One point that doesn't seem to be covered is GPIO.The mega has over 50 Digital and 16 Analogue, are you using them all? or is there a header that we can hook up to?