Arduino
  • Products
  • More
Arduino
Blog Need some help with arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 10 Jul 2015 5:00 PM Date Created
  • Views 1586 views
  • Likes 0 likes
  • Comments 8 comments
Related
Recommended

Need some help with arduino

e14 Contributor
e14 Contributor
10 Jul 2015

Hellow guys, after watching tutorials and videos, about creating a new arduino coutdown with buttons, i found nothing so i can use, i am very new at this, all i want is a tutorial or something similar


i need something that has a button so players can hold for a amount of seconds so that they can wait to respawn.

At the same time i need it to have a screen with an amount of tickets left for the team, each player when respawn takes 1 ticket. 

Also need 2 buttons so we can increase/decrease  the amount of seconds to hold for player to respawn

and the numbers of tickets

Also need to have sound alarm ( pc speaker or same ) that sounds a alarm when tickets are down to 0

 

 

Button A - this is what players hold so that they can respawn ( hold for X amount of time ) Example : 5 secs hold - you can see a bar loading until you are alive again

 

Button 1 - increase time that players need to hold so that they can respawn / increase number of total tickets when u  are setting up  match

 

Button 2 - decrease time that players need to hold so that they can respawn / descrease number of total tickets when u are setting up match

 

Screen - when in menu setting the game  - select amount tickets  more/less  - select amount secconds so players have to hold so respawn / at the same time ticket needs to drop by 1 , each  respawn ( revive ) - select sound on/ off   - when tickets get to 0 , screen shows NO RESPAWN LEFT , GOOD LUCK  and reset to menu

 

Sound - Alarma sounds when number of tickets get to 0 for 5 seconds and off

 

 

Thank you very much hope this helps and someone that knows how to do or even point me out see this. THANK YOU AGAIN VERY MUCH

if you can point out to someone that hast these skills, i would like to chat with that person. Thank you

  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    you need to start by simply creating programs that just read buttons and let you know if they are detected, this involves simple input statements then look at display drivers (Google "Night Rider and Arduino…
  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Thank you guys for all answers, i am actually learning arduino, i managed to learn button states and now im rolling to button to lcd prints , Thank you all again
  • clem57
    clem57 over 11 years ago in reply to e14 Contributor +1
    How are your project(s) going. I know motivation can be hard if you get lost. But keep trying. It is the mistakes we make that we learn the most from. C
  • clem57
    clem57 over 11 years ago in reply to e14 Contributor

    How are your project(s) going. I know motivation can be hard if you get lost. But keep trying. It is the mistakes we make that we learn the most from.

    C

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    I ended up following this tutorial, is it possible to add a button to this sketch, that after 3 seconds of pushing it will drop by 1 the number from the display ? , and when the number raches 0 , a small speaker goes like a alarm?.

     

    mby a beep each second the button is pushed and after last beep, a difrent tone indicating player can leave

    Example : set button to 3 seconds, after 3rd beep when pushed , a different beep , the number on the display drops by one and player can go

    2 Digit 7 Segment Display with Buttons using Arduino

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Thank you guys for all answers, i am actually learning arduino, i managed to learn button states and now im rolling to button to lcd prints , Thank you all again

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 11 years ago in reply to alacosta

    Hi alacosta - this is being answered as the new question you posted.

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • alacosta
    alacosta over 11 years ago

    not sure if this the right place to ask this question

     

    Hope you can help / advise me. I have an Arduino program reading 5 different temperature settings as a csv file   this is set as csv to be monitored in a Windows PC program.

     

    set as :-

     

    // prints values to serial port  / PC Graphics Program
     
              Serial.print (water);
              Serial.print (",");
              Serial.print (WavMinn);
              Serial.print (",");
              Serial.print (panel);
              Serial.print (",");
              Serial.print (PavMinn);
              Serial.print (",");
              Serial.print (air);
              Serial.println ("");

    I am new to App inventor , have mastered Bluetooth connection but now at a total loss of how to display  this data  on my phone (Android ) the more I try to find a way the more I get confused !!!

     

    what I would like is to be displayed as :-

     

    Solar Temperature  Monitor

    Label    Data 

    Label    Data

    Label    Data

    Label    Data

    Label    Data

     

    Any advice on the App Inventor  reading a csv  data, setup or sample program would be greatly appreciated

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>