Arduino
  • Products & Partners
  • More
Arduino
Blog Notes on Stepper Motors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 6 Jan 2014 7:34 PM Date Created
  • Views 1382 views
  • Likes 0 likes
  • Comments 1 comment
Related
Recommended

Notes on Stepper Motors

Workshopshed
Workshopshed
6 Jan 2014

For small robotic and other projects you can pick up small 28BYJ-48 stepper motors and gearbox with ULN2003ULN2003 driver boards quite cheaply. These motors are used in comercial projects like washing machines etc hence are made in very large quantities and are cheap. The gearbox means that they have a decent torque and can move a small robot ok. Because these have a gearbox I'll need to include a "home" sensor to work out when they are pointing at the top as my application I need to know the absolute position of the motor. I'm hoping to use a slotted opto sensorslotted opto sensor to do this and have made some disks to attach to the motor gears and will add a stripe to these so that I can detect an abosolute position.

 

image

I initially had issues with the standard Arduino stepper library but Yuan Liu @LiuYuanster mentioned on twitter that the default Arduino Stepper library only works with cross-wire pin sequence e.g. 8,10,9,11 and sent me the following link for information about Small Steppers. I tried the cross wired approach and that worked just fine with the motors turning in both directions.

 

The small steppers article had a link to an alternative library AccelStepper which appears to have all of the features I need. It already has a "setposition" which I'll need when I wire up the optical sensor to detect the home position. I found another potential library via the Arduino playground called CustomStepper. This library works in a similar manner to the AccelStepper but has less features, I may need to switch to this if I run into memory issues with the AccelStepper library or even cut into that.

 

Workshopshed: stepper motor

  • Sign in to reply
  • Workshopshed
    Workshopshed over 12 years ago

    I've had a bit of a play with the AccelStepper library and note that it also needs the cross wire sequence 8,10,9,11. I did not find it too straight forward to use this library so I might try the CustomStepper instead.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    Here's my experiments with the opto switch and homing the motors