Arduino
  • Products & Partners
  • More
Arduino
Blog QLab MIDI Controller - The Build
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gadget.iom
  • Date Created: 10 Dec 2014 9:08 PM Date Created
  • Views 5474 views
  • Likes 0 likes
  • Comments 12 comments
  • qlab
  • fritzing
  • midi
Related
Recommended

QLab MIDI Controller - The Build

gadget.iom
gadget.iom
10 Dec 2014

This is part II of a three part post.

Please read Part I QLab Midi Controller for an introduction to the project.

 

Parts Required

1x Teensy 3.1 - https://www.pjrc.com/store/teensy31.html

1x 60mm Illuminated Arcade Button - http://www.arcadeworlduk.com/products/High-Profile-60mm-Arcade-Button.html

1x Rectangular Arcade Button - http://www.arcadeworlduk.com/products/Rectangular-Illuminated-Arcade-Button.html

1x Triangular Arcade Button - http://www.arcadeworlduk.com/products/Triangular-Arcade-Button.html

5x 5V Wedge Base LEDs - http://www.arcadeworlduk.com/products/awuk-5v-10mm-wedge-base-led.html

1x Hammond Instrument Enclosure - http://uk.farnell.com/hammond/1456fg4bkbu/enclosure-aluminium-instrument/dp/1415246

1x USB A TO MINI B PLUG - http://uk.farnell.com/bulgin/px0441-2m00/cable-usb-a-plug-to-usb-mini-b/dp/1229677

1x USB B RECEPTACLE (PANEL) - http://uk.farnell.com/bulgin/px0443/connector-usb-b-receptacle-panel/dp/1229685

1x Sacrificial Micro-USB cable

 

Schematic

The wiring for the controller is very simple. Internal pull-ups negate the need to resistors on the switches. I’ve put together a very rough schematic in Fritzing. Please let me know if you have any questions, comments or suggestions.

image

 

Operation

 

When powered up all three of the buttons will illuminate.

 

The Go button is intended to fire the currently selected cue. To do this it sends a MIDI note to the computer when the button is pressed, and turns the note off when the button is released. During this time the go button will blink 3 times.

 

The next button will send a different note to the computer when pressed. The LED on this button will extinguish while the button is pressed.

 

The Stop button has two functions. QLab will fade all active cues when the ‘Panic’ button is pressed. The time of this fade can be modified in the preferences. If the button is pressed a second time the track will stop immediately. To reflect this, the first press of the stop button will cause the button to flash for three seconds. the second press will cancel the flash and re-illuminate the button.

 

 

 

Construction

The enclosure front was cut to accommodate the three buttons, the rear face was cut to accept the panel mounted USB receptacle (apologies for the lack of photos). Each of the Buttons was installed and four cables were run to each of them. The Teensy and wire ends were then mounted onto a piece of strip-board

imageimageimage

 

The inclusion of the specific Bulgin connectors are purely optional, I chose them because the USB cable can be ‘locked’ in place, and a standard Mini USB can also be accepted.

 

 

The QLab MIDI Controller Arduino code will follow in part III.

This project is still work in progress. Comments, questions, and suggestions are welcome.

  • Sign in to reply
  • gadget.iom
    gadget.iom over 11 years ago in reply to e14 Contributor

    Hi robduro

     

    Good to hear somebody else is interested in the project. Version 1 has been built and tested. It haa complayed two show runs. Another version with additional features is in the pipeline.

     

    Would be happy to assist you. What would you like photos of?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    great work! this is what I was looking for. Do you have pics of the finished project and/or a more detailed diagram? Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<