Arduino
  • Products & Partners
  • More
Arduino
Blog Simple Threading and Serial User Interface library for the Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 9 Apr 2014 4:24 AM Date Created
  • Views 3588 views
  • Likes 2 likes
  • Comments 7 comments
  • thread
  • arduino
  • threading
  • ui
Related
Recommended

Simple Threading and Serial User Interface library for the Arduino

e14 Contributor
e14 Contributor
9 Apr 2014

One of my first big micro-controller projects was called the Neonatal Closed Loop Oxygen System. When babies are born prematurely, they have to be fed very specific amounts of oxygen. Too little oxygen and they suffocate, too much oxygen and they can die from oxygen toxicity. Current methods are not advanced, essentially involving a nurse adjusting the oxygen levels manually. The goal of the project was to develop an automatic system.

 

We had to prevent this little guy from getting oxygen poisoning

450px-Premature_infant_with_ventilator.jpg

The project had the following design requirements:

  • Check oxygen levels from a UART input.
  • Process oxygen levels and respond appropriately (long calculation time).
  • Adjust valves electronically to correct oxygen levels.

 

The project also had to do the following:

  • implement a simple user interface with a few buttons and an LCD screen
  • Be able to sound an alarm for a set amount of time if there were issues.
  • Export periodic debugging data to improve the product.


All of these things had to happen simultaneously, and it was critical that nothing prevented the microcontroller from adjusting the oxygen. It would be no good if the Alarm sounding caused all other functions to cease!


I was in charge a few aspects of the project, but one of the main ones was developing a user interface and threading structure. Essentially my problem was: how do you do all of these things at once? I'm not going to go over the solution I used (it was nasty and difficult to understand), but about a year later I discovered the protothreading library written by Adam Dunkels. This made threading significantly easier, but it was still a pain -- you had to declare each thread object individually, it seemed almost impossible for functions to use multiple threads (as variables have to be static), and it still felt way too much like micro-controller programming (and not enough like Arduino programming!)

 

Why do you need a user interface?

Maybe you aren't trying to save a baby's life, maybe you are trying to figure out how to control a robot like the line follower below. You have to take user input, output debug data, take line readings, and control each motor separately. That's a lot of things for a little Arduino to do!


Line follower robot using an the ArduinoArduino and the  Motor Control ShieldMotor Control Shield

800px-Line_follower.jpg

 

So, a few months ago I started writing a threading and user interfacing library called usertools. Usertools contains the following files:

  • threading.h -- basic and lightweight threading. threading_led_example2 is only 6.8 KB of program memory and 240bytes of RAM!
  • ui.h -- lightweight and full featured user interface. ui_led_example3 and ui_led_example4 take up only about 11.5KB of program space and 320 bytes of RAM to implement a full featured user interface. This is the focus of this post.
  • errorhandling.h -- An error handling and debugging library. This will be the subject of a later post.

To demonstrate the usefulness of the library, this post is going to focus on ui_led_example4 -- as this example demonstrates most of the benefits of the user interface library. Before I go into that, lets overview what has to happen to create a low-memory threading and user interface

 

  • You have to store everything you can into Program Memory (Flash). This is done through the setup functions. For more information on the internals, see my blog post.
  • You want to be able to dynamically create and destroy data. This is done through the pthread class. Also, dynamically allocating and freeing memory is something you are not supposed to do on microcontrollers, so I had to create a class to do it. See my blog post about it.
  • You have to expose the threads and then "handle" them. In other words you have to have a way to know if they are active, deactivated, or should be killed and do the appropriate thing to them. This is done by expose_threads(...), schedule_thread(thread), and kill_thread(thread). Threads are handled from ui_loop() or thread_loop()
  • You have to monitor the serial data and behave appropriately, allowing the user to schedule threads, kill threads, call functions, and set/get variables. This is all done in ui_loop()

 

Upload the code to your Arduino

 

Get the latest release of usertools library from github. Move the "usertools" folder to your Arduino libraries ([Arduino Folder]/libraries). Start Arduino and go to:

file->Examples->usertools->ui_led_example4


Then upload the code to your Arduino. Open your Serial Terminal (Cntrl + Shift + M) and make sure to set the drop-down boxes in the bottom left to "Both NL & CR" and "57600 Baud".

 

Once you have done that, type the following (each followed by enter):

  • “?” to get info on commands you can type.
  • "v sub_time 500" -- you will see the led's blink much faster (500ms is being taken off both periods)
  • "v sub_time" -- get the value of sub_time in hex
  • "v sub_time 0" -- set it back to 0 (slow blinking)
  • "k led1" -- Kills thread led1. This will make it so that only 1 thread is blinking (blinks at period of 900ms)
  • “k led2” -- everything will be killed (no blinking)
  • “reinit” -- calls the reinit function, everything will be set to default values!

 

Explanation

 

Note: There is full featured documentation for all modules located in the Documentation folder (just open the .pdf files). If anything is confusing you, please reference these documents as they should explain most questions.

 

Declaring our Thread function

 

In this part of the code, we include our usertools library <ui.h> and write our main thread function "blinky_thread". As you can imagine, this thread will cause the LED to blink.

 

At first blinky_thread might look a little odd -- that is an awful lot of code to just blink an LED! The key is in the PT_WAIT_MS call -- this call is what makes the whole thing tick. If you run this program, you will notice that your LED is blinking... weird. Sometimes it's a long period, sometimes it is really short. This is because we have two threads running that are toggling the same LED. Well get to that soon!

 

Keeping track of Threads

 

in this part, we label the index names of our threads, functions and variables (we will give them string names later). This is just so that it is easy to get them and schedule them later in the code.

 

Creating the reinit function (accessible through the terminal)

 

This function will be used in our setup -- but it is also declared such that it can be called from the command line. Take note of the function type: uint8_t thread_function(pthread * pt). All functions or threads must be of this type.

 

Let's go through this function step by step:

  thread *th;

We will use this pointer to access our thread's data later in the function.

 

  TRY(set_thread_innactive(get_thread(LED1)));

  clrerr();

  TRY(set_thread_innactive(get_thread(LED2)));

  clrerr();

Remember that this function will be called by both the setup AND by the user. If it is called by the setup, then we wouldn't need to set these threads innactive. However, if it is called by the user we will need to set them inactive before we can re initialize them.

 

The TRY macro is part of the errorhandling library I wrote to make debugging and error checking easier. For more information, open Documentation/errorhandling.html in your web browser.

 

th = get_thread(LED1);

th->pt.put_input(1000);

th = get_thread(LED2);

th->pt.put_input(900);

These lines retrieve the thread objects and then put a value into their input buffers. This sets one thread to toggle the LED at a 1000ms period, and the other to toggle at a 900 ms period.

 

Note that every protothread implements a dynamically allocated linked list. This means that you can add input and output data to the pthread object and then delete it (with clear_data() or del_input(index)). In addition, when a thread is killed or set innactive, all of it's data is destroyed and reclaimed for future use.

 

  schedule_thread(LED1);

  schedule_thread(LED2);

The threads are finally scheduled, and will be called by the ui_loop at the bottom of the file.

 

Setting everything up

 

During setup is probably one of the most confusing parts of this module. It is very important that you do things in the right order and in the right way. Let's take a look!

 

expose_threads(TH_T(blinky_thread), TH_T(blinky_thread));  // wrap threads in TH_T

This line declares the threads that you are exposing. Once exposed, you can schedule or kill threads through the user interface or through code (as you saw above).

This is the only place that you can expose threads. Every "thread" is really a function of the type uint8_t (*TH_funptr)(pthread *pt) (for the newbee, this is a function pointer object. Your function must take one input pthread* and return uint8_t)

 

Note that all of this is done for you by wrapping each function name with TH_T.

 

expose_threads simultaneously allows you to schedule the thread, as well as kill (or schedule) the thread from the command line. For example, because of the names we are creating below, LED1 can be killed with "k led1" and then rescheduled with "t led1 PERIOD", where period is the blinking period you want (an integer).

 

expose_functions(UI_F(reinit));    // Wrap functions in UI_F

The same concept as expose_threads (except you use UI_F). This allows you to access the function reinit from the command line. Because of our naming scheme below, this function can be called with simply "reinit"

 

Note: Functions that are called from the command line only run once, whereas threads will be called every loop (until they return PT_EXITED or are killed)

 

UI_V(v1, sub_time);              // Variables have to be declared specially. Declare variable names first with UI_V

//UI_V(v2, othervar) -- if you had more variables, continue in this way

expose_variables(UI_VA(v1));     // Then wrap the variable names in UI_VA. Alot of things have to be done to take up

                                 // zero RAM!

 

Exposing variables is a little more involved, and requires you to pre-set a name to each variable, and then expose the names by wrapping them in UI_VA. If you are wondering why this has to be the process, then please see my blog post about it.

 

Because of our naming scheme, we will be able to access this variable from the terminal with the command "v sub" or set it with "v sub VALUE"

 

// The names have to be done similarily to variables

UI_STR(tn1, "led1");

UI_STR(tn2, "led2");

expose_thread_names(tn1, tn2);  // no wrapping required here.

 

UI_STR(fn1, "reinit");

expose_function_names(fn1);

 

UI_STR(vn1, "sub");

expose_variable_names(vn1);

Exposing names is done similarly to variables.

 

Note: if you are not using functions or variables, you have to explicitly declare this with no_functions() and no_variables(). See this in ui_led_example3

 

void setup() {

  pinMode(LEDPIN, OUTPUT); // LED init

  Serial.begin(57600);

 

  Serial.println("\n\n#########################  Start Setup");

  Serial.println(freeMemory());

  // This makes the names actually accessible to the threading module.

  set_thread_names();

  set_function_names();

  set_variable_names();

 

  // this must be called before any threading (except setting names)

  setup_ui(200);  // 200 == the amount of dynamic memory our threads can use.

                  // I recommend at least 100, more if you use alot of strings

 

  // This has two purposes: it initilizes the values during setup, and it can be called

  // by the user to reinitilize the values.

  reinit(NULL); // Note: NULL is only used because the function doesn't actually use it's pthread input.

 

}

 

In our setup function we call the set_NAME_names() to expose the names to the system, and then call setup_ui(200).

 

setup_ui(mem) must be called before anything is done with threading or the user interface (except setting the names). The "200" is the amount of memory we have set asside for dynamic memory. This memory is used for all of our pthread put_input and put_output data. If you are using strings, I recommend using at least 200 bytes. For more information about dynamic reusable memory see my blog post about my ReMem module.

 

 

Call in the loop

Now the only thing left is to call one function during the loop:

void loop() {

  ui_loop();

}

ui_loop takes care of everything for you -- reading the user input, putting into the threads pthread objects so you can get the inputs, and killing threads.

 

Summary

 

As you can imagine, this library took a significant amount of work to complete. It is currently in Beta because it does not have enough testers and is not currently used in any project. I ask the Element14 community to help me with the following:

  • Are you working on an open source project that could use threading and user interface functionality? If you are, please let me know if you would like help implementing this library in your project. I would love to be part of the team!
  • This library needs additional testers, and developers would be much appreciated as well! There are a few features I am planning to implement in the next couple of months, like Signal blocking and a better thread-spawning system. My hope is that this will eventually become a standard Arduino library, and to make that happen I could use other developers!

If you are interested in either of these, please contact me at Garrett@CloudformDesign.com. Together we can make the usertools library fantastic!

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Post has been updated to reflect the most recent revision. Functions and Variables now take up 0 bytes of SRAM, and threads only take up 4!
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    you put the scanning of the IO (Analog or Digital) into the interrupt routine and have it coded very efficiently so no maths or other interpretation of the results, just raw input then the main routine…
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Dear Members as I read your blogs I am daily thankful and amazed. What a gift to be able to create, make, fix. Thankyou to all, Laureen
  • e14 Contributor
    e14 Contributor over 12 years ago

    Dear Members as I read your blogs I am daily thankful and amazed.

    What a gift to be able to create, make, fix.

     

    Thankyou to all,

    Laureen

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Workshopshed

    Hey Andy,

     

    I agree that a lot of the threading operations are not difficult per-say. Really all you need is a bunch of if-else statements so that you can exit the function without blocking. All I have done is create a standard and dynamic (memory) method of blocking and yielding functions on the arduino. Things like alarms are relatively easy to do conventionally, but when you've got a function that needs to call other functions, or has over 10 blocks that need to be yeilded -- it can be helpful to have a library handle that for you.

     

    Take the LCD screen -- it requires quite a long time write all of it's data to the screen. The protothread library makes this easier to implement and understand (using the PT_WAIT_MS macro). That is the purpose of this library. Even an I2C LCD will require delays for the I2C functions -- sometimes as much as tens of milliseconds.

     

    For long calculations you could do part of the calculation and then just do a PT_YIELD function. This would ensure that it didn't block too much.

     

    For your project I would point out that this library is essentially intended to help people make simple non-blocking functions with an easy to understand and standard process flow. It might be perfect for your project then!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to Workshopshed

    Its all about isolation of processes, scale and speed image

     

    In this case your using a little more memory but the principles are the same and it works very effectively

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 12 years ago in reply to Robert Peter Oakes

    Yes interrupt handlers should be kept small and fast.

    I've successfully used that double buffer technique to decouple a slow process although that was in a database system not a microcontroller.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    you put the scanning of the IO (Analog or Digital) into the interrupt routine and have it coded very efficiently so no maths or other interpretation of the results, just raw input

     

    then the main routine that can be interrupted without affect can simply monitor the variables managed by the IO interrupt to make decisions and perform maths functions to its hearts content

     

    A semaphore system could be used to notify the routines when critical calculations are under-way to inhibit the interrupt from changing values part way through use. Or use a double buffer where the interrupt updates only one buffer and the main routine disables interrupts only long enough to copy the buffer. This would eliminate the race hazard altogether

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>