Arduino
  • Products & Partners
  • More
Arduino
Blog The MEGA_Stick
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: R_Phoenix
  • Date Created: 20 Jan 2011 1:10 AM Date Created
  • Views 1627 views
  • Likes 5 likes
  • Comments 10 comments
  • open-source
  • avr
  • robots
  • prototyping
  • arduino
  • atmel
Related
Recommended

The MEGA_Stick

R_Phoenix
R_Phoenix
20 Jan 2011
My Issue:
Needing an Arduino that is both small in size and “portable”, meaning that it can be used in several different projects.
The Arduino Mini-Pro (to name a few) answers this issue on a smaller scale but I was looking for something in the 2560 size so I developed my own.
 
My Solution:
The MEGA_Stick
image
 
The MEGA_Stick allows me to simply unplug the system from one project and plug it into another.
Two unique things about the MEGA_Stick; all 100 pins are available to the user allowing advanced programmers to utilize the full capacity
of the ATMEGA 2560 chip and the addition of a on board battery backed up Real Time Clock.
This can be turned on or off via a solder jumper (note picture is missing the 2 pull ups).
image
This might be old news to some, but while developing this board I found that Digi pins 45 and 46 can also be used as PWM pins.
Pin 44 should be one as well but it is not yet in the Arduino boot loader.
image
Currently I use the MEGA_Stick for my Phoenix Monitor System, which monitors the fluid levels of up to 4 different tanks.
As you can see in the picture I have the main board with a dual footprint. This board can use the Pro-Mini, or my MEGA_Stick,
depending on the features requested like Automatic water fill, Bay heating, or controlling other outside devices. The info can then be
displayed on a veriety of medium. There is lots of room for expanding on this system. Note that the female headers aren’t soldered in yet.
image
 
Near future plans for the MEGA_Stick is to develop a board for my AeroQuads.
This board also would be dual footprint for multiple types of brains so I can use the same main board in different Quad setups.
At least that’s the plan as I get time to build it.
 
For my use the MEGA_Stick simply makes the Arduino MEGA more portable as well as a more permanent solution in one package.
The biggest issue right now is the cost to build considering the prices of the ATMEGA chip in low quantity.
 
2/21/2012 UPDATE
The MEGA Stick is no longer in production and is being replaced with the even smaller MEGA STICK II
image
The board measures 1"x2.5" and is better suited for embedded applications. The FTDI and RTC is now off board making it a bit more affordable to replace if something goes wrong.
It will also require a regulated 5v supply as the the regulator has also been removed.
 
I will notify when production starts.
  • Sign in to reply
  • billabott
    billabott over 14 years ago

    That is a very attractive board design you have there.

    As a shiney new student of PCB layout, I have a "dumb" question.  Would it not be better for the manufacturer to package this digital processing capacity in a PDIP and just socket/solder that into your application board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • BitHead
    BitHead over 15 years ago

    My first thoughts?  "Holy Moly Bit Man!"

    And then my brain  strained to think of an app worthy of all that I/O.

    For some reason, "A centipede that..." started the next thought.

    Thanks for sharing!  ( And raising the PCB layout bar. image

      )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • R_Phoenix
    R_Phoenix over 15 years ago in reply to sciguy14

    Thanks!

     

    Jeremy Blum wrote:

     

     

    This is really awesome!  Great work - will you be making the pcb/cad files available for this?

     

    Probably the schematic once it is cleaned up a bit - looks like chicken scratchings at the moment image but the cad files are in Pad2Pad, not eagle. It's basically the Arduino Mega reconfigured. I did however reverses engineer it so I understood what everything was and why it was there and what I could safely take out. I do have extra boards as I order them in quanity to keep the cost down.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tronixstuff
    tronixstuff over 15 years ago

    Great work! You could really have a marketable product there. Congratulations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago

    This is really awesome!  Great work - will you be making the pcb/cad files available for this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<