Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum PIR
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 415 subscribers
  • Views 1398 views
  • Users 0 members are here
Related

PIR

lanzrye
lanzrye over 7 years ago

is it possible that the PIR motion sensor only detects a human only?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 7 years ago +4
    Hi Lanz, Unfortunately the design of the basic PIR can not discriminate between different heat sources. It reacts to changes in the heat signatures in the field of its view. If they are static it remains…
  • genebren
    genebren over 7 years ago +4
    Hi Lanz, Welcome to the element14 community. There have been a lot of conversation here on this same topic. Like jw0752 mentions above, PIR sensors in and of themselves do not discriminate the source of…
  • genebren
    genebren over 7 years ago in reply to jw0752 +4
    Another good point. On the same concept I referenced above (shuttering), we used notch filters on top of an array of PIR elements to narrow our view to certain areas of the IR spectrum (both long and short…
Parents
  • genebren
    genebren over 7 years ago

    Hi Lanz,

     

    Welcome to the element14 community.  There have been a lot of conversation here on this same topic.  Like jw0752 mentions above, PIR sensors in and of themselves do not discriminate the source of heat they are seeing.  There are some ways that a standard PIR sensor could give you some more information about a source, but most PIR motions sensors are designed to look only at large changes in heat.

     

    Having said that, there are some ways to get more information.  One is to use a comparative approach, where the PIR sees a reference signal and compares it to the potential human signal.  I have seen this done where a shutter is placed inline with the field of view. The shutter is a wheel like structure that is 50% open (to view the heat source in question) and 50% closed to sense an ambient condition that rotates, periodically obscuring the PIR detector.  The electronics compare the live to ambient signal to develop a difference level (think of a sinusoidal waveform where the peak to peak voltage is difference value).  This level could be used to determine the strength of the heat source.  Too low or too high of a signal would imply a non-human heat source, where a signal between the extremes might be more likely to imply a human heat source.  The gain of the circuit would need to be determined such that the human temperature range was always near the middle of the reading range.  This approach does suffer in that it is very sensitive to the distance the human heat source and the PIR sensor, i.e. sensitivity decreases as the distance increases.

     

    Good luck with your project.

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 7 years ago

    Hi Lanz,

     

    Welcome to the element14 community.  There have been a lot of conversation here on this same topic.  Like jw0752 mentions above, PIR sensors in and of themselves do not discriminate the source of heat they are seeing.  There are some ways that a standard PIR sensor could give you some more information about a source, but most PIR motions sensors are designed to look only at large changes in heat.

     

    Having said that, there are some ways to get more information.  One is to use a comparative approach, where the PIR sees a reference signal and compares it to the potential human signal.  I have seen this done where a shutter is placed inline with the field of view. The shutter is a wheel like structure that is 50% open (to view the heat source in question) and 50% closed to sense an ambient condition that rotates, periodically obscuring the PIR detector.  The electronics compare the live to ambient signal to develop a difference level (think of a sinusoidal waveform where the peak to peak voltage is difference value).  This level could be used to determine the strength of the heat source.  Too low or too high of a signal would imply a non-human heat source, where a signal between the extremes might be more likely to imply a human heat source.  The gain of the circuit would need to be determined such that the human temperature range was always near the middle of the reading range.  This approach does suffer in that it is very sensitive to the distance the human heat source and the PIR sensor, i.e. sensitivity decreases as the distance increases.

     

    Good luck with your project.

    Gene

    • Cancel
    • Vote Up +4 Vote Down