Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Want to connect a speaker/amazon echo to arduino.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 414 subscribers
  • Views 1747 views
  • Users 0 members are here
Related

Want to connect a speaker/amazon echo to arduino.

thomasdruz
thomasdruz over 7 years ago

Hey all. So I am working on this project in which, when an IR sensor senses an object, it will trigger the speaker and play a greeting like "Hello" or "Welcome". I am trying to achieve this using an Arduino. I was planning to connect the speaker to the arduino using a 3.5mm cable. How can I achieve this? Any help is appreciated.

 

https://www.reddit.com/r/arduino/comments/cnyqz9/want_to_connect_a_speakeramazon_echo_to_arduino/

 

  • Sign in to reply
  • Cancel

Top Replies

  • aswinth
    aswinth over 7 years ago +3
    Sounds like a fun project and it is easy to build. But connecting your Echo to Arduino though a audio cable will not work. Your Echo cannot take input through its audio port. The best way to do it sending…
  • BigG
    BigG over 7 years ago +1
    There is a way to connect a speaker to Arduino UNO, for example, and play audio but it won't sound very good. An online search on google or youtube will reveal. To get Arduino to play decent audio through…
  • beacon_dave
    beacon_dave over 7 years ago +1
    If you want to output audio samples to a loudspeaker, then you may find Mike Cook's book "Arduino Music and Audio Projects" of interest, especially the chapter on sampling: https://books.google.co.uk/books…
Parents
  • aswinth
    aswinth over 7 years ago

    Sounds like a fun project and it is easy to build. But connecting your Echo to Arduino though a audio cable will not work. Your Echo cannot take input through its audio port. The best way to do it sending signal to it wireless, and since your echo is already connected to internet the best way is to send signal to your echo using this internet.

     

    Also this way you can place your Arduino with IR senor (or any desired sensor) at any location in your home. All you have to do is connect your Arduino to internet using a wi-fi module like ESP8266. If you are confused on how to get it done refer this Arduino Amazon echo interfacing project. The project uses an Arduino UNO to control an AC bulb but, you can edit it and adapt the project easily for your requirement.

     

    All the best have fun!!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • aswinth
    aswinth over 7 years ago

    Sounds like a fun project and it is easy to build. But connecting your Echo to Arduino though a audio cable will not work. Your Echo cannot take input through its audio port. The best way to do it sending signal to it wireless, and since your echo is already connected to internet the best way is to send signal to your echo using this internet.

     

    Also this way you can place your Arduino with IR senor (or any desired sensor) at any location in your home. All you have to do is connect your Arduino to internet using a wi-fi module like ESP8266. If you are confused on how to get it done refer this Arduino Amazon echo interfacing project. The project uses an Arduino UNO to control an AC bulb but, you can edit it and adapt the project easily for your requirement.

     

    All the best have fun!!

    • Cancel
    • Vote Up +3 Vote Down