Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Checking for Backspace char, ASCII 8
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 415 subscribers
  • Views 2645 views
  • Users 0 members are here
Related

Checking for Backspace char, ASCII 8

SGarciaV
SGarciaV over 6 years ago

Hello!

 

I've got a sketch that gets text characters from the serial (USB) port that's connected to a PC running Putty. The user types in commands. A chr(13) (Enter key) indicates the end of the text.

 

I check for a char 13 to detect the end of the command without any problem, but I can't detect the back space char 8:

 

if (inChar == 13) {

 

whatever

}

 

if (inChar == 8) ...

 

I added a Serial.println(inChar); to display the ASCII of the char and it displays 12 for the backspace char.

 

How can I check for the BS char?

 

Thanks! Sgarciav

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 6 years ago +2
    It may be the fault of PuTTY - see https://www.ssh.com/ssh/putty/putty-manuals/0.68/Chapter4.html#config-backspace 4.4.1 Changing the action of the Backspace key Some terminals believe that the Backspace…
  • SGarciaV
    SGarciaV over 6 years ago in reply to Gough Lui +2
    Argh. I wouldn't have occurred to me to look at Putty. I refactored my code to no avail. I select the Control-H option in Putty and everything is working. Thank you! Sgarciav
  • Gough Lui
    Gough Lui over 6 years ago

    It may be the fault of PuTTY - see https://www.ssh.com/ssh/putty/putty-manuals/0.68/Chapter4.html#config-backspace

    4.4.1 Changing the action of the Backspace key

    Some terminals believe that the Backspace key should send the same thing to the server as Control-H (ASCII code 8). Other terminals believe that the Backspace key should send ASCII code 127 (usually known as Control-?) so that it can be distinguished from Control-H. This option allows you to choose which code PuTTY generates when you press Backspace.

    Check your connection options when you set-up in PuTTY:

    image

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • SGarciaV
    SGarciaV over 6 years ago in reply to Gough Lui

    Argh. I wouldn't have occurred to me to look at Putty. I refactored my code to no avail. I select the Control-H option in Putty and everything is working. Thank you! Sgarciav