Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Reading UART Rx Buffer (MKR WiFi 1010 / MKR 1000)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 415 subscribers
  • Views 3822 views
  • Users 0 members are here
  • rx
  • uart
  • arduino
Related

Reading UART Rx Buffer (MKR WiFi 1010 / MKR 1000)

kas.lewis
kas.lewis over 6 years ago

Hello All,

 

I'm looking to create my own UART interrupt. For those who need to know why it's because I need to stop the timer as soon as a value comes in. While I know I will get a lot of reasons and explanations why this is not necessary I'm a lot more interested in how to go about doing this.

 

I have to commented out

 

void SERCOM5_Handler()

{

  Serial1.IrqHandler();

}

 

in the variant.cpp file which works to remove the Arduino code from doing what it wants. The issue I'm having now is finding the function Serial.read(). I'm trying to read the uart rx buffer but with Atmel's documentation what it is this is not as easy as it should be.

 

 

I have tried

 

void SERCOM5_Handler()

{

  char temp = SERCOM5->USART.DATA.reg;

  if (temp == 'h' || temp == 'H'){

    digitalWrite(LED_BUILTIN, HIGH);

  }

  if (temp == 'l' || temp == 'L'){

    digitalWrite(LED_BUILTIN, LOW);

  }

}

 

 

without much success. Therefore any help in reading the UART rx register would be very much appreciated.

 

Kas

  • Sign in to reply
  • Cancel

Top Replies

  • BigG
    BigG over 6 years ago +1
    I can see where you are coming from. Usually you could use the "serialEvent()" function but I see that this is not possible with Arduino SAMD Boards. Unortunately, I have no idea why but will be following…
  • michaelkellett
    michaelkellett over 6 years ago +1
    Is (temp == 'h'||temp == 'H') the same as ((temp == 'h')||(temp == 'H')) ? (brackets are free and make code easier to follow, (actually == has precedence over || in C )) How are you debugging this - can…
  • kas.lewis
    kas.lewis over 6 years ago in reply to michaelkellett +1
    Hello michaelkellett I didn't know you can put breakpoints in the Arduino IDE. Truth is there is lots about Arduino I don't know as I usually do bare metal with direct control of al registers and I also…
Parents
  • kas.lewis
    kas.lewis over 6 years ago

    CONCLUSION:

     

    I believe the reason why I can't find how to access the UART Rx register directly is because very few people know this as well. I feel this is the same reason when looking on Arduino forums to find this information thee are pages defending the use of Serial.available(). Some users in there defence have even gone so far as to write demos to show that timing and whatever other issue might be brought up is in fact a none issue.

     

    I feel the reality is that it's easier to do all this work then find how to read the Rx register directly. Sadly it seems this will continue as even Microchip can't offer me much in the way of a solid answer other than go through their API and find what I'm looking for myself. If I choose to do that and do find a usable solution I'll "try" post it for others to use as well.

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kas.lewis
    kas.lewis over 6 years ago

    CONCLUSION:

     

    I believe the reason why I can't find how to access the UART Rx register directly is because very few people know this as well. I feel this is the same reason when looking on Arduino forums to find this information thee are pages defending the use of Serial.available(). Some users in there defence have even gone so far as to write demos to show that timing and whatever other issue might be brought up is in fact a none issue.

     

    I feel the reality is that it's easier to do all this work then find how to read the Rx register directly. Sadly it seems this will continue as even Microchip can't offer me much in the way of a solid answer other than go through their API and find what I'm looking for myself. If I choose to do that and do find a usable solution I'll "try" post it for others to use as well.

     

    Kas