Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Reading UART Rx Buffer (MKR WiFi 1010 / MKR 1000)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 415 subscribers
  • Views 3822 views
  • Users 0 members are here
  • rx
  • uart
  • arduino
Related

Reading UART Rx Buffer (MKR WiFi 1010 / MKR 1000)

kas.lewis
kas.lewis over 6 years ago

Hello All,

 

I'm looking to create my own UART interrupt. For those who need to know why it's because I need to stop the timer as soon as a value comes in. While I know I will get a lot of reasons and explanations why this is not necessary I'm a lot more interested in how to go about doing this.

 

I have to commented out

 

void SERCOM5_Handler()

{

  Serial1.IrqHandler();

}

 

in the variant.cpp file which works to remove the Arduino code from doing what it wants. The issue I'm having now is finding the function Serial.read(). I'm trying to read the uart rx buffer but with Atmel's documentation what it is this is not as easy as it should be.

 

 

I have tried

 

void SERCOM5_Handler()

{

  char temp = SERCOM5->USART.DATA.reg;

  if (temp == 'h' || temp == 'H'){

    digitalWrite(LED_BUILTIN, HIGH);

  }

  if (temp == 'l' || temp == 'L'){

    digitalWrite(LED_BUILTIN, LOW);

  }

}

 

 

without much success. Therefore any help in reading the UART rx register would be very much appreciated.

 

Kas

  • Sign in to reply
  • Cancel

Top Replies

  • BigG
    BigG over 6 years ago +1
    I can see where you are coming from. Usually you could use the "serialEvent()" function but I see that this is not possible with Arduino SAMD Boards. Unortunately, I have no idea why but will be following…
  • michaelkellett
    michaelkellett over 6 years ago +1
    Is (temp == 'h'||temp == 'H') the same as ((temp == 'h')||(temp == 'H')) ? (brackets are free and make code easier to follow, (actually == has precedence over || in C )) How are you debugging this - can…
  • kas.lewis
    kas.lewis over 6 years ago in reply to michaelkellett +1
    Hello michaelkellett I didn't know you can put breakpoints in the Arduino IDE. Truth is there is lots about Arduino I don't know as I usually do bare metal with direct control of al registers and I also…
Parents
  • kas.lewis
    kas.lewis over 6 years ago

    Hello All, (michaelkellett)

     

    I think I may have made some progress... It doesn't really help having spent so long with C and left my C++ behind image although I guess this is also found in C.

     

    Have have found some code that may point me in the right direction but pointers and references...

     

    In \AppData\Local\Arduino15\packages\arduino\hardware\samd\1.8.4\variants\mkrwifi1010\variant.cpp

    Uart Serial1(&sercom5, PIN_SERIAL1_RX, PIN_SERIAL1_TX, PAD_SERIAL1_RX, PAD_SERIAL1_TX);

     

    In \AppData\Local\Arduino15\packages\arduino\hardware\samd\1.8.4\cores\arduino\Uart.cpp

    Uart::Uart(SERCOM *_s, uint8_t _pinRX, uint8_t _pinTX, SercomRXPad _padRX, SercomUartTXPad _padTX, uint8_t _pinRTS, uint8_t _pinCTS)

    {

      sercom = _s;

     

    In \AppData\Local\Arduino15\packages\arduino\hardware\samd\1.8.4\cores\arduino\SERCOM.cpp

    uint8_t SERCOM::readDataUART()

     

    In \AppData\Local\Arduino15\packages\arduino\hardware\samd\1.8.4\cores\arduino\Uart.cpp

    sercom->readDataUART();

     

    In \AppData\Local\Arduino15\packages\arduino\hardware\samd\1.8.4\cores\arduino\SERCOM.cpp

    return sercom->USART.DATA.bit.DATA;

     

    Its this last line I'm having issues with. sercom is a pointer to sercom5, which I assume (I can't find it for sure) is a pointer to the UART registers? I'm not really sure what to make of this line, so I'm putting it out there and hoping someone can help me make heads or tails of this.

     

    Thanks

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to kas.lewis

    I've just ordered an MKR 1010 - in stock at F so should get here tomorrow .

    More stuff to do before Christmas so it  might be a week before I get a look at it.

     

    I did find this:

    https://community.atmel.com/forum/atsamd21-sercom-interrupt-using-asf

     

    If it helps - great.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kas.lewis
    kas.lewis over 6 years ago in reply to michaelkellett

    Hello michaelkellett,

     

    I've read over that link now and cant find a clear answer. I've attempted to look for the functions mentioned as well as tried running their code in the Arduino IDE, no dice image. I have also continued to try drill down with in the code to find the callback function that puts the received characters in the ring buffer, also no dice. This is really turning out to be a hunt that doesn't look like will have an easy or quick solution.

     

    If you have any further ideas, I'll be more than happy to entertain them. The one thing I'm trying to avoid is installing Microchips IDE. I currently don't have much space left on my hard drive or the SD card I'm using to extend my storage space. So if this can be resolved with out going that route, I'd greatly appreciate that.

     

    Kas

     

    P.s

    After a bit more reading and digging there maybe something else to try. I'm putting it here for later reference as well as so others can possibly try this out.

     

    There is a file called variant.cpp that has a function

    void SERCOM5_Handler()
    {
      Serial1.IrqHandler();
    }

    this appears to be where the interrupt is handled in real time (this is what would need to be tested) if this is correct then this would be where any additional code can be added to stop timers or get data directly from the UART. I have already tried

    (sercom5).readDataUART();

    in the arduino IDE and it complies. This does not mean it works but there is a better chance then it not even compiling. This might therefore allow me to stop or reset a timer as well as getting received bytes right away. Once tested I'll update this post.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to kas.lewis

    Hello Kas,

     

    Sorry. I've been busy with lots of other stuff and haven't looked at this since I did the last post.

     

    My initial conclusion was that I just can't see any value (for me at least) in getting bogged down in the Arduino stuff. I can get more value from my time just hitting an ARM or AVR processor in C directly.

     

    I know that's not much help to you -  but good luck with your efforts.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 6 years ago in reply to kas.lewis

    Hello Kas,

     

    Sorry. I've been busy with lots of other stuff and haven't looked at this since I did the last post.

     

    My initial conclusion was that I just can't see any value (for me at least) in getting bogged down in the Arduino stuff. I can get more value from my time just hitting an ARM or AVR processor in C directly.

     

    I know that's not much help to you -  but good luck with your efforts.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • kas.lewis
    kas.lewis over 6 years ago in reply to michaelkellett

    michaelkellett,

     

    I hear your sentiment 100%, Arduino is not my platform of choice for this exact reason. I find I can get stuff most stuff done faster and easier using straight C (unless is really is doing something generic). Unfortunately for this project I need to use an Arduino and so here I am, using a product with hard to find documentation (I can't find clear register information for the AVR).

     

    Kas