Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino reset with induction motor and contactor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 414 subscribers
  • Views 930 views
  • Users 0 members are here
Related

Arduino reset with induction motor and contactor

hawre.balak
hawre.balak over 6 years ago

Hello guys,

hope i could find a solution for my arduino based automation for a machine which contains an induction motor, the arduino is powered by a linear power supply and it controls a relay then it turns on a three phase contactor to turn on the induction motor, my problem is that whenever the induction motor starts the arduino randomly resets! How can i fix it

Note:

-the arduino works fine when the motor is not connected!

-the relay has protection diode on the coil!

-the power supply has a big 3300uF capacitor to prevent voltage dips and 0.1uF ceramic across the microcontroller.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 6 years ago +1
    You probably need to isolate the Arduino power from the coil and motor power. Use a diode to feed power to the Arduino and put a reasonably large cap on the Arduino side of the diode.
  • neilk
    neilk over 6 years ago

    A schematic is needed to understand what the problem migh be

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 6 years ago

    You probably need to isolate the Arduino power from the coil and motor power.

    Use a diode to feed power to the Arduino and put a reasonably large cap on the Arduino side of the diode.