Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum I need help in converting Arduino code to C language code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 424 subscribers
  • Views 8732 views
  • Users 0 members are here
Related

I need help in converting Arduino code to C language code

e14 Contributor
e14 Contributor over 10 years ago

 

#include

 


Servo myservo; //creates a servo object
//a maximum of eight servo objects can be created

 

int pos = 0; //variable to store servo position

 

 

 

int calibrationTime = 30;

 

//the time when the sensor outputs a low impulse
long unsigned int lowIn;

 

//the amount of milliseconds the sensor has to be low
//before we assume all motion has stopped
long unsigned int pause = 5000;

 

boolean lockLow = true;
boolean takeLowTime;

 

int pirPin = 12; //digital pin connected to the PIR's output
int pirPos = 13; //connects to the PIR's 5V pin

 

void setup(){
myservo.attach(4); //attaches servo to pin 4
Serial.begin(9600); //begins serial communication
pinMode(pirPin, INPUT);
pinMode(pirPos, OUTPUT);
digitalWrite(pirPos, HIGH);

 

//give the sensor time to calibrate
Serial.println("calibrating sensor ");
for(int i = 0; i < calibrationTime; i++){
Serial.print(calibrationTime - i);
Serial.print("-");
delay(1000);
}
Serial.println();
Serial.println("done");

 


while (digitalRead(pirPin) == HIGH) {
delay(500);
Serial.print(".");
}
Serial.print("SENSOR ACTIVE");
}

 

void loop(){

 

if(digitalRead(pirPin) == HIGH){ //if the PIR output is HIGH, turn servo

 

/*turns servo from 0 to 180 degrees and back
it does this by increasing the variable "pos" by 1 every 5 milliseconds until it hits 180
and setting the servo's position in degrees to "pos" every 5 milliseconds
it then does it in reverse to have it go back
**/

 

for(pos = 0; pos < 180; pos += 1) //goes from 0 to 180 degrees
{ //in steps of one degree
myservo.write(pos); //tells servo to go to position in variable "pos"
delay(5); //waits for the servo to reach the position
}
for(pos = 180; pos>=1; pos-=1) //goes from 180 to 0 degrees
{
myservo.write(pos); //to make the servo go faster, decrease the time in delays for
delay(5); //to make it go slower, increase the number.
}

 

if(lockLow){

 

lockLow = false;
Serial.println("---");
Serial.print("motion detected at ");
Serial.print(millis()/1000);
Serial.println(" sec");
delay(50);
}
takeLowTime = true;
}

 

if(digitalRead(pirPin) == LOW){

 

if(takeLowTime){
lowIn = millis(); //save the time of the transition from HIGH to LOW
takeLowTime = false; //make sure this is only done at the start of a LOW phase
}

 

//if the sensor is low for more than the given pause,
//we can assume the motion has stopped

 

if(!lockLow && millis() - lowIn > pause){

 

lockLow = true;
Serial.print("motion ended at "); //output
Serial.print((millis() - pause)/1000);
Serial.println(" sec");
delay(50);
}
}
}

  • Sign in to reply
  • Cancel

Top Replies

  • COMPACT
    COMPACT over 10 years ago in reply to e14 Contributor +3
    For which particular aspects of C++? C++ is really c with objects and some changes to syntax and structure to support objects (e.g. polymorphism). C++ can make the compiled object code bloated, fat and…
  • mconners
    mconners over 10 years ago in reply to e14 Contributor +3
    Well, in that case the flavor of C used for the Arduino already meets your needs. C++ is a super set of the C language, and the Arduino compiler already supports this. A major difference is when using…
  • mconners
    mconners over 10 years ago +2
    Hi shajeeh, Arduino code is C language code. It just has a simplified API to allow you to access the IO pins available on the AVR chip. What platform are you wanting to convert this to? We would need that…
Parents
  • lmc98cdddt16c
    lmc98cdddt16c over 8 years ago

    chào cac chàng trai,có thể giúp tôi về vấn đề chuyển đổi code của adruino sang code cua ccs cho arm được không

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lmc98cdddt16c
    lmc98cdddt16c over 8 years ago in reply to lmc98cdddt16c

    Hello guys, can you help me on converting adruino code to ccs code for arm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to lmc98cdddt16c

    Do you mean Arduino? Or something else?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 8 years ago in reply to lmc98cdddt16c

    If by CCS you mean TI's Code Composer Studio then you can just open up an Energia sketch and run it on some of their ARM processors. I'm not up on the details because I avoid Arduino. You will find 43oh.com is a good resource for Energia stuff.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 8 years ago in reply to lmc98cdddt16c

    You can start here, although the post is a bit older since CCS is at version 8

    https://43oh.com/2014/07/import-energia-sketches-into-ccs6-for-line-by-line-debugging/

     

    If you are looking to drop the Arduino code completely then you'll have a bit of work ahead for you and would have to create your own code to stimulate the Arduino libraries. That is unless you can find one within the SimpleLink packages or other code.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lmc98cdddt16c
    lmc98cdddt16c over 8 years ago in reply to shabaz

    hi, specifically i want to translate this code from adurino side to MDK 5 KelC

    Can you help me?

    thank you very much

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lmc98cdddt16c
    lmc98cdddt16c over 8 years ago in reply to Fred27

    Thank you so much, but the idea is to transfer adrunio code to code code of MDK 5 KelC, can you help me?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lmc98cdddt16c
    lmc98cdddt16c over 8 years ago in reply to jomoenginer

    Thank you very much, but the idea is to transfer adrunio code to code code of MDK 5 KelC, can you help me?

    code Adrunio:

    1. // (c) Michael Schoeffler 2017, http://www.mschoeffler.de
    2. #include <HX711_ADC.h> // https://github.com/olkal/HX711_ADC
    3. #include <Wire.h>
    4. #include <LiquidCrystal_I2C.h> // LiquidCrystal_I2C library
    5. HX711_ADC LoadCell(4, 5); // parameters: dt pin, sck pin<span data-mce-type="bookmark" style="display: inline-block; width: 0px; overflow: hidden; line-height: 0;"></span>
    6. LiquidCrystal_I2C lcd(0x27, 2, 1, 0, 4, 5, 6, 7, 3, POSITIVE); // 0x27 is the i2c address of the LCM1602 IIC v1 module (might differ)
    7. voidsetup(){
    8.   LoadCell.begin(); // start connection to HX711
    9.   LoadCell.start(2000); // load cells gets 2000ms of time to stabilize
    10.   LoadCell.setCalFactor(999.0); // calibration factor for load cell => strongly dependent on your individual setup
    11.   lcd.begin(16, 2); // begins connection to the LCD module
    12.   lcd.backlight(); // turns on the backlight
    13. }
    14. voidloop(){
    15.   LoadCell.update(); // retrieves data from the load cell
    16. float i = LoadCell.getData(); // get output value
    17.   lcd.setCursor(0, 0); // set cursor to first row
    18.   lcd.print("Weight[g]:"); // print out to LCD
    19.   lcd.setCursor(0, 1); // set cursor to secon row
    20.   lcd.print(i); // print out the retrieved value to the second row
    21. }
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lmc98cdddt16c
    lmc98cdddt16c over 8 years ago in reply to lmc98cdddt16c

    code Adruino:

    1. // (c) Michael Schoeffler 2017, http://www.mschoeffler.de
    2. #include <HX711_ADC.h> // https://github.com/olkal/HX711_ADC
    3. #include <Wire.h>
    4. #include <LiquidCrystal_I2C.h> // LiquidCrystal_I2C library
    5. HX711_ADC LoadCell(4, 5); // parameters: dt pin, sck pin<span data-mce-type="bookmark" style="display: inline-block; width: 0px; overflow: hidden; line-height: 0;"></span>
    6. LiquidCrystal_I2C lcd(0x27, 2, 1, 0, 4, 5, 6, 7, 3, POSITIVE); // 0x27 is the i2c address of the LCM1602 IIC v1 module (might differ)
    7. voidsetup(){
    8.   LoadCell.begin(); // start connection to HX711
    9.   LoadCell.start(2000); // load cells gets 2000ms of time to stabilize
    10.   LoadCell.setCalFactor(999.0); // calibration factor for load cell => strongly dependent on your individual setup
    11.   lcd.begin(16, 2); // begins connection to the LCD module
    12.   lcd.backlight(); // turns on the backlight
    13. }
    14. voidloop(){
    15.   LoadCell.update(); // retrieves data from the load cell
    16. float i = LoadCell.getData(); // get output value
    17.   lcd.setCursor(0, 0); // set cursor to first row
    18.   lcd.print("Weight[g]:"); // print out to LCD
    19.   lcd.setCursor(0, 1); // set cursor to secon row
    20.   lcd.print(i); // print out the retrieved value to the second row
    21. }
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lmc98cdddt16c
    lmc98cdddt16c over 8 years ago in reply to lmc98cdddt16c

    code Adrunio :

    1. // (c) Michael Schoeffler 2017, http://www.mschoeffler.de
    2. #include <HX711_ADC.h> // https://github.com/olkal/HX711_ADC
    3. #include <Wire.h>
    4. #include <LiquidCrystal_I2C.h> // LiquidCrystal_I2C library
    5. HX711_ADC LoadCell(4, 5); // parameters: dt pin, sck pin<span data-mce-type="bookmark" style="display: inline-block; width: 0px; overflow: hidden; line-height: 0;"></span>
    6. LiquidCrystal_I2C lcd(0x27, 2, 1, 0, 4, 5, 6, 7, 3, POSITIVE); // 0x27 is the i2c address of the LCM1602 IIC v1 module (might differ)
    7. voidsetup(){
    8.   LoadCell.begin(); // start connection to HX711
    9.   LoadCell.start(2000); // load cells gets 2000ms of time to stabilize
    10.   LoadCell.setCalFactor(999.0); // calibration factor for load cell => strongly dependent on your individual setup
    11.   lcd.begin(16, 2); // begins connection to the LCD module
    12.   lcd.backlight(); // turns on the backlight
    13. }
    14. voidloop(){
    15.   LoadCell.update(); // retrieves data from the load cell
    16. float i = LoadCell.getData(); // get output value
    17.   lcd.setCursor(0, 0); // set cursor to first row
    18.   lcd.print("Weight[g]:"); // print out to LCD
    19.   lcd.setCursor(0, 1); // set cursor to secon row
    20.   lcd.print(i); // print out the retrieved value to the second row
    21. }
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 8 years ago in reply to lmc98cdddt16c

    Hi cong le,

     

    The issue you'll run into is that the HX711_ADC and LiquidCrystal_I2C libraries are probably not available for keil.

     

    You can get the source and port them your self, which often isn't too terribly hard, and the source is usually available.

     

    You would also need to create a main() function and call setup() and loop() (or move those into main)

     

    Take a look at mbed.com, they have arduino like libraries for a variety of arm processors, and they have the capability to export to a few different dev environments such as keil, gcc, etc...

     

    This won't be terribly difficult as a mid level c (or c++) programmer.

     

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 8 years ago in reply to lmc98cdddt16c

    What MCU/Board are you looking to connect this to?

     

    Also, have you attempted to port this over to MDK yourself?  If not, why not?

     

    My first suggest would be to look at the code at github link listed in the example code you posted:

    https://github.com/olkal/HX711_ADC

     

    Search online for any non Arduino examples that might be more appropriate for your efforts.

     

    Have a look at HX711_ADC.cpp and HX711_ADC.h under 'src'.   Note, there is a include for Arduino.h, so this is where you'll have to either find replacement code for your MCU or create it yourself.  You'll have to replace things such as begin, start, pinMode and digitalRead to code that is appropriate for the new development environment.  You can search the web for what Ardiuno.h provides to get a clue as to what you need to do in your code.

     

    If you do not have an equivalent to the Wiring.h code, unless someone else wrote it, you'll have to initialize the MCU to match the connections to the HX711.  So, if you can not find code that covers this already, you'll have to write this yourself meaning you'll need to look at the datasheet for the MCU your are using.

     

    This is where I suggest you start.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jomoenginer
    jomoenginer over 8 years ago in reply to lmc98cdddt16c

    What MCU/Board are you looking to connect this to?

     

    Also, have you attempted to port this over to MDK yourself?  If not, why not?

     

    My first suggest would be to look at the code at github link listed in the example code you posted:

    https://github.com/olkal/HX711_ADC

     

    Search online for any non Arduino examples that might be more appropriate for your efforts.

     

    Have a look at HX711_ADC.cpp and HX711_ADC.h under 'src'.   Note, there is a include for Arduino.h, so this is where you'll have to either find replacement code for your MCU or create it yourself.  You'll have to replace things such as begin, start, pinMode and digitalRead to code that is appropriate for the new development environment.  You can search the web for what Ardiuno.h provides to get a clue as to what you need to do in your code.

     

    If you do not have an equivalent to the Wiring.h code, unless someone else wrote it, you'll have to initialize the MCU to match the connections to the HX711.  So, if you can not find code that covers this already, you'll have to write this yourself meaning you'll need to look at the datasheet for the MCU your are using.

     

    This is where I suggest you start.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • lmc98cdddt16c
    lmc98cdddt16c over 8 years ago in reply to jomoenginer

    thanks you so much