Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum how to connect arduino to the computer ??
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 414 subscribers
  • Views 1258 views
  • Users 0 members are here
Related

how to connect arduino to the computer ??

yayalzz
yayalzz over 6 years ago

i have projects i can do only with python so i wanna connect the card to the computer somehow using some library that i can give through it instructions to arduino card via the usb cable.

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 6 years ago +6
    Hi Yahya, There are many tutorials on this subject. For example, the following link discusses using USB serial between Python on a Raspberry Pi and an Arduino. https://roboticsbackend.com/raspberry-pi…
  • ralphjy
    ralphjy over 6 years ago +6
    It would be helpful if you described what you are trying to do with Python and the Arduino. If you are using the Uno, here is a simple Python library and the associated Arduino program that you can use…
  • DAB
    DAB over 6 years ago +5
    You can use any basic UART protocol with the Arduino so you do not need to use only the USB connection. DAB
Parents
  • ralphjy
    ralphjy over 6 years ago

    It would be helpful if you described what you are trying to do with Python and the Arduino.  If you are using the Uno, here is a simple Python library and the associated Arduino program that you can use as an example and modify https://github.com/dbarattini/ArduPy.   Note: this is not ArduPy from Seeed Studios which uses CircuitPython.   This is a basic Python library that provides some base functionality but would be easy to adapt.  You can modify the pinout if you are using a different board.  Requires that you have Python and PySerial installed on your host computer.

    How to use

    Upload the ardupy/ardupy.ino sketch to your Arduino Uno

    Create a new python project and import ardupy

    Learn from these examples:

    • use a button
    • use a led
    • use a temperature sensor
    • use a photoresistor
    • use an RGB led
    • use a servo
    • use a potentiometer
    • use a piezo
    • use a tilt switch
    • use a dc motor
    • use a dc motor through an h-bridge
    • use an lcd

    You can also use ArduPy to comunicate directly to arduino

    • use arduino directly
    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ralphjy
    ralphjy over 6 years ago

    It would be helpful if you described what you are trying to do with Python and the Arduino.  If you are using the Uno, here is a simple Python library and the associated Arduino program that you can use as an example and modify https://github.com/dbarattini/ArduPy.   Note: this is not ArduPy from Seeed Studios which uses CircuitPython.   This is a basic Python library that provides some base functionality but would be easy to adapt.  You can modify the pinout if you are using a different board.  Requires that you have Python and PySerial installed on your host computer.

    How to use

    Upload the ardupy/ardupy.ino sketch to your Arduino Uno

    Create a new python project and import ardupy

    Learn from these examples:

    • use a button
    • use a led
    • use a temperature sensor
    • use a photoresistor
    • use an RGB led
    • use a servo
    • use a potentiometer
    • use a piezo
    • use a tilt switch
    • use a dc motor
    • use a dc motor through an h-bridge
    • use an lcd

    You can also use ArduPy to comunicate directly to arduino

    • use arduino directly
    • Cancel
    • Vote Up +6 Vote Down