Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum How to configure an Arduino GPIO as an input
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 414 subscribers
  • Views 6739 views
  • Users 0 members are here
  • arduino best practice
  • arduino circuit
Related

How to configure an Arduino GPIO as an input

colporteur
colporteur over 5 years ago

What would you recommend to reduce the spurious triggers on the input of a Nano?

 

Up to now I have been using Arduino Nano microcontrollers for animation support on a model railroad without issue. With the recent completion of the airport scene, I started to experience issues of Nano's receiving spurious triggers. At first I thought maybe I set the input resistor to high, so I reduced the value from 100K to 47K. I got some relief but it has recently raised it ugly head again. Without the resistor the triggering is unpredictable.

 

Currently there are 5 animations that have button control.

  • Aircraft landing simulation (LED)
  • Hanger building Lighting (LED)
  • Simulate arc welder at bench (LED)
  • Compound gate open/close (28BYJ-48 ULN2003 controller)
  • Hanger aircraft engine startup/shutdown (L293 brushless motor)

 

The compound gate sometimes triggers the Hanger aircraft engine animation and vise versa. The input circuit I am using for the Nano is minimal.  These two animations did share the same twisted pair from the button panel. I have separated the animations button to different pairs and I have some relief. I'm thinking maybe there is a simple way to dampen inputs so they are not as sensitive?

 

I'm hoping someone might have a suggestion/best practice recommendation for connecting inputs, that is designed to eliminate the problem.

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 5 years ago +9
    100K and 47K are very weak pull-down (or up) resistors. If you're in a known noisy environment, you probably want something in the 1K to 4.7K range.
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago +8
    Try a small capacitor ( 10nF ) in parallel to the resistor. This is called de-bouncing an input. Can also be done in software, there might even Arduino libraries for that. - W.
  • dougw
    dougw over 5 years ago +7
    It sounds like you are getting cross-talk as well as switch bouncing. If you put a resistor in series with the switch and a capacitor at the digital input as wolfgangfriedrich mentioned, there won't be…
Parents
  • milosrasic98
    milosrasic98 over 5 years ago

    Hi colporteur

     

    The best option is to of course go for both hardware and software debouncing. Hardware debouncing can be done easily as mentioned already by wolfgangfriedrich , as for the software debouncing here is a simple piece of code which could help:

     

    #define debounceDelay 100
    
    
    int lastButtonState = 0;
    int lastDebounceTime = 0;
    int buttonState;
    
    
    
    
    void setup() {
    
    
      pinMode(BUTTON_CENTER, INPUT);
      
    }
    
    
    
    
    void loop(){
    
    
      int reading = digitalRead(BUTTON_CENTER);
        if (reading != lastButtonState) {
          // reset the debouncing timer
          lastDebounceTime = millis();
        }
        if ((millis() - lastDebounceTime) > debounceDelay) {
          if (reading != buttonState) {
            buttonState = reading;
            if (buttonState == HIGH) {
              //Here you will know that the button was pressed
            }
          }
        }
        lastButtonState = reading;
      
      }

     

         I've found that this approach works great, and it's using millis instead of delay so there isn't any code flow blocking. I've put the debounce delay to 100ms in the code, but you can tweak it to your liking. I found it works great like this, though, maybe a touch slower. For how this code works, when we detect a button reading which was different from the last button reading we just remember at what point that occurred. If we keep the buttons pressed long enough (100ms in our case), lastDebounceTime won't change and our second if statement will be fulfilled. Once the buttons was On for 100ms at least, it still won't register the press until you release the button. Hope this helps you!

     

    Milos

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 5 years ago in reply to milosrasic98

    Thanks MR, I saw a code example https://www.arduino.cc/en/Tutorial/BuiltInExamples/Debounce  and wondered about the delay value.

     

    I'm a code resurrectionist and not an programmer, so I tend to default to hardware for solution. Your code is slightly different than what I found. What advantage is

    1. #define debounceDelay 100

     

    verses unsigned long debounceDelay = 50;    // the debounce time; increase if the output flickers

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 5 years ago in reply to colporteur

    If you want to fully debounce a switch in hardware it is easy to achieve 100% instantaneous debouncing if you use a double throw switch. You don't need any other hardware if you feed 2 digital inputs from the the switch, but you can use a couple of inverters or NAND gates if you want to do it all in hardware.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 5 years ago in reply to colporteur

    I found this Arduino library to be pretty good and it's versatile: https://www.arduino.cc/reference/en/libraries/bounce2/

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 5 years ago in reply to colporteur

    I found this Arduino library to be pretty good and it's versatile: https://www.arduino.cc/reference/en/libraries/bounce2/