Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum How to configure an Arduino GPIO as an input
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 414 subscribers
  • Views 6739 views
  • Users 0 members are here
  • arduino best practice
  • arduino circuit
Related

How to configure an Arduino GPIO as an input

colporteur
colporteur over 5 years ago

What would you recommend to reduce the spurious triggers on the input of a Nano?

 

Up to now I have been using Arduino Nano microcontrollers for animation support on a model railroad without issue. With the recent completion of the airport scene, I started to experience issues of Nano's receiving spurious triggers. At first I thought maybe I set the input resistor to high, so I reduced the value from 100K to 47K. I got some relief but it has recently raised it ugly head again. Without the resistor the triggering is unpredictable.

 

Currently there are 5 animations that have button control.

  • Aircraft landing simulation (LED)
  • Hanger building Lighting (LED)
  • Simulate arc welder at bench (LED)
  • Compound gate open/close (28BYJ-48 ULN2003 controller)
  • Hanger aircraft engine startup/shutdown (L293 brushless motor)

 

The compound gate sometimes triggers the Hanger aircraft engine animation and vise versa. The input circuit I am using for the Nano is minimal.  These two animations did share the same twisted pair from the button panel. I have separated the animations button to different pairs and I have some relief. I'm thinking maybe there is a simple way to dampen inputs so they are not as sensitive?

 

I'm hoping someone might have a suggestion/best practice recommendation for connecting inputs, that is designed to eliminate the problem.

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 5 years ago +9
    100K and 47K are very weak pull-down (or up) resistors. If you're in a known noisy environment, you probably want something in the 1K to 4.7K range.
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago +8
    Try a small capacitor ( 10nF ) in parallel to the resistor. This is called de-bouncing an input. Can also be done in software, there might even Arduino libraries for that. - W.
  • dougw
    dougw over 5 years ago +7
    It sounds like you are getting cross-talk as well as switch bouncing. If you put a resistor in series with the switch and a capacitor at the digital input as wolfgangfriedrich mentioned, there won't be…
Parents
  • colporteur
    colporteur over 5 years ago

    I implemented BEJ baldengineer 4.7Kohm to ground resistor today. I then reconnected the two simulations to the same pair. I then went off to do something else and in short while experienced false triggers once again. Triggering the gate simulation button and the hanger simulation started up as well.

     

    I haven't implemented a bounce routine yet, I like BigG share. That will be the next test.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago in reply to colporteur

    Another easy test for a simple solution would to make the 4.7k resistor a pull-up and wire the switch to GND. This gives you a higher immunity because the voltage difference from the 5V rail to a false '0' is larger than from GND to a false '1'. Assuming TTL logic would be 5V to 0.8V vs. 0V to ~2V.

    And you would need to invert your logic in the code. image

    Worth a try.

    - W.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago in reply to colporteur

    Another easy test for a simple solution would to make the 4.7k resistor a pull-up and wire the switch to GND. This gives you a higher immunity because the voltage difference from the 5V rail to a false '0' is larger than from GND to a false '1'. Assuming TTL logic would be 5V to 0.8V vs. 0V to ~2V.

    And you would need to invert your logic in the code. image

    Worth a try.

    - W.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Children
  • neilk
    neilk over 5 years ago in reply to wolfgangfriedrich

    I've done this, but with a 10k pull up resistor. I put a 2.7 nF capacitor across the switch. Works well for me with no debouncing code.

     

     

     

    Neil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to neilk

    Wolfgang's suggestion may give some headroom. Same for the resistors.

    I'm not sure about the capacitors though. They help with bounce but not with external interferences.

    These unwanted triggering events aren't bounce artifacts.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 5 years ago in reply to wolfgangfriedrich

    Thanks WF. I have used ground trigger before on the Raspberry Pi normally. For some reason I have numerous voltage triggered Arduino's now. I can't recall when I did the switch. I really try to be consistent. I think I found an Arduino sketch that had voltage triggered in it that worked. I then started using that as a pattern.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to colporteur

    If you are into adventure, Sean, you could switch over to CAN bus.

     

    Disadvantage:

    - you'd need to have a receiver with a microcontroller at the point of action.

    - receiving nodes have to be programmed to react on messages for them.

    Advantage:

    - it's a bus. you can loop the bus wire to every place you need, usually 4 wires are enough for power and signals.

    - resilient to induced mayhem.

    - learning path isn't steep

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 5 years ago in reply to Jan Cumps

    My in my next life of helping put the foundation in for a model railroad layout I can consider the CAN bus suggestion. I installed a LAN to start because we were only supposed to be using Pi's. Arduino's filled a niche and now there is about 20 deployed and more to come. There are five Pi's running animation also.