Arduino Forum ATTiny 85
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
  • Replies 6 replies
  • Subscribers 392 subscribers
  • Views 851 views
  • Users 0 members are here
Related

ATTiny 85

morbee
morbee over 9 years ago

Hi Guy's,

 

I have a little alarm i am trying to put together that consists of a HC SRO4 distance sensor and a Piezo Buzzer. wiring this up to the arduino is straight forward and the code is fairly straight forward as can be seen below.

My Question is which pins would i connect to on an ATTiny 85 once i have programmed it with this code?

 

*/

 

 

#define trigPin 13

#define echoPin 12

#define buzzer 11

 

 

 

 

void setup() {

 

 

  pinMode(trigPin, OUTPUT);

  pinMode(echoPin, INPUT);

  pinMode(buzzer, OUTPUT);

 

 

}

 

 

void loop() {

  long duration, distance;

  digitalWrite(trigPin, LOW);

  delayMicroseconds(2);

  digitalWrite(trigPin, HIGH);

//  delayMicroseconds(1000);

  delayMicroseconds(10);

  digitalWrite(trigPin, LOW);

  duration = pulseIn(echoPin, HIGH);

  distance = (duration/2) / 29.1;

  if (distance < 50) {  // This is where the buzzer On/Off happens

    digitalWrite(buzzer,HIGH);

}

  else {

    digitalWrite(buzzer,LOW);

   

   (distance >= 200 || distance <= 0);}

  }

  • Sign in to reply
  • Cancel

Top Replies

  • morbee
    morbee over 9 years ago +1
    Hi Guys, Thank you to Henry for putting me on the right track and i now understand the method for programming ATTiny. I have a little yorkshire terrier that insists on sneaking out the back courtyard gate…
Parents
  • snu
    snu over 9 years ago

    Use this instead:

     

    #define trigPin 2

    #define echoPin 1

    #define buzzer 0

     

    It will use pin 5 as pin 0, pin 6 as pin 1, and pin 7 as pin 2, although for pin 2 you may have to burn the fuses differently.52713d5b757b7fc0658b4567.png

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morbee
    morbee over 9 years ago in reply to snu

    Hello Henry,

     

    Thank you very much for your reply and i will change my code to what you have suggested.

    I am newbie to the world of electronics and have started up with it as a hobby more than anything else. Please could you explain the meaning of burning the fuses for pin 2 differently. I am sure if i understand what you mean by this i can try and figure this out.

     

    Kind Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • snu
    snu over 9 years ago in reply to morbee

    Use AVRdudess and the Arduino as ISP setup or your own AVR programmer. There's a fuse calculator in AVRdudess. I will gladly find the fuse setup for you if you want, but first try programming the chip and see if pin D2 works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morbee
    morbee over 9 years ago in reply to snu

    Hi Henry,

    Thanks for the feedback, I have used my arduino as the programmer using pins 2 (Trigg), 3 (Echo) and 0 for the buzzer. ATTiny is now programmed perfectly and working as i planned.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morbee
    morbee over 9 years ago in reply to snu

    Hi Henry,

    Thanks for the feedback, I have used my arduino as the programmer using pins 2 (Trigg), 3 (Echo) and 0 for the buzzer. ATTiny is now programmed perfectly and working as i planned.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • snu
    snu over 9 years ago in reply to morbee

    Glad to hear it! Very creative project.