Arduino Forum No power flowing, please help
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
  • Replies 16 replies
  • Subscribers 393 subscribers
  • Views 1098 views
  • Users 0 members are here
  • mega
  • adk
  • arduino
Related

No power flowing, please help

Former Member
Former Member over 9 years ago

I am using an Arduino ADK with a motor control plugin (the thing with several pins that sits on top of the Arduino board), and I have the arduino connected to a PS3 controller via bluetooth.  I am sure that that part is working properly.  However, when I connect a battery to the plugin and then connect a DC motor on the other end, I find that the controller does not do anything.  Further looking into it, I checked both ends with a meter.  The battery was putting out 20.2 V, whereas the receiving end with the motor measured at 0.  I have two of the boards and it is doing it on both of them.  Did I not do something that I should have?  Any help at all would be appreciated, as I need to get this working for a robotics competition in a few months.  Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +1
    Hi Tyler, Can you supply the information below, and specifically mention what battery you're using, and exactly what/where you're probing (mark it on a diagram or photo) to see your 0V measurement. As…
  • mcb1
    mcb1 over 9 years ago in reply to peterjcs23 +1
    The board shows it was designed by BDG Customs. There is a video here https://www.youtube.com/watch?v=M-ulU21j1hc&feature=youtu.be from their facebook page on March 2014 https://www.facebook.com/xBDGcustoms…
  • peterjcs23
    peterjcs23 over 9 years ago in reply to Former Member +1
    Hi Tyler You must contact BDG and request a datasheet for the board and any Arduino sketch they offer. Contact_Us This is a guess...The board looks like an H-Bridge and the reason you have no output is…
  • shabaz
    shabaz over 9 years ago

    Hi Tyler,

     

    Can you supply the information below, and specifically mention what battery you're using, and exactly what/where you're probing (mark it on a diagram or photo) to see your 0V measurement.

    As it stands, the information is insufficient to give good advice. Hopefully with the additional information we can make suggestions.



    What hardware, tools and software I'm using

              (e.g. part number, link to the tools and software)

    Non-blurry photographs of the set-up (zoomed out for context, and detail), and video if needed


    Code snippet or schematic showing the problem area


    Entire code and schematics if possible in attachments

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • peterjcs23
    peterjcs23 over 9 years ago

    what is the part number of the motor control plugin?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to shabaz

    Shabaz,

         Thank you so much for replying.  I am using a Ridgid 4.0 Ah Li-ion drill battery.  As for the diagram: image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to peterjcs23

    Does this help? I couldn't find it.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to Former Member

    It might help if you flip the motor shield over.  There's frequently manufacturer and model info on the underside of the PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to Former Member

    Product documentation, or a part number leading to a product URL and some documentation is needed for that motor controller board. Where did you get it, and how do you know which pins on the Arduino are used to control the motor?

    It is expected to see 0V on the motor outputs, until the correct logic level inputs are applied to the board. It would be guesswork to know what pins need what signals, without documentation (or manually tracing the wires and examining the part numbers of the components on the board).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to shabaz

    There is nothing that resembles a number on the underside of either the motor shield or the board itself. Here is the website for the board we are using https://www.arduino.cc/en/Main/ArduinoBoardMegaADK.  The motor thing that connects into the board is "The USB host interface given by MAX3421E IC".  Does that help?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to Former Member

    No, need the documentation or product page for the motor controller board, not the Arduino board. How did you determine what pins needed driving, without the documentation?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • peterjcs23
    peterjcs23 over 9 years ago in reply to Former Member

    I've turned your picture round and looked at the motor drive, which actually looks like an H Bridge.

    image

    What does it say up at the top right? PM-2 and something under that. Is there any clue as to the manufacturer?

     

    Where did you buy it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to peterjcs23

    The board shows it was designed by BDG Customs.

     

    There is a video here

    https://www.youtube.com/watch?v=M-ulU21j1hc&feature=youtu.be

     

    from their facebook page on March 2014

    https://www.facebook.com/xBDGcustoms/?fref=nf

     

     

    Unfortunately it doesn't give a lot of other info.

    It seems that there is no code supplied by the OP .... maybe that is the issue.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>