Arduino
  • Products
  • More
Arduino
Arduino Forum Reminder:  New Arduino Product Now Available at the element14 Store
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 417 subscribers
  • Views 482 views
  • Users 0 members are here
  • product
  • arduino
Related

Reminder:  New Arduino Product Now Available at the element14 Store

GardenState
GardenState over 15 years ago

Some examples

Nano. The Arduino Nano is a small, complete, and breadboard-friendly board based on the ATmega328 (Arduino Nano 3.0Arduino Nano 3.0) or ATmega168 (Arduino Nano 2.x). The Arduino Nano can be powered via the Mini-B USB connection, 6-20V unregulated external power supply (pin 30), or 5V regulated external power supply (pin 27). The power source is automatically selected to the highest voltage source.
 
Mega. The Arduino Mega 2560Arduino Mega 2560 is a microcontroller board based on the ATmega2560. It has 54 digital input/output pins (of which 14 can be used as PWM outputs), 16 analog inputs, 4 UARTs (hardware serial ports), a 16 MHz crystal oscillator, a USB connection, a power jack, an ICSP header, and a reset button. It contains everything needed to support the microcontroller; simply connect it to a computer with a USB cable or power it with a AC-to-DC adapter or battery to get started .
 
XBee Shield.  Aruino shields are boards to be mounted on top of the Arduino board and that extend the functionality of Arduino to control different devices, acquire data, etc. The Xbee shieldXbee shield allows multiple Arduino boards to communicate wirelessly over distances up to 100 feet (indoors) or 300 feet (outdoors) using the Maxstream Xbee Zigbee module.

  • Sign in to reply
  • Cancel
Parents
  • chrisbaron
    chrisbaron over 15 years ago

    Howdy.  My company has several unique new Arduino products in the pipeline.  Can you tell me how to submit them for consideration by Element 14/Newark?

     

    Thanks,

     

    Chris Baron

    Robot Power

    chris@robotpower.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GardenState
    GardenState over 15 years ago in reply to chrisbaron

    Chris:

     

    By doing just what you are doing: posting info on the Arduino community site. Just one word of caution: don't run an ad and do not link to commercial sites. Otherwise you are good to go.

     

    GS

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • GardenState
    GardenState over 15 years ago in reply to chrisbaron

    Chris:

     

    By doing just what you are doing: posting info on the Arduino community site. Just one word of caution: don't run an ad and do not link to commercial sites. Otherwise you are good to go.

     

    GS

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • chrisbaron
    chrisbaron over 15 years ago in reply to GardenState

    Hi,

     

    Just to be clear we want to submit them for consideration for inclusion in the Newark/Farnell catalog.  Are you saying posting the announcement here is sufficient for that?