Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Have a question about Arduino? Ask me!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1914 replies
  • Subscribers 527 subscribers
  • Views 70191 views
  • Users 0 members are here
  • jeremy_blum
  • expert
  • student
  • arduino
Related

Have a question about Arduino? Ask me!

sciguy14
sciguy14 over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Questionabout Arduino in the element14 Community Arduino group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


image

Jeremy Blum

Jeremy is an Electrical and Computer Engineering Student at Cornell University. He has been building microcontroller projects since high school, from a prototype prosthetic hand with a novel control scheme, to a nerf gun that fires at the intruders and uploads their picture to the web.
  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to e14 Contributor +2
    @Brendan Your video is somewhat adequate for the intended purpose, however, from an engineer's point of view it is lacking in providing pertinent facts. Such as the part number, data sheet, and source…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Jeremy, thanks for your intro videos. I am just getting started myself in Arduino though I have done some simple electronics projects using Atmel chips. Here is an example using ATTiny13 chips. www.youtube…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi Jeremy I've built a device (see picture) with an Arduino and Ethernet shield that connects to our Network Monitor (Nagios) and moves an arrow to indicate if any of the computers we monitor are not responding…
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Jeremy. Im new to arduino technology and I want to embark myself upon a project.

    I want to read the data from two accelerometers(x,y coordinates) and send this data wirelessly to an arduino board. I currently have two solutions:

     

    1) One solution is to attach attach an Arduino to the object, and using an XBee shield to send data  from the accelerometer to another Arduino (or desktop machine)

    2) Another solution proposed by a fellow engineer was to connect the accelerometers to an XBee antenna,

    then having your Arduino paired with an XBee shield to receive data. Is that possible?

     

    I personally like solution number 2 the most because space is an issue in this project.

    Do you think there is a better approach to this problem? What advise would you give me?

     

    2) What arduino board do you suggest I should buy first in order to start developing this project. I have seen many arduino

    boards, but im unsure which one to buy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Jeremy. Im new to arduino technology and I want to embark myself upon a project.

    I want to read the data from two accelerometers(x,y coordinates) and send this data wirelessly to an arduino board. I currently have two solutions:

     

    1) One solution is to attach attach an Arduino to the object, and using an XBee shield to send data  from the accelerometer to another Arduino (or desktop machine)

    2) Another solution proposed by a fellow engineer was to connect the accelerometers to an XBee antenna,

    then having your Arduino paired with an XBee shield to receive data. Is that possible?

     

    I personally like solution number 2 the most because space is an issue in this project.

    Do you think there is a better approach to this problem? What advise would you give me?

     

    2) What arduino board do you suggest I should buy first in order to start developing this project. I have seen many arduino

    boards, but im unsure which one to buy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • sciguy14
    sciguy14 over 15 years ago in reply to e14 Contributor

    Which board you get depends mostly on the space you have available.  You'll need to choose a balance between features and physcal size.  Using the XBee alone would be a good solutions ,since you wouldn't need an arduino on both ends that way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to sciguy14

    IF i only use te Xbee antenna hooked up to the accelerometer, is there a speacial  program for the Xbee to display the data on the computer?

    what programming language would i be using to write te software i need for tis system? (i know java, c, c++)

     

    2) can i use an accelerometer to measure the force applied to a surface? ( i know there are force/pressure sensors but I'm trying to use few hardware components)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago in reply to e14 Contributor

    XBees have the ability to transmit signals from a few digital I/O lines.  You would just need to feed those same lines into an arduino on the receiving end, then hook that arduino up to the computer via serial.  You can write the computer software in any programming language that can talk to a serial port.

     

    I can't think of a way to use an accelerometer to measure surface force.