Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Have a question about Arduino? Ask me!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1914 replies
  • Subscribers 527 subscribers
  • Views 69664 views
  • Users 0 members are here
  • jeremy_blum
  • expert
  • student
  • arduino
Related

Have a question about Arduino? Ask me!

sciguy14
sciguy14 over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Questionabout Arduino in the element14 Community Arduino group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


image

Jeremy Blum

Jeremy is an Electrical and Computer Engineering Student at Cornell University. He has been building microcontroller projects since high school, from a prototype prosthetic hand with a novel control scheme, to a nerf gun that fires at the intruders and uploads their picture to the web.
  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to e14 Contributor +2
    @Brendan Your video is somewhat adequate for the intended purpose, however, from an engineer's point of view it is lacking in providing pertinent facts. Such as the part number, data sheet, and source…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Jeremy, thanks for your intro videos. I am just getting started myself in Arduino though I have done some simple electronics projects using Atmel chips. Here is an example using ATTiny13 chips. www.youtube…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi Jeremy I've built a device (see picture) with an Arduino and Ethernet shield that connects to our Network Monitor (Nagios) and moves an arrow to indicate if any of the computers we monitor are not responding…
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Jeremy

     

    I've built a device (see picture) with an Arduino and Ethernet shield that connects to our Network Monitor (Nagios) and moves an arrow to indicate if any of the computers we monitor are not responding. It all works fine, and I'd like to re-build it as a more finished product. I can build an Arduino on stripboard, but I can't find anywhere that describes how to make build an ethernet shield. Do you now I can build one which I can put on the same stripboard as the Arduino?

     

    Thanks

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    as the ENC chip now has a comparable library with the WIZnet chip, your code should run on either which means...

     

    this should work along with the standard support components ENC28J60-I/SP - MICROCHIP ENC28J60-I/SP - IC, ENET CTRL, IEEE 802.3, 10MBPS, DIP28 | Newark element14 Canada

     

    the library is available here https://github.com/ntruchsess/arduino_uip

     

    or you can purchase a small an inexpensive 28J60 board with a header (10pin or 8pin options available) for a few dollars and simply use pin strips to adapt to the strip board

     

    here ENC28J60 Ethernet LAN Module | eBay or simply google "ENC28J60", there are loads of options and i is easy to us

     

    ENC chip is far cheaper than the WIZNet providing you have the memory for the library

    Have fun

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    as the ENC chip now has a comparable library with the WIZnet chip, your code should run on either which means...

     

    this should work along with the standard support components ENC28J60-I/SP - MICROCHIP ENC28J60-I/SP - IC, ENET CTRL, IEEE 802.3, 10MBPS, DIP28 | Newark element14 Canada

     

    the library is available here https://github.com/ntruchsess/arduino_uip

     

    or you can purchase a small an inexpensive 28J60 board with a header (10pin or 8pin options available) for a few dollars and simply use pin strips to adapt to the strip board

     

    here ENC28J60 Ethernet LAN Module | eBay or simply google "ENC28J60", there are loads of options and i is easy to us

     

    ENC chip is far cheaper than the WIZNet providing you have the memory for the library

    Have fun

     

    Peter