Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Have a question about Arduino? Ask me!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1914 replies
  • Subscribers 527 subscribers
  • Views 69626 views
  • Users 0 members are here
  • jeremy_blum
  • expert
  • student
  • arduino
Related

Have a question about Arduino? Ask me!

sciguy14
sciguy14 over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Questionabout Arduino in the element14 Community Arduino group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


image

Jeremy Blum

Jeremy is an Electrical and Computer Engineering Student at Cornell University. He has been building microcontroller projects since high school, from a prototype prosthetic hand with a novel control scheme, to a nerf gun that fires at the intruders and uploads their picture to the web.
  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to e14 Contributor +2
    @Brendan Your video is somewhat adequate for the intended purpose, however, from an engineer's point of view it is lacking in providing pertinent facts. Such as the part number, data sheet, and source…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Jeremy, thanks for your intro videos. I am just getting started myself in Arduino though I have done some simple electronics projects using Atmel chips. Here is an example using ATTiny13 chips. www.youtube…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi Jeremy I've built a device (see picture) with an Arduino and Ethernet shield that connects to our Network Monitor (Nagios) and moves an arrow to indicate if any of the computers we monitor are not responding…
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hello,

    I`m new to arduino, but I`m willing to use it (love open-source). I already used Microship PIC thought. I wanted to know about the feasability of a solar tracker with an arduino.

    -What kind of motor can I control with (with which additionnal board?) I`m thinking about a single stepper motor, do I need additional board?

    -I`m thinking of putting a form of communication as an "extra", ex. : can I communicate through the USB port inside my program? Is there a library? Or should I better use an ethernet shield? Then would it be easy to get the hour from the internet with this?

    -To follow the sun, should I better follow it with some photodiodes, or a GPS+compass, or get hour from internet and calculate with the latitude+longitude?

    -Will I have enough I/O for all this, enough "room" for my code... or should I go for something bigger like the arduino mega?

    This solar tracker wil be something small, more as a demo project than something big and generating lots of power. I`m quite new to solar things, and don`t know where to start. Any clue appreciated. Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago in reply to e14 Contributor

    Hey there!

     

    This certainly sounds possible with an arduino, and I don't even think you would need the mega.  You should be able to control a standard stepper motor with the arduino using only a darlington transistor array.  An entire stepper control board shouldn't be necessary for just one stepper.  Serial communication over USB with the arduino is easy.  In Tutorial 06 for Arduino: Serial Communication and Processing I explained how you can use it to send data from the arduino to a display on your computer.  Using an ethernet shield would work equally well.  The advantage of using an ethernet shield would be that bi-directional communication from the web would be easier.  This can also be achieved using a USB Serial connection and a helper program running on the computer (See a video where I did that here: http://www.youtube.com/watch?v=y7vSyxLAtxI). I think the most accurate way to follow the sun would be to use latitude/longitude data plus information from the web.  Photodiodes wouldn't be accurate enough, and GPS modules are expensive and unecessary if you don't plan to move this around too much.

     

    Let me know if that helps, and if you need any further advice.  Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • sciguy14
    sciguy14 over 15 years ago in reply to e14 Contributor

    Hey there!

     

    This certainly sounds possible with an arduino, and I don't even think you would need the mega.  You should be able to control a standard stepper motor with the arduino using only a darlington transistor array.  An entire stepper control board shouldn't be necessary for just one stepper.  Serial communication over USB with the arduino is easy.  In Tutorial 06 for Arduino: Serial Communication and Processing I explained how you can use it to send data from the arduino to a display on your computer.  Using an ethernet shield would work equally well.  The advantage of using an ethernet shield would be that bi-directional communication from the web would be easier.  This can also be achieved using a USB Serial connection and a helper program running on the computer (See a video where I did that here: http://www.youtube.com/watch?v=y7vSyxLAtxI). I think the most accurate way to follow the sun would be to use latitude/longitude data plus information from the web.  Photodiodes wouldn't be accurate enough, and GPS modules are expensive and unecessary if you don't plan to move this around too much.

     

    Let me know if that helps, and if you need any further advice.  Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to sciguy14

    Thank you for all these good advices! I`ll look at it, and see if I feel confident enough to start it. I`ll look at your suggestions, but this seems to make sense. Thank you!