Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Have a question about Arduino? Ask me!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1914 replies
  • Subscribers 527 subscribers
  • Views 69894 views
  • Users 0 members are here
  • jeremy_blum
  • expert
  • student
  • arduino
Related

Have a question about Arduino? Ask me!

sciguy14
sciguy14 over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Questionabout Arduino in the element14 Community Arduino group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


image

Jeremy Blum

Jeremy is an Electrical and Computer Engineering Student at Cornell University. He has been building microcontroller projects since high school, from a prototype prosthetic hand with a novel control scheme, to a nerf gun that fires at the intruders and uploads their picture to the web.
  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to e14 Contributor +2
    @Brendan Your video is somewhat adequate for the intended purpose, however, from an engineer's point of view it is lacking in providing pertinent facts. Such as the part number, data sheet, and source…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Jeremy, thanks for your intro videos. I am just getting started myself in Arduino though I have done some simple electronics projects using Atmel chips. Here is an example using ATTiny13 chips. www.youtube…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi Jeremy I've built a device (see picture) with an Arduino and Ethernet shield that connects to our Network Monitor (Nagios) and moves an arrow to indicate if any of the computers we monitor are not responding…
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    I forgot to mention that with an Arduino, you can contrly MOSFETs to drive the stepper motor directly, sorry!!

    Maybe someone has already developed code that you can use or adapt.

    As your motor has 4 connections, that is a BIPOLAR Stepper Motor. Not a Unipolar!!! Never forget that!!

    Its easy to identify both coils simply by using an Ohmeter on Ohms. Each coil will have two connections, label them coil A and coil B. If the motor ever drives the "wrong" direction, you only need to reverse the connections to ONE COIL ONLY!

    Sorry that I forgot so much.....

    regards

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago in reply to e14 Contributor

    Yes, Andrew is correct.  Referring to this diagram might help you understand better: http://www.robotgear.com.au/Cache/Files/ProductImageOriginals/679_Bipolar%20stepper%20motor%20wiring%20diagram.jpg  You can use the continuity function of a multimeter to identify the wires.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to sciguy14

    Im actually trying to follow this instructible: http://www.instructables.com/id/Pocket-laser-engraver/ this is my first project with an Arduino or any type of a micro controller but i thought it would be a good prelude to building a full size cnc router, anyways i can identify the two seperate coils on the motor but how do i know which is contact is a, c, d, b? i tried applying voltage (first 3.5 V then 5V) to each one of the coils but i got no movement out of them, also i thought that dvd drives run or 5v instead of 12v so i will try applying 12v tomorrow, if it burns out then too bad i can always salvage another motor out of a different drive. I was also think about just running some g code to the controllers so it would be constantly putting out a signal to the motor and breadboarding my easy driver so i could easly plug in the wires from the motor and just try different combinations im just afraid of damaging the driver board so please let me know if thats a bad idea. i will try to get  apicture of my motor as soon as my camera charger comes in as i lost it on vacations and my battery died compleatly, once again thanks for all the great help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Stepper motors ONLY understand a complex sequence of pulses, on one or the other coils in either of two directions, you cannot drive them with DC power!! You may just burn out a coil and destroy the motor completely.....

     

    TIP. Never apply power to something you don't understand.......it can even be dangerous to you personally, but not in this case, it was only dangerous to the motors......

     

    There are no contacts in a stepper motor.

     

    A picture is unlikely to help further.

     

    Look for tutorials and the like on the web, read before proceeding further.....

     

    Best wishes.

     

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi, what is the   pin number ATMEGA328P-PUATMEGA328P-PU  input power, and ground, I have connect output 0 led positive, and ground negative, how connect correct wire to atmega's pins?, final led blinked.

    Thanks for answer

    Bye

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tronixstuff
    tronixstuff over 15 years ago in reply to e14 Contributor

    You should download yourself an Arduino board schematic so you can see what goes where.The design files (.pdf and Eagle) can be downloaded from here:

    http://arduino.cc/en/Main/ArduinoBoardUno

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi,

    I was wondering if there is a way to use a barcode scanner to display the information using an arduino to a lcd screen. W/O using a computer.

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hello, I have an Arduino Uno and would like to get advice on the following project: I would like to control two DC motors so they have the same speed. I'm thinking about using Hall sensors to measure RPM, but perhaps there are other ways? The control needs to be in the area of 3600 RPM each motor.

     

    Thanks, Flywheel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    What program would I use to open an .sch file downloaded via Jeremy Blum's arduino tutorials?

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago in reply to e14 Contributor

    That sounds possible.  You could use this (http://www.sparkfun.com/products/9166) on a device with USB host support, such as the chipKIT arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>