Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Have a question about Arduino? Ask me!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1914 replies
  • Subscribers 527 subscribers
  • Views 69940 views
  • Users 0 members are here
  • jeremy_blum
  • expert
  • student
  • arduino
Related

Have a question about Arduino? Ask me!

sciguy14
sciguy14 over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Questionabout Arduino in the element14 Community Arduino group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


image

Jeremy Blum

Jeremy is an Electrical and Computer Engineering Student at Cornell University. He has been building microcontroller projects since high school, from a prototype prosthetic hand with a novel control scheme, to a nerf gun that fires at the intruders and uploads their picture to the web.
  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to e14 Contributor +2
    @Brendan Your video is somewhat adequate for the intended purpose, however, from an engineer's point of view it is lacking in providing pertinent facts. Such as the part number, data sheet, and source…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Jeremy, thanks for your intro videos. I am just getting started myself in Arduino though I have done some simple electronics projects using Atmel chips. Here is an example using ATTiny13 chips. www.youtube…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi Jeremy I've built a device (see picture) with an Arduino and Ethernet shield that connects to our Network Monitor (Nagios) and moves an arrow to indicate if any of the computers we monitor are not responding…
  • sciguy14
    sciguy14 over 15 years ago in reply to e14 Contributor

    Hall sensors or optical encoders are probably a good bet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago in reply to e14 Contributor

    Eagle CAD.  You can grab it here: http://www.cadsoftusa.com/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • misterwalrus
    misterwalrus over 15 years ago

    Thank you very much for your help. It is very much appreciated.

    I am planning a new project and andruino looks promising. I need to capture 24 bits every 15 ms and send it to the PC. I was looking at the Uno and the Mega models and I can decide which one to use.

    Please advise,

    Best regards,

    Andres

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tronixstuff
    tronixstuff over 15 years ago in reply to e14 Contributor

    Cadsoft Eagle -  http://www.cadsoftusa.com/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago in reply to misterwalrus

    Either one should work fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Jeremy,

    I have a fresh 13.37 x64 system and trying to compile some avr code. When I try to compile I get the following error ;

    /usr/lib/gcc/avr/4.4.4/avr5/libc.a: could not read symbols: File format not recognized

    Actually there were bunch of errors like ;


    /usr/lib/gcc/avr/4.4.4/../../../../avr/bin/ld: skipping incompatible  /usr/lib/gcc/avr/4.4.4/../../../../avr/lib/avr5/libm.a when searching  for -lm
    /usr/lib/gcc/avr/4.4.4/../../../../avr/bin/ld: skipping incompatible  /usr/lib/gcc/avr/4.4.4/../../../../avr/lib/libm.a when searching for -lm
    /usr/lib/gcc/avr/4.4.4/../../../../avr/bin/ld: cannot find -lm
    /usr/lib/gcc/avr/4.4.4/../../../../avr/bin/ld: skipping incompatible  /usr/lib/gcc/avr/4.4.4/avr5/libgcc.a when searching for -lgcc
    /usr/lib/gcc/avr/4.4.4/../../../../avr/bin/ld: skipping incompatible /usr/lib/gcc/avr/4.4.4/libgcc.a when searching for -lgcc
    /usr/lib/gcc/avr/4.4.4/../../../../avr/bin/ld: cannot find -lgcc
    /usr/lib/gcc/avr/4.4.4/../../../../avr/bin/ld: skipping incompatible  /usr/lib/gcc/avr/4.4.4/../../../../avr/lib/avr5/libc.a when searching  for -lc
    /usr/lib/gcc/avr/4.4.4/../../../../avr/bin/ld: skipping incompatible  /usr/lib/gcc/avr/4.4.4/../../../../avr/lib/libc.a when searching for -lc
    /usr/lib/gcc/avr/4.4.4/../../../../avr/bin/ld: cannot find -lc
    /usr/lib/gcc/avr/4.4.4/../../../../avr/bin/ld: skipping incompatible  /usr/lib/gcc/avr/4.4.4/avr5/libgcc.a when searching for -lgcc
    /usr/lib/gcc/avr/4.4.4/../../../../avr/bin/ld: skipping incompatible /usr/lib/gcc/avr/4.4.4/libgcc.a when searching for -lgcc
    /usr/lib/gcc/avr/4.4.4/../../../../avr/bin/ld: cannot find -lgcc

    and I copied the 64bit versions of the libraries to destination folders  and got rid of all the errors except that I am stuck at libc.a couldn't  read symbols.

    So I am asking you, any help is appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    which ardunio suitable for low power energy harbvesting from solar/wind/others  and can be connected to  Near Field Communication  (NFC) or RFID

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Jeremy. Im new to arduino technology and I want to embark myself upon a project.

    I want to read the data from two accelerometers(x,y coordinates) and send this data wirelessly to an arduino board. I currently have two solutions:

     

    1) One solution is to attach attach an Arduino to the object, and using an XBee shield to send data  from the accelerometer to another Arduino (or desktop machine)

    2) Another solution proposed by a fellow engineer was to connect the accelerometers to an XBee antenna,

    then having your Arduino paired with an XBee shield to receive data. Is that possible?

     

    I personally like solution number 2 the most because space is an issue in this project.

    Do you think there is a better approach to this problem? What advise would you give me?

     

    2) What arduino board do you suggest I should buy first in order to start developing this project. I have seen many arduino

    boards, but im unsure which one to buy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Jeremy, thanks for being such a great resource...I am a complete newbie but wanting to learn fast. My project is to take the voltage measurements (0 to 2 VDC) from two distinct sensors and use a look-up table that I have for these sensors to convert them to temperature readings, and then display the temps on an LCD (at a later date would like to access them through the internet if that is possible). How do I do all this? How do I enter the look-up table? How do I display the temperatures? Can I store these temp and download at a later time?

    If this is too simple, pls direct me to another site as not to be a nuisance.

    Thanks for your help.

    Regards,
    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wb8nbs
    wb8nbs over 15 years ago in reply to e14 Contributor

    What is the temp sensor you are using?  Most of them are linear and you can calculate the temperature very simply from the voltage read rather than use a lookup table. For storage and later retrieval, Arduino has a 512 byte EEPROM you should be able to store a hundred readings in that.  See the EEPROM library on the Arduino site.

     

    Here is some code you can study from a class I took. It reads from a TMP36 sensor and sends the reading to both serial and a parallel LCD.

     

    /* Sensor test sketch
      for more information see http://www.ladyada.net/make/logshield/lighttemp.html
      */

     

    #define aref_voltage 3.3         // we tie 3.3V to ARef and measure it with a multimeter!

     

    // include the LCD library code:
    #include <LiquidCrystal.h>
    // initialize the LCD library with the numbers of the interface pins
    LiquidCrystal lcd(12, 11, 5, 4, 3, 2);

     


    //TMP36 Pin Variables
    int tempPin = A1;        //the analog pin the TMP36's Vout (sense) pin is connected to
                            //the resolution is 10 mV / degree centigrade with a
                            //500 mV offset to allow for negative temperatures
    int tempReading;        // the analog reading from the sensor

     

    void setup(void) {
      // We'll send debugging information via the Serial monitor
      Serial.begin(9600);
       lcd.begin(16, 2);  // for debug
      // If you want to set the aref to something other than 5v
      analogReference(EXTERNAL);
    }

     


    void loop(void) {

     

      tempReading = analogRead(tempPin);

     

      Serial.print("Temp reading = ");
      Serial.print(tempReading);     // the raw analog reading

     

      // converting that reading to voltage, which is based off the reference voltage
      float voltage = tempReading * aref_voltage;
      voltage /= 1024.0;

     

      // print out the voltage
      Serial.print(" - ");
      Serial.print(voltage); Serial.println(" volts");

     

      // now print out the temperature
      float temperatureC = (voltage - 0.5) * 100 ;  //converting from 10 mv per degree wit 500 mV offset
                                                   //to degrees ((volatge - 500mV) times 100)
      Serial.print(temperatureC); Serial.println(" degress C");
      lcd.clear();
    lcd.print(temperatureC);

     

      // now convert to Fahrenheight
      float temperatureF = (temperatureC * 9.0 / 5.0) + 32.0;
      Serial.print(temperatureF); Serial.println(" degress F");
      lcd.setCursor(0,1);
    lcd.print(temperatureF);
      delay(1000);
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>