Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Have a question about Arduino? Ask me!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1914 replies
  • Subscribers 527 subscribers
  • Views 69683 views
  • Users 0 members are here
  • jeremy_blum
  • expert
  • student
  • arduino
Related

Have a question about Arduino? Ask me!

sciguy14
sciguy14 over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Questionabout Arduino in the element14 Community Arduino group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


image

Jeremy Blum

Jeremy is an Electrical and Computer Engineering Student at Cornell University. He has been building microcontroller projects since high school, from a prototype prosthetic hand with a novel control scheme, to a nerf gun that fires at the intruders and uploads their picture to the web.
  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to e14 Contributor +2
    @Brendan Your video is somewhat adequate for the intended purpose, however, from an engineer's point of view it is lacking in providing pertinent facts. Such as the part number, data sheet, and source…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Jeremy, thanks for your intro videos. I am just getting started myself in Arduino though I have done some simple electronics projects using Atmel chips. Here is an example using ATTiny13 chips. www.youtube…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi Jeremy I've built a device (see picture) with an Arduino and Ethernet shield that connects to our Network Monitor (Nagios) and moves an arrow to indicate if any of the computers we monitor are not responding…
  • sciguy14
    sciguy14 over 15 years ago in reply to billabott

    It's likely possible, but you'll need to use a scope or a logic analyzer to reverse engineer the control signal for the lcd.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago in reply to Ikana

    Yes, send data to the computer via serial, and use just about any programming language on the computer to interpret it and generate video.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to sciguy14

    Here's a link to all of Newark's LED dot matrices:

     

    http://www.newark.com/jsp/search/browse.jsp?N=500003+1003830&Ntk=gensearch_001&Ntt=LED+matrix&Ntx=mode+matchallpartial

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    how can i make a pcb design?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 15 years ago in reply to e14 Contributor

    The most populare seems to be Eagle Cad, http://cadsoftusa.com/ which is free download.

     

    I prefer Pad2Pad however - http://www.pad2pad.com/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • simon.monk
    simon.monk over 15 years ago in reply to R_Phoenix

    I have not tried Pad2Pad, but Eagle CAD is very good. It also works on Macs as well as Windows.

     

    IMHO, its also very strange to use. It doesn't really obey any of the mouse / menu / drawing conventions that we are so used to on our PCs. So, buy a book about it and accept that it will take a good few hours of not doing anything productive with it, before you understand what's going on.

     

    Si.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago in reply to simon.monk

    I use eagle cad, and agree that the interface can be a little weird.  Sparkfun has some excellent tutorials on using it though.  http://www.sparkfun.com/tutorials/109

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Jeremy, what IC's would you recommend for novices needing multiplexing/demultiplexing? I'm only after 8 lines the now but expandability would be nice.

     

    Also, I was reading the datasheet for the 74AC138 decoder/demultiplexor. It says it "can be used as an 8-output demultiplexer by using one of the active LOW Enable inputs as the data input and the other Enable     
    inputs as strobes." Can you clarify what it means by strobes? Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    If I want to import some external signal on the built-in DFIG model in simulink(Phasor Simulation of a Wind Farm Using Doubly-Fed Induction Generator Wind Turbines). such as other generators (call generator A)  of the rotation speed (wr),the value should be put 1pu ..However, in the dfig (only connect to the oscilloscope in DFIG), signal value, become 0pu, also, it affects the rotor speed of generator A, the speed becomes to 0 pu , if i disconnect the connnection of DFIG,, then the rotor speed in generator A will return to 1pu. DFIG model block/absort the signal ? or what?. please help. Thank you.

    Attachments:
    image
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hello,

    thank you for your interesting and very useful tutorials especually for the beginners like me.

    I got a question: Have you ever used Arduino with Max/MSP(or Arduino + Processing + Max/Msp/Jitter )?

    If yes, then could you upload some of the examples? I would love to see it in one of your next tutorials.

    Thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>