Arduino
  • Products
  • More
Arduino
Arduino Forum Servos and coding
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 417 subscribers
  • Views 753 views
  • Users 0 members are here
  • coding
  • tutorial
  • maker
  • arduino_month
  • openhardware
  • rotation
  • help
  • hardware
  • animatronic
  • robots
  • delay
  • robot
  • make
  • led
  • Design
  • servo
  • prototyping
  • code
  • platform
  • arduino_development_environment
  • engineering
  • arm
  • electrical
  • motor
  • arduino
  • hand
  • opensource
Related

Servos and coding

dirtdiver
dirtdiver over 15 years ago

Hi, so I'm new to the Arduino, I've done only one project so far and now -with my second..I ran into some trouble-

 

I am tring to make my robot arm do  something repeatedly - like a Factory robotic arm - assembling stuff.The problem is that I have 2 servos on 1 axis and I cant make them rotate at the same direction. here's the code I made (I used the library)

 

void loop()
{
  for(pos = 0; pos < 180; pos += 1)

  {                                  
    myservo.write(pos);
    myservo1.write(pos);           
    delay(15);                     
  }

}

 

how to reverse one of them?

 

also this wont work at all :

 


void loop()
{
 

  myservo.write(90);

   
  myservo1.write(90);
    
  myservo.write(0);
 
  myservo1.write(0);
 
}

 

and when I add the delay it works but not at the same time.

 

Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • cookieglitch
    cookieglitch over 15 years ago

    Reversing them is just a matter of switching the values around and decrementing rather than incrementing. As such, it will look something like:

     

     

    void loop ()
    {
         for(int pos=180; pos > 0; pos--)
         {
              myservo.write(pos);
              myservo1.write(pos);
              delay(15);
         }
    }

     

    For your other piece of code, it may be worth inserting a delay between each statement. Telling a servo to move to a position takes a small amount of time and as a result will not happen at the same time, there will always be a little delay between the two. This is why on the example code, it has delay(15) after each write.

     

    Hope this helps!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cookieglitch
    cookieglitch over 15 years ago

    Reversing them is just a matter of switching the values around and decrementing rather than incrementing. As such, it will look something like:

     

     

    void loop ()
    {
         for(int pos=180; pos > 0; pos--)
         {
              myservo.write(pos);
              myservo1.write(pos);
              delay(15);
         }
    }

     

    For your other piece of code, it may be worth inserting a delay between each statement. Telling a servo to move to a position takes a small amount of time and as a result will not happen at the same time, there will always be a little delay between the two. This is why on the example code, it has delay(15) after each write.

     

    Hope this helps!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dirtdiver
    dirtdiver over 15 years ago in reply to cookieglitch

    well I want the servos doing this:

     

    servo 1 - from 0 to 180

    servo 2 -from 180 to 0

    no delay between them

     

    what would that look like?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cookieglitch
    cookieglitch over 15 years ago in reply to dirtdiver

    I would use something like this. Having no delay is relatively hard to do due to the write delays. PWM sadly isn't an instant thing. The best you can hope for (Without having a fancy distributed system) is reducing it to a tiny display that you won't notice too much.

     

    void loop()
    {
         int pos = 0; //Number of times the loop has run
         int serPos1 = 0; //Position of servo1
         int serPos2 = 180; //Position of servo2
    
         while(pos < 180)              //While the loop has been done less than 180 times...
         {
              myservo.write(serPos1);
              myservo1.write(serPos2);
              serPos1++;               //Increment position of servo1
              serPos2--;               //Decrement position of servo2
              pos++;                   //Increment loop counter.
    
              delay(15);               //Write delay. Can always try without, but no guarantees it would work
         }
    }

     

    This is by no means the only way to do it, but should give you an idea.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 15 years ago in reply to cookieglitch

    Thanks for the idea! I will try that.