Arduino
  • Products
  • More
Arduino
Arduino Forum Randomisation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 418 subscribers
  • Views 746 views
  • Users 0 members are here
  • tutorial
  • open-source
  • help
  • up
  • robot
  • light
  • slamman
  • led
  • random
  • engineering
  • order
  • electrical
  • no
  • arduino
Related

Randomisation

dirtdiver
dirtdiver over 15 years ago

Hi everyone, my question is simple-I have two LED-s hooked up to the arduino and I want them to light up one at a time, but without order.

 

I'm trying to make something like the SlamMan

image

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    You might be able to use one of the pins as an analog pin, have it be a floating pin (nothing attached) and read the value of that pin. Since it is floating, you might get a pretty random value, which you can then use to determine if you want the LEDs on or off, or use two pins for two "random" sources. It could also be that depending on how the analog to digital conversion works, this may not be useful at all, that is you might get 1 sudo-random read, and then 0 for the rest. Just a thought. Don't know if it would work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 15 years ago in reply to e14 Contributor

    this might work, but I want to add delay (one led lights up for 1sec, then the other one-for 1 sec...)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to dirtdiver

    A quick google search gives me this code:

     

    long randNumber;
    
    void setup(){
      Serial.begin(9600);
    
      // if analog input pin 0 is unconnected, random analog
      // noise will cause the call to randomSeed() to generate
      // different seed numbers each time the sketch runs.
      // randomSeed() will then shuffle the random function.
      randomSeed(analogRead(0));
    }
    
    void loop() {
      // print a random number from 0 to 299
      randNumber = random(300);
      Serial.println(randNumber);  
    
      // print a random number from 10 to 19
      randNumber = random(10, 20);
      Serial.println(randNumber);
    
      delay(50);
    }
    
    

    from http://www.arduino.cc/en/Reference/Random

     

    You should be able to use that to easily rig up a randomiser for lighting LEDs..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    That's a much better idea.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vivamort
    vivamort over 14 years ago

    There is a library function called TrueRandom for the arduino which I used in my last project. Its using the same principle but with a lot more bits rather than a single value like above so should be more random in results. a Quick google search will find it. You can then use the randomizer as an offset for the delay to create any time delays you wish.