Arduino Forum Activating Servos Simultaneously
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
  • Replies 13 replies
  • Subscribers 396 subscribers
  • Views 2215 views
  • Users 0 members are here
Related

Activating Servos Simultaneously

Former Member
Former Member over 9 years ago

Hello...I need help...and I don't think it is a difficult issue, but I just can't seem to get it yet.

 

I am trying to push a button that makes a servo move 90 degrees for 10 seconds, then turn back. I have this working fine. The problem happens when I try to do this for more than one servo.

 

I can make it work for two servos, but not while the first one is still counting off its 10 second period.

 

Here is my code...CAN SOMEONE GUIDE ME TO A SOLUTION?

 

/*

  SweepTwoServos

  By Philip van Allen <philvanallen.com> for the VarSpeedServo.h library (October 2013)

  This example code is in the public domain

*/

 

#include <VarSpeedServo.h>

 

VarSpeedServo myservo_1;            // create servo object to control a servo

VarSpeedServo myservo_2;            //a maximum of eight servo objects can be created

 

const int servoPin1 = 9;                     // the digital pin used for the first servo

const int servoPin2 = 10;                     // the digital pin used for the second servo

 

unsigned long startTime_1 = 0;     // will store last time servo was opened

unsigned long startTime_2 = 0;     // will store last time servo was opened

int valveOpenPeriod_1 = 10000;    // sets the period the servo should be opened - 10 seconds

int valveOpenPeriod_2 = 5000;     // sets the period the servo should be opened - 5 seconds

 

void setup() {

  myservo_1.attach(servoPin1);  // attaches the servo on pin 9 to the servo object

  myservo_1.write(90,30,false);  // set the intial position of the servo, move slowly, run in background

  myservo_2.attach(servoPin2);  // attaches the servo on pin 10 to the servo object

  myservo_2.write(90,30,false);  // set the intial position of the servo, move slowly, run in background

}

 

void loop()

{

  unsigned long currentMillis = millis(); // start counting

 

  if(digitalRead(3) == HIGH)              // if inflation button is pushed

  {   

    startTime_1 = currentMillis;          // reset start time to current time

    while(millis() - startTime_1 < valveOpenPeriod_1)

    {

      myservo_1.write(180,30,false);   // tell servo to go to position 180 to open valve

      delay(10);                                    // waits 10ms for the servo to reach the position

    }

     myservo_1.write(90,30,false);     // tell servo to go to back to original position 90 to close valve

     delay(10);                                    // waits 10ms for the servo to reach the position

  }

 

/* THE PROBLEM

The two blocks of code, one above and one below, work independently but not simultaneously.

How do I get them to work simultaneously. In other words, I need each servo to move 90 degrees

for a period of time, then move back to its original position. I need this to work for

each servo whenever I press the putton.

*/

 

  if(digitalRead(5) == HIGH)              // if inflation button is pushed

  {   

    startTime_2 = currentMillis;           // reset start time to current time

    while(millis() - startTime_2 < valveOpenPeriod_2)

    {

      myservo_2.write(180,127,true);   // tell servo to go to position 180 to open valve

      delay(10);                               // waits 10ms for the servo to reach the position

    }

     myservo_2.write(90,127,true);    // tell servo to go to position 90 to close valve

     delay(10);                               // waits 10ms for the servo to reach the position

  }

}

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +3
    So everyone is saying the right words but to help you categorically (But you will still have to read and learn as im not giving you a direct solution ) https://www.arduino.cc/en/Tutorial/BlinkWithoutDelay…
  • shabaz
    shabaz over 9 years ago +2
    Hi Remo, As John says, typically expect one processor to do one thing at a time. There are methods to make it appear that multiple things are occurring at the same time, but you need to structure your…
  • neilk
    neilk over 9 years ago +1
    Hi Remo, have a look here: http://www.doctormonk.com/2012/01/arduino-timer-library.html This describes a timer library which allows the arduino to perform tasks at different time intervals, without "blocking…
Parents
  • mudz
    mudz over 9 years ago

    Well you can't do it with arduino but there are other microcontrollers which are capable of performing such tasks i.e. have multitasking capabilities with less coding. For example: check this :XK-STK-A8DEV XK-STK-A8DEV

    It's a basic development kit by XMOS i.e. Xmos startkit & features a multitasking microcontroller. If you take a look at its code you'll understand how easy is to do : XMOS startkit basic Multitasking code

    Hope this helps image

     

    mudz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mudz
    mudz over 9 years ago

    Well you can't do it with arduino but there are other microcontrollers which are capable of performing such tasks i.e. have multitasking capabilities with less coding. For example: check this :XK-STK-A8DEV XK-STK-A8DEV

    It's a basic development kit by XMOS i.e. Xmos startkit & features a multitasking microcontroller. If you take a look at its code you'll understand how easy is to do : XMOS startkit basic Multitasking code

    Hope this helps image

     

    mudz