Arduino Forum Activating Servos Simultaneously
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
  • Replies 13 replies
  • Subscribers 396 subscribers
  • Views 2220 views
  • Users 0 members are here
Related

Activating Servos Simultaneously

Former Member
Former Member over 9 years ago

Hello...I need help...and I don't think it is a difficult issue, but I just can't seem to get it yet.

 

I am trying to push a button that makes a servo move 90 degrees for 10 seconds, then turn back. I have this working fine. The problem happens when I try to do this for more than one servo.

 

I can make it work for two servos, but not while the first one is still counting off its 10 second period.

 

Here is my code...CAN SOMEONE GUIDE ME TO A SOLUTION?

 

/*

  SweepTwoServos

  By Philip van Allen <philvanallen.com> for the VarSpeedServo.h library (October 2013)

  This example code is in the public domain

*/

 

#include <VarSpeedServo.h>

 

VarSpeedServo myservo_1;            // create servo object to control a servo

VarSpeedServo myservo_2;            //a maximum of eight servo objects can be created

 

const int servoPin1 = 9;                     // the digital pin used for the first servo

const int servoPin2 = 10;                     // the digital pin used for the second servo

 

unsigned long startTime_1 = 0;     // will store last time servo was opened

unsigned long startTime_2 = 0;     // will store last time servo was opened

int valveOpenPeriod_1 = 10000;    // sets the period the servo should be opened - 10 seconds

int valveOpenPeriod_2 = 5000;     // sets the period the servo should be opened - 5 seconds

 

void setup() {

  myservo_1.attach(servoPin1);  // attaches the servo on pin 9 to the servo object

  myservo_1.write(90,30,false);  // set the intial position of the servo, move slowly, run in background

  myservo_2.attach(servoPin2);  // attaches the servo on pin 10 to the servo object

  myservo_2.write(90,30,false);  // set the intial position of the servo, move slowly, run in background

}

 

void loop()

{

  unsigned long currentMillis = millis(); // start counting

 

  if(digitalRead(3) == HIGH)              // if inflation button is pushed

  {   

    startTime_1 = currentMillis;          // reset start time to current time

    while(millis() - startTime_1 < valveOpenPeriod_1)

    {

      myservo_1.write(180,30,false);   // tell servo to go to position 180 to open valve

      delay(10);                                    // waits 10ms for the servo to reach the position

    }

     myservo_1.write(90,30,false);     // tell servo to go to back to original position 90 to close valve

     delay(10);                                    // waits 10ms for the servo to reach the position

  }

 

/* THE PROBLEM

The two blocks of code, one above and one below, work independently but not simultaneously.

How do I get them to work simultaneously. In other words, I need each servo to move 90 degrees

for a period of time, then move back to its original position. I need this to work for

each servo whenever I press the putton.

*/

 

  if(digitalRead(5) == HIGH)              // if inflation button is pushed

  {   

    startTime_2 = currentMillis;           // reset start time to current time

    while(millis() - startTime_2 < valveOpenPeriod_2)

    {

      myservo_2.write(180,127,true);   // tell servo to go to position 180 to open valve

      delay(10);                               // waits 10ms for the servo to reach the position

    }

     myservo_2.write(90,127,true);    // tell servo to go to position 90 to close valve

     delay(10);                               // waits 10ms for the servo to reach the position

  }

}

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +3
    So everyone is saying the right words but to help you categorically (But you will still have to read and learn as im not giving you a direct solution ) https://www.arduino.cc/en/Tutorial/BlinkWithoutDelay…
  • shabaz
    shabaz over 9 years ago +2
    Hi Remo, As John says, typically expect one processor to do one thing at a time. There are methods to make it appear that multiple things are occurring at the same time, but you need to structure your…
  • neilk
    neilk over 9 years ago +1
    Hi Remo, have a look here: http://www.doctormonk.com/2012/01/arduino-timer-library.html This describes a timer library which allows the arduino to perform tasks at different time intervals, without "blocking…
Parents
  • neilk
    neilk over 9 years ago

    Hi Remo, have a look here: http://www.doctormonk.com/2012/01/arduino-timer-library.html

     

    This describes a timer library which allows the arduino to perform tasks at different time intervals, without "blocking" - ie waiting for one task to finish before it's possible to start another task.

     

    I have used this library myself and found it extremely valuable.

     

    Hope this helps

     

    Neil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to neilk

    Well, yes Neil...I think I will need to check this out...

     

    But with all your help I actually have it working...at least I have 3 servos responding to 3 pushbuttons that start their valve open period.

     

    And they do work simultaneously. Here it is...

     

    // I am using this library...

    #include <VarSpeedServo.h>

     

    // I am creating 3 servo objects

    VarSpeedServo myservo_1;

    VarSpeedServo myservo_2

    VarSpeedServo myservo_3;

     

    // 3 digital pins

    const int servoPin1 = 9;

    const int servoPin2 = 10;

    const int servoPin3 = 11;

     

    // 3 valves can be set to 3 different open time

    const long valveOpenPeriod_1 = 7000;      // 7 seconds

    const long valveOpenPeriod_2 = 5000;      // 5 seconds

    const long valveOpenPeriod_3 = 2000;      // 2 seconds

     

    // store state of 3 servos, HIGH is open

    int valveOpen_1;

    int valveOpen_2;

    int valveOpen_3;

     

    // store last time servo was open

    unsigned long startTime_1 = 0;

    unsigned long startTime_2 = 0;

    unsigned long startTime_3 = 0;

     

    // attaches servos & pins to the servo object

    void setup() {

      myservo_1.attach(servoPin1);

      myservo_2.attach(servoPin2);

      myservo_3.attach(servoPin3);

    }

     

    void loop()

    {

      unsigned long currentMillis = millis();   // start counting

     

      if(digitalRead(2) == HIGH)                    // if inflation button #1 is pushed

      {   

        startTime_1 = currentMillis;                // reset start time to current time

      } 

      if(digitalRead(3) == HIGH)

      {   

        startTime_2 = currentMillis;

      }

      if(digitalRead(4) == HIGH)

      {   

        startTime_3 = currentMillis;

      }

     

    // subtract startTime from current time and compare it to the valve period

      if(millis() - startTime_1 >= valveOpenPeriod_1)

      {

        myservo_1.write(180,30,false);        // valve opens until period is reached

      }

      else

      {

        myservo_1.write(90,30,false);           // valve closed when period reached

      }

     

    // same for valve #2

      if(millis() - startTime_2 >= valveOpenPeriod_2)

      {

        myservo_2.write(180,30,false);      

      }

      else

      {

        myservo_2.write(90,30,false); 

      }

     

    // same for valve #3

      if(millis() - startTime_3 >= valveOpenPeriod_3)

      {

        myservo_3.write(180,30,false);

      }

      else

      {

        myservo_3.write(90,30,false);

      }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to Former Member

    In the code above, there is an issue that I can't explain.

     

    Then I send the code to the Arduino, it thinks all the buttons have been pressed. In other words, all three valves open for the period they are supposed to be open, then they close.

     

    This does not bother me except for the fact that I don't know why it does that.

     

    Can anyone explain it to me?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 9 years ago in reply to Former Member

    In the code above, there is an issue that I can't explain.

     

    Then I send the code to the Arduino, it thinks all the buttons have been pressed. In other words, all three valves open for the period they are supposed to be open, then they close.

     

    This does not bother me except for the fact that I don't know why it does that.

     

    Can anyone explain it to me?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • clem57
    clem57 over 9 years ago in reply to Former Member

    // store state of 3 servos, HIGH is open

    int valveOpen_1;

    int valveOpen_2;

    int valveOpen_3;

     

    where is initial value = ???

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to Former Member

    Because the Start time is zero.

    startTime_1 = 0;

     

    When it gets to here

    if(millis() - startTime_1 >= valveOpenPeriod_1)

    it will always be true on the first pass, so it will do it's thing.

     

    You probably need to set the start time to millis() in Setup (rather than 0) which will stop it.

    You simply do this startTime_1 = millis();   and similar for the others.

     

     

    These do need something to have the extra qualifier added to the if statement (as I suggested earlier)

    They will always trigger each time the loop comes around.

    I also wonder if the sense is the right way, since the start time will always be less than millis() it potentially will always be greater than the ValveOpenPeriod_x.

     

    perhaps it should be

    if(millis() - startTime_1 <= valveOpenPeriod_1)

     

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to mcb1

    Thanks Mark that makes sense...I changed the if() statement to the following, which solves the issue:

     

    //if the button has been pressed, and we haven't elapsed the OpenPeriod yet, then open.

    if(startTime_1 > 0 && millis() - startTime_1 <= valveOpenPeriod_1)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to Former Member

    That looks like it would work to stop it triggering, but what happens after the button is pressed.

    Does it re-run again?

     

    I suggested the 'flag' variable simply because on more complicated code you can use it for other things.

    I've been in the situation where I did this because it was a short bit of code then later expanded it or re-used it.... image

     

    Mark