Arduino
  • Products
  • More
Arduino
Arduino Forum Searching for parts LARGE 7 segment displays
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 421 subscribers
  • Views 1081 views
  • Users 0 members are here
  • sports_technology
  • led
  • electrical
  • arduino
Related

Searching for parts LARGE 7 segment displays

e14 Contributor
e14 Contributor over 14 years ago

I'm working on a clock to be run off an arduino. I have most of my hardware down, including an LED controller chip, an RTC breakout board, etc. I have hooked up some 7 segment LEDs and am working on the code, but I have one big problem:

 

My project calls for very large displays. specifically, I'm looking to match the displays here, which look to be 7" (5.25" character height) dual character displays. they also interestingly have commas in the corner (instead of the decimal point on most 7 segment displays).

 

I've looked on various sites (octopart, jameco, many many more) but so far havent come up with many options. I found a 7" single character on sale at a couple sites (including element14), but it isn't a great match. I know there must be more variety made, as I see these all the time for scoreboards and such.

 

Does anyone know where I might find these displays?

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 12 years ago +1
    Every large 7-segment LED display I've seen uses rows of normal-size LEDs for each segment, probably hooked up in series and driven through constant-current voltage-boost LED drivers. You can use plastic…
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    Every large 7-segment LED display I've seen uses rows of normal-size LEDs for each segment, probably hooked up in series and driven through constant-current voltage-boost LED drivers.  You can use plastic bars to diffuse the LEDs so they look like continuous segments.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • goldenshuttle
    goldenshuttle over 12 years ago in reply to johnbeetem

    John idea works all the time. You may also abrase (file) strip shapes on a plain acrylic board to create 7 segment(or any other shape) then light each strip with one LED embedded .this works well if you get single high Lum LEDs, performs very well except in high glare surrounding.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • goldenshuttle
    goldenshuttle over 12 years ago in reply to johnbeetem

    John idea works all the time. You may also abrase (file) strip shapes on a plain acrylic board to create 7 segment(or any other shape) then light each strip with one LED embedded .this works well if you get single high Lum LEDs, performs very well except in high glare surrounding.