Arduino
  • Products
  • More
Arduino
Arduino Forum New ultra-low power Arduino board with built-in RF (RFM69)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 424 subscribers
  • Views 3940 views
  • Users 0 members are here
  • lorawan
  • lora
  • rfm69
  • cr2032
  • battery
  • step-up
  • low-power
  • iot
  • arduino
Related

New ultra-low power Arduino board with built-in RF (RFM69)

musskopf
musskopf over 10 years ago

Hi Everyone,

 

for some time now I've been designing and testing a new Dev board, which I've created to fulfill some requirements I normally have for our projects. I basically need good Wireless communication and, at the same time, be able to run my Arduino for some long periods on standard battery.

 

For that reason we've created the "Whisper Node", which I'm glad to announce it was successfully founded via Kickstarter and it's now a real product available to everyone. Additional details can be found on the following link: https://wisen.com.au/store/products/whisper-node-avr/

 

image

 

Please check it out, share with your friends and support this project if you believe it's interesting.

 

Update May/2017: After the success of the Whisper Node RFM69 version (Semtech SX1231), we're now producing the LoRa version, featuring an even more smart power management and using the RFM95 (Semtech SX1276) radio.

 

Thank you all!

+

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +2
    Hello Mike. Thanks for posting that, I was actually looking for something similar as I'm after some board to run my IoT projects on batteries. Your video mentioned something like "The first Arduino to…
  • mcb1
    mcb1 over 10 years ago +2
    During the Forget Me Not challenge, I ran across these. All about Moteino | LowPowerLab I used one for my Hot Water, but in my case it was powered, so low consumption wasn't the criteria. eLDERmon External…
  • musskopf
    musskopf over 10 years ago in reply to e14 Contributor +1
    Hi mmoebius, I understand your frustration, and that's why I've started this little project to share our expertise and make it available to general public. I'll try to answer your questions - sorry for…
Parents
  • michaelkellett
    michaelkellett over 10 years ago

    In your Kickstarter pitch you don't mention any RF testing, approvals or plans to get such approvals. Is this an oversight or are you just hoping for the best.  It is very unusual for an RF design to meet FCC or EU regulations without at least one test and tweak cycle.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 10 years ago

    In your Kickstarter pitch you don't mention any RF testing, approvals or plans to get such approvals. Is this an oversight or are you just hoping for the best.  It is very unusual for an RF design to meet FCC or EU regulations without at least one test and tweak cycle.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 10 years ago in reply to michaelkellett

    The RFM69 have some testing, and state that they meet FCC regulations.

     

    Not sure if it's true but there are documents here.

    http://www.hoperf.com/rf_transceiver/modules/RFM69HW.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • musskopf
    musskopf over 10 years ago in reply to michaelkellett

    Hi michaelkellett, we're looking into FCC but it's nothing something we are promising for a few reasons, including the elevated cost for testing. This still a very small scale product and any additional cost would make the end-price prohibitive for our target public. Also being a development board it can be used on so many ways which would simply void the certification. As mcb1 commented, the RFM69 module has some testing results for their product which cover the intentional emission component.

     

    Cheers,
    Mike M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to musskopf

    being a development board it can be used on so many ways which would simply void the certification

    That arguement was used by Raspberry Pi until they finally submitted them for FCC testing and approval.

     

    Your biggest enemy is the Australian Government who seem to have locked down every frequency.

    Because of the power and easily adjustable settings of the RFM devices, it might be hard to get a worldwide type approval as the user can simply program whatever they want.

     

    Most of the frequencies fall within the telemetry band, however we've seen that abused by people feeding continuous data streams.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • musskopf
    musskopf over 10 years ago in reply to mcb1

    Hi mcb1 sure when we hit the 5 millions units we'll have all our boards tested like RPI and Arduino image. For the moment it's difficult to guarantee it'll be done for less than 500 boards. If you have a look on many Dev boards, including some from big manufactures it's not common to find the "FCC" logo on all.

     

    Regarding the Australian Government, I don't consider to be the biggest enemy. I see it like any country to be honest. There are some frequencies/bands which can be used by any person in an open-class license arrangement so they can clearly specify what are the restrictions. A Dev board is like a car for me, I bet 99% of the cars can do almost twice the speed limit of any road, is up to the driver to use it within the legislation and don't do anything silly. Similar to that, I bet the Airport security will be very disappointed if you try to fly a FCC approved drone close to the runway.

     

    Finally, I agree with you that some people might abuse on those open frequencies, like that bad neighbor that listen loud music at 3AM.

     

    Cheers!

    Mike M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to mcb1

    I thought that one of the many reasons to use an approved module was to simplify the passage of the complete device through the compliance procedure.

    I'm not sure if it can in effect inherit the pass of the module in relevant aspects  or merely you can have a warm feeling that you are more likely to pass with such a module.

     

    A company who's name escapes me has started selling a much more expensive competitor to the HopeRF devices whilst complaining that the current modules have such wide specs they couldn't pass EMC...All very interesting !