Arduino
  • Products
  • More
Arduino
Arduino Forum Print a string on lcd
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 418 subscribers
  • Views 14332 views
  • Users 0 members are here
Related

Print a string on lcd

e14 Contributor
e14 Contributor over 14 years ago

Hello,

first of all, I’m new to Arduino’s world.

Sorry if this question is very basic.

 

I simply want to print a string on a Parallax YJ-162A lcd screen.

 

This is the code

 

SoftwareSerial lcd = SoftwareSerial(2, 6); //Set RX/TX pins for LCD

#include <SoftwareSerial.h>

SoftwareSerial lcd = SoftwareSerial(2, 6); //Set RX/TX pins for LCD

String ds;

 

void setup(){

      ds = "test";

      Serial.begin(9600);

      lcd.begin(9600);

      serial.print(ds);

      lcd.print(ds);

}

 

The compiler returns an error on line lcd.print(ds);

I don't understand why it is working with serial monitor and not with lcd.

this works fine : lcd.print("test");

If ds is a char it also works so I must convert a string to char ?

Or SoftwareSerial.h is wrong ?

 

Do you have a suggestion ?

Thanks for your help.

  • Sign in to reply
  • Cancel

Top Replies

  • ntewinkel
    ntewinkel over 14 years ago +1
    I don't know why that line would show an error for you, but not for me, as I simply did a cut and paste from what you had in your post. I'm using the very basic install of the Arduino software, without…
  • tronixstuff
    tronixstuff over 14 years ago +1
    Perhaps have a run through here - tronixstuff.com/tutorials and click on chapter 24
  • fustini
    fustini over 14 years ago in reply to e14 Contributor +1
    Hi, I tried compiling your example and got in Arduino 022: sketch_jan31a:8: error: no matching function for call to ‘SoftwareSerial::print(String&)’ I found this thread: http://www.arduino.cc/cgi-bin/yabb2…
Parents
  • ntewinkel
    ntewinkel over 14 years ago

    I don't know why that line would show an error for you, but not for me, as I simply did a cut and paste from what you had in your post.

    I'm using the very basic install of the Arduino software, without any added libraries. On a Mac though, which might be different.

     

    Another line I just noticed, that may be causing issues, is the lcd.begin(9600) line - shouldn't that be lcd.begin(16,2) ?

     

    Also, have you already tried running the HelloWorld example? (File - Examples - LiquidCrystal - HelloWorld)

    It does the display, but without the serial printouts you have in your code. You could add that as a second step once the first hurdle is cleared.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ntewinkel
    ntewinkel over 14 years ago

    I don't know why that line would show an error for you, but not for me, as I simply did a cut and paste from what you had in your post.

    I'm using the very basic install of the Arduino software, without any added libraries. On a Mac though, which might be different.

     

    Another line I just noticed, that may be causing issues, is the lcd.begin(9600) line - shouldn't that be lcd.begin(16,2) ?

     

    Also, have you already tried running the HelloWorld example? (File - Examples - LiquidCrystal - HelloWorld)

    It does the display, but without the serial printouts you have in your code. You could add that as a second step once the first hurdle is cleared.

     

    Cheers,

    -Nico