Arduino
  • Products
  • More
Arduino
Arduino Forum Interesting Idea
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 418 subscribers
  • Views 665 views
  • Users 0 members are here
Related

Interesting Idea

R_Phoenix
R_Phoenix over 14 years ago

http://arduino.cc/forum/index.php/topic,92040.0.html

 

Any input?

  • Sign in to reply
  • Cancel
  • Catwell
    Catwell over 14 years ago

    R,

     

    Not impossible. I can write and edit code in any word processor type program on any platform.

     

    What would be useful is a emulator on the phone, tablet, etc. (Run the code on virtual dev-boards or machines.)

     

    Alternatively, how about using the phone as the dev-board? Our dual-core, 1gb ram, based phones mop the floor with most Arduino boards I have seen.

     

    Cabe

    http://twitter.com/Cabe_e14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago

    I can see how someone with an Android tablet and external keyboard could want to run the Arduino IDE to develop sketches, compile and upload to an Arduino via USB.  I think the first step would be to get avrdude to run on Android, but I've not seen anyone doing that yet.

     

    Alternatively, I know that some folks run a chroot'd distro of Linux like Debian on Android devices.  That might make it possible to run avrdude in a normal Linux environment and possibly the IDE too if Java is installed and X running.  However, I'm not sure if access to the USB port would be a problem or not to actually connect to the Arduino for uploading.

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago

    I am most interested in being able to update the code in units useing the Arduino that are out in the feild. That would be easier than pulling the board, or lugging a Laptop to the feild.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to R_Phoenix

    Yeah, I can imagine many people using that capability.  A friend who does electronics workshops had talked about wanting to program kits with a mobile device, too.  I think the first requirement would be USB host mode which most Android tablets have and also more phones now too (like my Samsung Galaxy S2).  The second requirement would be installing a Linux distro which could run avrdude.  The XDA Developer forums are good place to look for Linux chroot install instructions for a specific device: http://forum.xda-developers.com/